Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
CPU-Slide11

As you can see, the starting location of the SFR (Special Function Register) and RAM are the same for the R8C CPU core as they are for the M16C core. The SFR begins at 0000H and the RAM area begins at 400 hex and expands up. Flash or ROM memory begins at 0FFFF (base 16) and expands down.

PTM Published on: 2011-12-30