Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
Concerto MCU Overview Slide 9

The Concerto™ F28M35x series is offered at three levels; an entry level at 60 MHz on both cores, a mid-end level with 75 MHz on each core, or a high-end level where the customer must choose between 75 MHz on the M3 core and 150 MHZ on the C2000 core, or each of the cores at 100 MHz. Each level has the option of connectivity, different memory sizes, and soon will have different package options. Concerto initially launched with the 144-pin QFP package and will be offered in a larger 289-pin VGA package in 2012.

PTM Published on: 2012-05-25