Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Product List
CAN2-Slide3

CAN specifications are international standards. Two versions are now in use: CAN 2.0A, the low-speed version (125kbps) that is sometimes known as Basic or Standard CAN, is defined by the ISO-11519 standard. CAN 2.0B, the high-speed version (1Mbps) that is known as Full CAN or extended-frame CAN, is defined by the ISO- 11898 standard. Bosch developed CAN technology in the mid 1980’s for automotive systems, which remain the biggest users of the over 200 million nodes per year. But CAN usage is growing in industrial control systems and many other applications, where it replaces point-to-point wiring. There are at least six main reasons for CAN’s popularity. One is its previously mentioned ability to provide essentially error-free communication. It has low wiring and node-connection costs and is readily scalable. Off-the-shelf development tools aid network designs and a growing number of ICs support the technology. Also, there is an increasing knowledge base of implementation experience.

PTM Published on: 2011-11-02