Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Product List
CAN2-Slide28

The CRC Field is sent by the transmitter and verified by all receivers to ensure that a Data Frame has been correctly received. The hardware in the transmitter node uses the CRC polynomial shown here to generate a 15-bit CRC code that is followed in the CRC Field by a recessive delimiter bit. The hardware at each receiver node on the CAN network generates a CRC on the observed Data Frame, then compares it to the transmitted CRC check value. If the receiver node detects a match, it puts a dominant bit into the ACK slot. If it detects a mismatch, though, it does not transmit anything in ACK slot. Instead, it sends a ‘NO’ vote after the upcoming ACK delimiter; that is, at End of Frame.

PTM Published on: 2011-11-02