Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
CAN Basics Part 1 Slide 23

The bottom three layers in the OSI communication model-Physical, Data Link and Network- are the Media layers. The top four-Transport, Session, Presentation and Application- are the Host layers. CAN by itself is only concerned with the lowest layers of the model. That is, ISO11898 defines the Data Link and Physical layers, which are shown here in red. Additionally, the CAN 2.0B specification covers a portion of the Transport layer: the retransmission/retry control function.

PTM Published on: 2011-11-02