The application of XLi98(C) to a component is simple to achieve in the prototyping stage as well as mass manufacturing. First, it is essential to ensure that the bonding surface is clean and free from contamination. Then, the pull tab is removed and the XLi98 is firmly pressed on to the surface with a gentle rocking motion. After the initial application, 70% of the ultimate adhesive strength will have been achieved. After 15 minutes, approximately 80 to 90% of the final strength will be achieved.