Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
SAM9 MPU Boot Solutions and Application Deployment Slide 15
The SAM-BA Boot is a monitor that provides In-System Programming solutions through different communication channels: DBGU serial port interface and the USB device port. In-System Programming (ISP) is the ability of some programmable logic devices, microcontrollers and other programmable electronic chips to be programmed while installed in a complete system, rather than requiring the chip to be programmed prior to installing it into the system. The SAM-BA offers several basic read/write commands (WORD, HALF WORD, BYTE) for direct access to the memory mapped and the peripheral registers. The SAM-BA monitor also checks, in an infinite loop, the two possible interfaces (USB/DBGU) until a communication is detected on one of them.
PTM Published on: 2011-10-18