Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
Slide8
As a recap of the significant features, the Bourns® AMS22S non-contacting Hall Effect sensor design is based on non-contacting magnetic technology using a magnet and a programmable quad Hall Effect IC. Because it is non-contacting, it is compatible with uses in harsh environments typically encountered in industrial applications such as vibration, shock, and fluid/dust ingress. The position sensor is programmable for various angles of rotation and the performance is highly repeatable. This product is also RoHS compliant in conformance with current RoHS directives.
PTM Published on: 2012-05-14