Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
Slide5
The Bourns® AMS22S non-contacting analog rotary position sensor with sintered bronze bushing has excellent performance over its lifetime. This is very important in applications where the cost of replacing the sensor is high, as well as applications where the sensor is in a remote location and access for repair and replacement is limited. As compared to contacting technologies, this position sensor provides extremely long life and reliability reducing the cost of repair and maintenance.
PTM Published on: 2012-05-14