Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
Slide3
There are a few important specifications to highlight. The output signal is analog and is ratiometric to the angular position of the shaft based on the 5 V input. Note that the voltage output of the Bourns® AMS22S non-contacting analog rotary position sensor is programmable. So, for applications requiring a smaller angle of travel, the output can be appropriately programmed at the factory. Independent linearity of ±0.5 % is standard with ±0.3 % available on request. Finally, as previously highlighted, rotational life is up to 50 million shaft revolutions.
PTM Published on: 2012-05-14