BC118 Datasheet by Sierra Wireless

33.32?! SIERRA WIRELESS’
Product Technical Specification
BC118
41110676
Rev 1
Product Technical Specification
Rev 1 Apr.17 2 41110676
Important
Notice
Due to the nature of wireless communications, transmission and reception of data
can never be guaranteed. Data may be delayed, corrupted (i.e., have errors) or be
totally lost. Although significant delays or losses of data are rare when wireless
devices such as the Sierra Wireless modem are used in a normal manner with a
well-constructed network, the Sierra Wireless modem should not be used in
situations where failure to transmit or receive data could result in damage of any
kind to the user or any other party, including but not limited to personal injury,
death, or loss of property. Sierra Wireless accepts no responsibility for damages
of any kind resulting from delays or errors in data transmitted or received using
the Sierra Wireless modem, or for failure of the Sierra Wireless modem to
transmit or receive such data.
Safety and
Hazards
Do not operate the Sierra Wireless modem in areas where blasting is in progress,
where explosive atmospheres may be present, near medical equipment, near life
support equipment, or any equipment which may be susceptible to any form of
radio interference. In such areas, the Sierra Wireless modem MUST BE
POWERED OFF. The Sierra Wireless modem can transmit signals that could
interfere with this equipment.
Do not operate the Sierra Wireless modem in any aircraft, whether the aircraft is
on the ground or in flight. In aircraft, the Sierra Wireless modem MUST BE
POWERED OFF. When operating, the Sierra Wireless modem can transmit
signals that could interfere with various onboard systems.
Note: Some airlines may permit the use of cellular phones while the aircraft is on the
ground and the door is open. Sierra Wireless modems may be used at this time.
The driver or operator of any vehicle should not operate the Sierra Wireless
modem while in control of a vehicle. Doing so will detract from the driver or
operator's control and operation of that vehicle. In some states and provinces,
operating such communications devices while in control of a vehicle is an offence.
Limitation of
Liability
The information in this manual is subject to change without notice and does not
represent a commitment on the part of Sierra Wireless. SIERRA WIRELESS AND
ITS AFFILIATES SPECIFICALLY DISCLAIM LIABILITY FOR ANY AND ALL
DIRECT, INDIRECT, SPECIAL, GENERAL, INCIDENTAL, CONSEQUENTIAL,
PUNITIVE OR EXEMPLARY DAMAGES INCLUDING, BUT NOT LIMITED TO,
LOSS OF PROFITS OR REVENUE OR ANTICIPATED PROFITS OR REVENUE
ARISING OUT OF THE USE OR INABILITY TO USE ANY SIERRA WIRELESS
PRODUCT, EVEN IF SIERRA WIRELESS AND/OR ITS AFFILIATES HAS BEEN
ADVISED OF THE POSSIBILITY OF SUCH DAMAGES OR THEY ARE
FORESEEABLE OR FOR CLAIMS BY ANY THIRD PARTY.
Notwithstanding the foregoing, in no event shall Sierra Wireless and/or its
affiliates aggregate liability arising under or in connection with the Sierra Wireless
product, regardless of the number of events, occurrences, or claims giving rise to
liability, be in excess of the price paid by the purchaser for the Sierra Wireless
product.
Preface
Rev 1 Apr.17 3 41110676
Patents This product may contain technology developed by or for Sierra Wireless Inc. This
product includes technology licensed from QUALCOMM®. This product is
manufactured or sold by Sierra Wireless Inc. or its affiliates under one or more
patents licensed from InterDigital Group and MMP Portfolio Licensing.
Copyright © 2017 Sierra Wireless. All rights reserved.
Trademarks Sierra Wireless®, AirPrime®, AirLink®, AirVantage® and the Sierra Wireless logo
are registered trademarks of Sierra Wireless.
Windows® and Windows Vista® are registered trademarks of Microsoft
Corporation.
Macintosh® and Mac OS X® are registered trademarks of Apple Inc., registered in
the U.S. and other countries.
QUALCOMM® is a registered trademark of QUALCOMM Incorporated. Used
under license.
Other trademarks are the property of their respective owners.
Contact
Information
Revision
History
Sales information and technical
support, including warranty and returns
Web: sierrawireless.com/company/contact-us/
Global toll-free number: 1-877-687-7795
6:00 am to 6:00 pm PST
Corporate and product information Web: sierrawireless.com
Revision
number
Release date Changes
1March 27, 2017 Initial conversion to SWI template.
—>>I
Rev 1 Apr.17 4 41110676
Contents
Introduction . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . .5
Applications . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 6
Key Specifications . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 6
General Specifications . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 6
RF Specifications . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 6
Electric Specifications. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 7
Power Measurements with Melody . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . .8
Physical Characteristics . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . .9
Module Drawing . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 9
Module Footprint. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 10
Placement Considerations . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 11
PIN Descriptions. . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 11
Notes . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 13
Hardware Design Guidelines . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . .14
BC118 with Battery and Host . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 14
BC118 with Fixed Supply and Host . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 14
BC118 with Battery and No Host . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 15
BC118 with Fixed Supply and No Host . . . . . . . . . . . . . . . . . . . . . . . . . . . . 15
Notes . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 15
Solder Reflow Profile . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . .16
Regulatory Certifications . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 17
United States - FCC . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 17
Canada IC . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . . 18
Bluetooth Qualification Program (BQP) . . . . . . . . . . . . . . . . . . . . . . . . . . . . 18
BC118 HAL le nn 4V Influx-(I FART smpcmk MCI L!- PW“ N > R0“ ijllz smu- m“. RU“ I/0 ~ MO > kit-11m "N [:11 SI’I \ >
Rev 1 Apr.17 5
41110676
1
1: Introduction
BC118 is a highly flexible, ultra low power, small form factor Bluetooth Version 4.1
Certified module. It comes preloaded with Sierra Wireless Melody Smart software,
and is ideal for developers who want to quickly and cost effectively integrate Bluetooth
Low Energy functionality into their products or develop standalone sensors or
accessories.
Figure 1-1: BC118
Note: this is an example image and does not represent the label used on commercial
shipments.
Figure 1-2: BC118 Flow Diagram
Product Technical Specification
Rev 1 Apr.17 6 41110676
Applications
Industrial Automation
Lighting
Automotive
Medical Devices
Wearable Devices
Sensors, Actuators
Key Specifications
Bluetooth Certified 4.1 Audio module
Single Mode: Bluetooth Low Energy (BLE)
Embedded Bluetooth Protocol Stack
Supports GATT Profile, Audio, Proximity, and iBeacon
Supports I2C and UART transparent Data Modes
Simple UART, GPIO, APP interface for command and control
Small form factor (19.3mm x 14.4mm x 2.8mm)
General Specifications
RF Specifications
Table 1-1: General Specifications
Specification Description
Bluetooth Standard Bluetooth 4.1
Interfaces UART, AIO, GPIO, USB, I2C
Size 19.3mm x 14.4mm x 2.8mm
Weight 0.9g
Table 1-2: RF Specifications
Specification Description
Frequency Band 2,402 MHz to 2,480 MHz
Modulation 8 DPSK, PI/4 DQPSK, GFSK
Maximum Data Rate 270kbps (typical 60kbps)
Operating Range Up to 50m
RF Sensitivity 0.1% BER at -92.5dBm
Transmit Power 7.5dBm
Introduction
Rev 1 Apr.17 7 41110676
Electric Specifications
Table 1-3: Electrical Specifications
Specification Description
Supply Voltage 1.8V to 3.6V DC (Supports Lithium battery voltage
range)a
a. For using SLEEP MODE (for low power consumption), the maximum voltage is 3.8V.
Typical Current Tx 16mA (Only on Tx/Rx)
Typical Deep Sleep <8µA (Connected)
Typical Hibernate <1.9µA (Not Connected)
Typical Dormant <900nA
Operating Temperature -40°C to 85°C
Storage Temperature -40°C to 105°C
Rev 1 Apr.17 8
41110676
2
2: Power Measurements with Melody
All measurements made with Melody Smart configured to: SLEEP=ON, TRSE=ON,
TRSM=1, WAKE=OFF. Please refer to Melody Smart UART manual for more details.
UART disconnected to remove leakage, RX pin pulled high via a 5k6 resistor (resistor
leakage current included in current measurement values).
For Send/Receive tests wired loopback used on UART interface connecting TX to RX
pins on device measured.
Measurements performed using analogue integration across a 1 1% resistor
measured with an Agilent 5½ digit Digital Multimeter at 100mA precision.
Table 2-1: Reference Power Measurements
Set Up Idle [mA] Fast
Advertisinga
[mA]
Slow
Advertising
[mA]
Scanningb
[mA]
Connected
Idlec
[mA]
Connected
Send+Recvd
[mA]
Melody
Smart
Defaulte
0.008 0.478 0.043 4.650 0.430 0.5.00f
Lowest
Powerg0.008 NA 0.032 0.100 0.010 0.045h
a. Applicable to Melody Smart in Peripheral mode only.
b. Applicable to Melody Smart in Central mode only.
c. Tested with Slave latency equal to zero. Peripheral consumption can be lower with a larger a slave latency.
d. Applicable to Melody Smart in Central mode only.
e. Measurements done using the default Melody Smart Advertisement, Connection and Scan parameters;
f. Send and receive of 1 20 byte packet/s at 9600 baud UART.
g. Measurements done using Melody Smart configured to: ADVP=2800 2800, SCNP=009C400 000009C4,
CONP=0C80 0C80 0006 0C80.
h. Send and receive of 1 20 byte packet/connection interval at 9600 baud UART.
Module Drawin 14.4mm ' A— E ; GND CLEARANCE AREA ('9 1 35 '0.8mm E I. r} I l 20.4mm m T 12 24_ '_ _ O 1.2mm M13 I0I 23.4 1.2mm 0,8mm
Rev 1 Apr.17 9
41110676
3
3: Physical Characteristics
Module Drawing
Figure 3-1: Module Drawing
l T nAmm Ii 2mm f Und Pad Dal-i III 205”” f-’. .mm 11mm Mm summ- 19 3mm _| 1.03m 11.2mm (-1“ — _ - 078mm I I I Wham,“ 12mm M 0 8mm E 6ND CLEARANCE AREA mm um: m u..- !:1 0.3mm , mm Sch-V I D-Bm'“ 134""; M'm Ewan-m
Product Technical Specification
Rev 1 Apr.17 10 41110676
Module Footprint
Figure 3-2: Module Footprint
GND CLEARANCE AREA 39mm Place mowle on me man: edge all around shou‘d be removed 1mm me mam am an all lam 01M PCB m :mm gamma» antenna PCB
Physical Characteristics
Rev 1 Apr.17 11 41110676
Placement Considerations
Figure 3-3: Placement Layout
PIN Descriptions
Note: No1 is top left on the module after which the PINS are ordered anti clockwise.
Table 3-1: Pin Descriptions
No Pin Name Pin Type Pin Description
1GND GND Common Ground
2GND GND Common Ground
3AIO_2 Bi-Directional Analog programmable input/output line
4AIO_1 Bi-Directional Analog programmable input/output line
5AIO_0 Bi-Directional Analog programmable input/output line
6UART_TX Bi-Directional UART TX Data
7UART_RX Bi-Directional UART TX Data
8PIO_3 Bi-Directional Programmable input/output line
Product Technical Specification
Rev 1 Apr.17 12 41110676
Notes
9PIO_4 Bi-Directional Programmable input/output line
10 PIO_5/
SPI_CLK
Bi-Directional Programmable input/output line
11 PIO_6/
SPI_CSB
Bi-Directional Programmable input/output line
12 GND GND Common Ground
13 GND GND Common Ground
14 PIO_7/
SPI_MOSI
Bi-Directional Programmable input/output line
15 GND GND Common Ground
16 GND GND Common Ground
17 VDD_PADS Supply Positive Supply Input
18 GND GND Common Ground
19 PIO_8/
SPI_MISO
Bi-Directional Programmable input/output line
20 SPI_PIO# Input Select SPI/PIO
21 PIO_2 Bi-Directional Programmable input/output line
22 I2C_SCL Bi-Directional Programmable input/output line
23 GND GND Common Ground
24 GND GND Common Ground
25 I2C_SDA Bi-Directional Programmable input/output line
26 PIO_9 Bi-Directional Programmable input/output line
27 VBAT Battery terminal +ve Battery Positive
28 PIO_10 Bi-Directional Programmable input/output line
29 PIO_11 Bi-Directional Programmable input/output line
30 WAKE Wake Pin Wake Pin
31 GND GND Common Ground
32 GND GND Common Ground
33 GND GND Common Ground
34 GND GND Common Ground
35 GND GND Common Ground
Table 3-1: Pin Descriptions
No Pin Name Pin Type Pin Description
Physical Characteristics
Rev 1 Apr.17 13 41110676
Notes
PIO_X are bidirectional with weak pull down
Reset Input is with strong pull-up
UART are Bidirectional with weak pull up
w, M ,f m :n ‘4? 5 i a x In \ _ s < ,="" w”="" —.,="" mm="" m,="" ww="" i="" (vflm‘flgm‘vkl="" mi,="" in="" mu="" mw="" \mul,="" ""“mh‘m‘”="" ‘="" u="" ,="" (.="" -_="" h,”="" “#m="" .="" a,="" ~="" wm,%2_r="" “m,="" 14“”:="" 3="" m3,="" 105‘;="" a="" w“="" a150="" 5‘="" "a“="" plum="" 94%="" ho="" .mm="" mum,="" .="" mk";="" mum"="" guy”)="" 1,="" w=""> anml , g x g , A g z : “Wm,” WWW , , a , WW“: m 325%? /, yerxll/x : X) H V‘ARHLN , \ memm m \u > M, 4W, AmL‘m-l mMcHle IKIIXHu’UiMMu‘: IML‘" 1mm?“ . , ,,,, \ ‘le 'IH v NW 143:}: #1 M .mh; \ < mn#4¥,="" mm,="" .="" ,="" h="" ,w="" .m,="">
Rev 1 Apr.17 14
41110676
4
4: Hardware Design Guidelines
BC118 with Battery and Host
Figure 4-1: Hardware Design for BC118 with Battery and Host
BC118 with Fixed Supply and Host
Figure 4-2: Hardware Design for BC118 with Fixed Supply and Host
w 2 a x»; mm E g ; WWW }§ mam E A M . mums”. mm M y m .m mm pm $8 4 :9; m.) 1.. .m m .w_, m» wmmm 9;.“me 1mm .Jm_. .m m7) xfl_.m m m m .v—m.m m m m a,&.m m. m mun a mm, «mm m.» Am, "WW eggegggggegags mm, oooaooucoocouc vm, WP" u 5““.th a flu strum» g E ; ”(ammo Raisin : , mmmmm} $63“ 9 mama.» mum“ , ,una) M Ana) , M, M m m.» m ”(H)“.- QQEQEEEQEEEQEE mun-xv...- \ x 2 n
Hardware Design Guidelines
Rev 1 Apr.17 15 41110676
BC118 with Battery and No Host
Figure 4-3: Hardware Design for the BC118 with Battery and No Host
BC118 with Fixed Supply and No Host
Figure 4-4: Hardware Design for the BC118 with Fixed Supply and No Host
Notes
The voltage applied to VBAT should meet a maximum rise time (VBAT = 0V
to VBAT = 1.8V) of 5ms under all circumstances.
250 217 110 15 mln
Rev 1 Apr.17 16
41110676
5
5: Solder Reflow Profile
The solder profile is described below.
Figure 5-1: Solder Profile
Zone A: Preheat: This raises the temperature at a controlled rate, typically 0.5 - 2C/s.
This will preheat the component to 120°C to 150°C to distribute the heat uniformly to
the PCB.
Zone B: Equilibrium1: In this zone, the flux becomes soft and uniformly spreads
solder particles over the PCB board, preventing re-oxidisation. The recommended
temperature for this zone is 150°C to 200°C for 60s to 120s.
Zone C: Equilibrium2: This is optional and in order to resolve the upright component
issue. Temperature is 210°C to 217°C for 20s to 30s.
Zone D: Reflow zone: The temperature should be high enough to avoid wetting but
low enough to avoid component deterioration. The recommended peak temperature is
230°C to 250°C. The soldering time should be 30s to 90s when the temperature is
above 217°C.
Zone E: Cooling: The cooling rate should be fast to keep the solder grains small
which will give a longer lasting joint. A typical cooling rate is 4°C/s.
Rev 1 Apr.17 17
41110676
A
A: Regulatory Certifications
Caution: Unauthorized modifications or changes not expressly approved by Sierra Wireless
could void compliance with regulatory rules, and thereby your authority to use this equipment.
The BC118 module is designed to meet, and upon commercial release, will meet the
requirements of the following regulatory bodies and regulations, where applicable:
Federal Communications Commission (FCC) of the United States
The Certification and Engineering Bureau of Industry Canada (IC)
Ministry of Internal Affairs and Communications (MIC) of Japan
Radio Equipment and Telecommunications Terminal Equipment (R&TTE)
Directive of the European Union
Upon commercial release, the following industry certification will have been obtained,
where applicable:
Bluetooth SIG
Additional certifications and details on specific country approvals may be obtained
upon customer request — contact your Sierra Wireless account representative for
details.
Additional testing and certification may be required for the end product with an
embedded BC118 module and are the responsibility of the OEM. Sierra Wireless
offers professional services-based assistance to OEMs with the testing and
certification process, if required.
United States - FCC
The BC118 module, upon commercial release, will have been granted modular
approval by the FCC. Integrators may use the BC118 module in their end products
without additional FCC certification if the following conditions are met.
At least 20 cm separation distance between the antenna and the user’s body
must be maintained at all times.
The BC118 module must not be collocated with any other transmitter within a
host device.
The regulatory label on the end product must include the text “Contains FCC ID:
SSS-BC11X” and the following compliance statement:
This device complies with Part 15 of the FCC Rules. Operation is subject to the
following two conditions: (1) This device may not cause harmful interference,
and (2) this device must accept any interference received, including interfer-
ence that may cause undesired operation.
A user manual with the end product must clearly indicate the operating requirements
and conditions to ensure compliance with current FCC RF exposure guidelines.
The end product with an embedded BC118 module may also need to meet the FCC
Part 15 unintentional emission requirements and be properly authorized per FCC Part
15 Subpart B.
I¢I m 122:3;
Product Technical Specification
Rev 1 Apr.17 18 41110676
Canada IC
The BC118 module, upon commercial release, will have been granted modular
approval by IC. Integrators may use the BC118 module in their end products
without additional IC certification if the following conditions are met.
At least 20 cm separation distance between the antenna and the user’s body
must be maintained at all times.
The BC118 module must not be collocated with any other transmitter within a
host device.
The regulatory label on the end product must include the text “Contains IC :
11012A-BC11X” and the following compliance statement:
This device complies with Industry Canada license-exempt RSS standard(s).
Operation is subject to the following two conditions: (1) this device may not
cause interference, and (2) this device must accept any interference,
including interference that may cause undesired operation of the device.
Le présent appareil est conforme aux CNR d'Industrie Canada applicables
aux appareils radio exempts de licence. L'exploitation est autorisée aux deux
conditions suivantes: (1) l'appareil ne doit pas produire de brouillage, et (2)
l'utilisateur de l'appareil doit accepter tout brouillage radioélectrique subi,
même si le brouillage est susceptible d'en compromettre le fonctionnement.
Bluetooth Qualification Program (BQP)
In case no other non-certified Bluetooth components are incorporated, the
BC118's BQP marking certification allows users to integrate the module into
products without the need to obtain subsequent and separate approval.
The BC118 has been approved by the Bluetooth Qualification Body (BQB) to
use the Bluetooth trademark and to offer official Bluetooth functionality. The
approval according to the V4.0B Bluetooth specification confirms that the
module complies with the Bluetooth specification and will successfully
operate with other products supporting the same profile. BQP certification
also ensures that the module has gone through safety assessment. This
certification was granted through a combination of product performance
testing and interoperability testing. This certification applies globally.
Labelling
Products complying with all relevant requirements are allowed to bear the
official Bluetooth logo
For further information regarding the BQP certification requirements please
review the following websites:
Bluetooth Special Interest Group:
https://www.bluetooth.org/apps/content/