30
W0."
‘o
t
WWI WOW
m-m
AVQGO
vzcuuoLooxss
For product information and a complete list of distributors, please go to our web site: www.avagotech.com
Avago, Avago Technologies, and the A logo are trademarks of Avago Technologies in the United States and other countries.
Data subject to change. Copyright © 2005-2015 Avago Technologies. All rights reserved. Obsoletes 5989-2159EN
AV02-0235EN - February 11, 2015
Propagation Delay, Pulse-Width Distortion and Propagation Delay Skew
operating temperature). As illustrated in Figure 23, if the
inputs of a group of optocouplers are switched either ON
or OFF at the same time, tPSK is the difference between the
shortest propagation delay,either tPLH or tPHL, and the
longest propagation delay,either tPLH or tPHL.
As mentioned earlier,tPSK can determine the maximum
parallel data transmission rate. Figure 24 is the timing
diagram of a typical parallel data application with both
the clock and the data lines being sent through opto-
couplers. The figure shows data and clock signals at the
inputs and outputs of the optocouplers. To obtain the
maximum data transmission rate, both edges of the
clock signal are being used to clock the data;if only one
edge were used, the clock signal would need to be twice
as fast.
Propagation delay skew repre- sents the uncertainty of
where an edge might be after being sent through an op-
tocoupler. Figure 24 shows that there will be uncertainty
in both the data and the clock lines. It is important that
these two areas of uncertainty not overlap, otherwise the
clock signal might arrive before all of the data outputs
have settled,or some of the data outputs may start to
change before the clock signal has arrived. From these
considerations, the absolute minimum pulse width that
can be sent through optocouplers in a parallel applica-
tion is twice tPSK. A cautious design should use a slightly
longer pulse width to ensure that any additional uncer-
tainty in the rest of the circuit does not cause a problem.
The tPSK specified optocouplers offer the advantages of
guaranteed specifications for propagation delays, pulse-
width distortion and propagation delay skew over the
recommended temperature, input current, and power
supply ranges.
Figure 23. Propagation delay skew – tPSK.Figure 24. Parallel data transmission example.
Propagation delay is a figure of merit which de-
scribes how quickly a logic signal propagates through
a system. The propagation delay from low to high
(tPLH) is the amount of time required for an input signal to
propagate to the output, causing the output to change
from low to high. Similarly, the propagation delay from
high to low (tPHL) is the amount of time required for the
input signal to propagate to the output causing the
output to change from high to low (see Figure 16).
Pulse-width distortion (PWD) results when tPLH and tPHL differ
in value. PWD is defined as the difference between tPLH and
tPHL and often determines the maximum data rate capability
of a transmission system. PWD can be expressed in percent
by dividing the PWD (in ns) by the minimum pulse width
(in ns) being transmitted. Typically, PWD on the order of
20-30% of the minimum pulse width is tolerable; the exact
figure depends on the particular application (RS232, RS422,
T-l, etc.).
Propagation delay skew,tPSK, is an important parameter
to consider in parallel data applica- tions where synchro-
nization of signals on parallel data lines is a concern. If
the parallel data is being sent through a group of op-
tocouplers, differences in propagation delays will cause
the data to arrive at the outputs of the optocouplers at
different times. If this difference in propagation delays
is large enough, it will determine the maximum rate at
which parallel data can be sent through the optocou-
plers.
Propagation delay skew is defined as the difference
between the minimum and maximum propagation
delays,either tPLH or tPHL, for any given group of optocou-
plers which are operating under the same conditions (i.e.,
the same drive current, supply voltage, output load, and
50%
50%
tPSK
IF
VO
IF
VO
1.5 V
1.5 V
DATA
INPUTS
CLOCK
DATA
OUTPUTS
CLOCK
tPSK
tPSK