In summary, the RX 10-bit A/D is a single successive approximation converter that is capable of handling up to 12 analog input channels. The ADC has three different operating modes which are Single Mode, Continuous Scan Mode and One-Cycle Scan Mode. The RX 10-bit ADC also has a self-diagnostic feature which simplifies the verification of the operating status of the ADC system. Finally, the ADC sampling time can also be adjusted which can be useful when the source impedance is high or a very slow P-clock is being used.