Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Product List
SF-Slide8

The illustration on this slide details the basic operation of the SF70 series. Inserting the SIM card is accomplished by inserting the card in an appropriate tray and then inserting the tray into the connector through the opening in the chassis. Removal of the card requires the user to insert an ejection pin through the hole provided in the tray to depress the actuator pin, which ejects the tray and allows removal of the card.

PTM Published on: 2015-12-17