+12V Power-Over-Ethernet
Application Kit
Hardware Reference
Digi document reference number: 90000940
© Digi International Inc. 2008. All Rights Reserved.
The Digi logo is a registered trademark of Digi International, Inc.
All other trademarks mentioned in this document are the property of their respective owners.
Information in this document is subject to change without notice and does not represent a
commitment on the part of Digi International.
Digi provides this document “as is,” without warranty of any kind, expressed or implied, including,
but not limited to, the implied warranties of fitness or merchantability for a particular purpose. Digi
may make improvements and/or changes in this manual or in the product(s) and/or the program(s)
described in this manual at any time.
This product could include technical inaccuracies or typographical errors. Changes are periodically
made to the information herein; these changes may be incorporated in new editions of the
publication.
Digi International Inc.
11001 Bren Road East
Minnetonka, MN 55343 (USA)
* +1 877 912-3444 or +1 952 912-3444
http://www.digi.com
2
3
Contents
Contents ........................................................................................................ 3
1
Overview .................................................................................................. 4
1.1Introduction to PoE ................................................................................................................................ 4
2
Detailed description ................................................................................. 5
2.1POE_12V_JS_0 ...................................................................................................................................... 5
2.1.1Mechanical .......................................................................................................................................................... 5
2.1.2Flyback Transformer ......................................................................................................................................... 6
2.1.3Current Limit / Current Sense .......................................................................................................................... 7
2.1.4Working Frequency ............................................................................................................................................ 7
2.1.5Error Amplifier ................................................................................................................................................... 7
2.2PoE module usage ................................................................................................................................... 7
3
Connectors pinout .................................................................................... 8
3.1Connector P1 .......................................................................................................................................... 8
3.2Connector P2 .......................................................................................................................................... 8
4
Application notes from National Semiconductors .................................. 9
1.1 Introduction to PoE
+12V Power-Over-Ethernet Application Kit - Hardware Reference
1
Overview
This document defines the characteristics of the PoE application kit board. This application kit
provides a reference design for PoE on the Power Device side using National LM5070 device.
The POE_12V_JS board is an extra-power module which can be plugged on the Digi JumpStart
development boards, providing +12V power supply to the JumpStart boards.
1.1
Introduction to PoE
Ethernet is becoming the standard communication interface of peripheral devices beyond
networked computers. In a PoE environment the Ethernet not only transports data between
computers and devices, but also provides power so that connected PoE capable devices do not need
separate power supplies.
Power over Ethernet gradually has became an industry standard and is covered by IEEE 802.3af.
The proposed standard can accommodate power over either the data transmission pairs or the spare
pairs of the Ethernet cable.
There are two sides to the Power over Ethernet system. The side that provides power is called
power Source Equipment (PSE) side, and the side that consumes power is called Power Device
(PD) side. A detection scheme is designed to detect if there is PD connected at the destination. This
prevents applying power to a non PoE system.
After a PD is detected the PoE sides has to match the power delivering capability of the PSE and
the power consumption of the PD. This is called power classification stage.
After a valid classification is determined and a match between PSE and PD is found, the PSE
applies a nominal 48V DC across the power delivering lines. The PD regulates the power down to
its needs.
4
2.1 POE_12V_JS_0 POE712V7JS P2 P1 I I I I I I I I I I Development Board
+12V Power-Over-Ethernet Application Kit - Hardware Reference
2
Detailed description
2.1
POE_12V_JS_0
The POE_12V_JS application kit is designed to provide an IEEE802.3af compliant, Power over
Ethernet (PoE) 12V power supply. This application kit is based on the National Semiconductor
LM5070 device.
The LM5070 is a power interface port and pulse width modulation(PWM) controller used in
Powered Devices (PD) that connect into Power over Ethernet (PoE) systems. This device complies
to the power detection, level classification, and does the power regulation for the end system. For
the LM5070 specific information and functional description please refer to the datasheet.
General performance features of the application kit are:
Fully compliant 802.3af Power Interface Port
Fully isolated +12V output
Input range: 32 to 57V
Output current: 0 to 1A
Output frequency: 20KHz
2.1.1
Mechanical
The module is connected to the JumpStart Kits through two one row, right angle, SMD, RM2.54
connectors. The first one (P1) is a four pin connector that provides access to the PoE signals
coming from the Ethernet interface. The second one (P2) is a six pin connector that provides the
output power supply from the PoE module. The module makes a right-angle with the development
board.
The size of the POE_12V_JS board is 65.88 x 25 mm.
The following figure shows the placement of the POE_12V_JS board.
5
N :l a S/N :. z a a :I m [MAC] :. a a n B L1 L} U LAEL‘ I: EB DEI P2
+12V Power-Over-Ethernet Application Kit - Hardware Reference
Figure 1. POE_12V_JS_0 TOP Placement
Figure 2. POE_12V_JS_0 BOTTOM Placement
2.1.2
Flyback Transformer
The flyback transformer is a coupled inductor with multiple windings wound on a single gapped
core. For simplification, we refer to the first, driven winding, as the primary and the main output
winding as the secondary winding of the flyback transformer.
The flyback converter is a converter in which inductive energy is stored by applying a voltage
across the primary in a similar manner to that of a boost converter. A second coupled winding
(secondary) of the inductor transfers the energy to a secondary side rectifier after the primary
voltage has been switched off.
In the PoE application kit, the LM5070 directly drives a MOSFET switch to apply voltage across
the primary. When the switch turns off, the secondary applies a forward current to the output
rectifier and charges the output capacitors.
6
1 RT: — Fx330x10“2 2.2 PoE module usage
+12V Power-Over-Ethernet Application Kit - Hardware Reference
2.1.3
Current Limit / Current Sense
The LM5070 provides a cycle-by-cycle over current protection function. Current limit is
accomplished by an internal current sense comparator. If the voltage at the current sense
comparator input CS exceeds 0.5V with respect to RTN/ARTN, the output pulse will be
immediately terminated. A small RC filter, located near the CS pin of the controller, is
recommended to filter noise from the current sense signal because the LM5070 current sense and
PWM comparators are very fast, and may respond to short duration noise pulses.
The PoE application kit has a 0.33R sense resistor that limits the output current to 1.5A for the 12V
signal.
2.1.4
Working Frequency
A single external resistor connected between the RT and ARTN pins sets the LM5070 oscillator
frequency. In the LM5070-50 the internal oscillator operates at twice the frequency of the output
(OUT). To set a desired output operational frequency, the RT resistor can be calculated from:
In the PoE application kit the RT resistor is 15KHz, so the output operational frequency is set to
20KHz.
2.1.5
Error Amplifier
An internal high gain error amplifier is provided within the LM5070. The amplifier’s non-inverting
reference is set to a fixed reference voltage of 1.25V. The inverting input is connected to the FB pin
For the PoE application kit the error amplifier function is implemented on the secondary side of the
converter and the internal error amplifier is not used. The internal error amplifier is configured as
an open drain output and can be disabled by connecting the FB pin to ARTN. An internal 5K pull-
up resistor between a 5V reference and COMP can be used as the pull-up for an optocoupler in
isolated applications.
2.2
PoE module usage
The POE_12V_JS application kit provides a +12V supply voltage. This +12V_POE supply output
is connected directly to the power switch of the JumpStart kit board through a diode and so we
reuse the Jump Start power controller, which provides +5V (and also +/-12V) from the input power
supply 9-30V (in our case the input power supply is +12V_POE).
The POE module can be used directly once it’s plugged on the Jump Start boards. In this case, the
module replaces the input power supply plug and so provides all internal power supplies.
7
3.1 Connector P1 3.2 Connector P2
+12V Power-Over-Ethernet Application Kit - Hardware Reference
3
Connectors pinout
3.1
Connector P1
Pin Description Comments
1 POE_TX_CT
2 POE_RX_CT
3 POE_RJ45_4/5
4 POE_RJ45_7/8
3.2
Connector P2
Pin Description Comments
1 +12V
2 +12V
3 GND
4 GND
5 POE_GND
6 POE_GND
8
+12V Power-Over-Ethernet Application Kit - Hardware Reference
9
4
Application notes from National Semiconductors
- Application Note 1358: LM5070 "AE" Evaluation Board
http://www.national.com/an/AN/AN-1358.pdf
- LM5070 Reference Design - Isolated Power-over-Ethernet (POE) Regulator, Low-cost, High
Efficiency 5V 7W Output
http://www.national.com/rd/PAhtml/PADC_POE_5V_7W_ISO.html

Products related to this Datasheet

KIT POE APPLICATION