LMP91000EVAL User Guide Datasheet by Texas Instruments

View All Related Products | Download PDF Datasheet
Q; TEXAS INSTRUMENTS
User’s Guide
SNAU121- June 2012
LMP91000EVM User’s Guide
SNAU121-April 2012 LMP91000EVM User’s Guide 1
CONTENTS
1 INTRODUCTION ....................................................................................................... 1
2 SETUP ....................................................................................................................... 1
3 BOARD LAYOUT ..................................................................................................... 5
4 SCHEMATIC ............................................................................................................. 7
LIST OF FIGURES
Figure 1: Gas sensor’s footprint .......................................................................................... 2
Figure 2: 2-WIRE Jumper Settings ..................................................................................... 2
Figure 3: J_MENB Jumper Settings ................................................................................... 3
Figure 4: Connection of the LMP91000EVM to SPIO4 board ............................................ 3
Figure 5: Top Layer Routing ............................................................................................... 5
Figure 6: Bottom Layer Routing .......................................................................................... 6
Figure 7: LMP91000EVM Schematic .................................................................................. 7
LIST OF TABLES
Table 1: Device and Package Configurations .................................................................... 1
Table 2: Recommended p-FETs for short circuiting RE and WE when LMP91000 is OFF 2
Table 2: LMP91000EVM Bill of Materials ........................................................................... 8
1. Introduction
The Texas Instruments LMP91000EVM evaluation module (EVM) helps designers evaluate the operation and
performance of the LMP91000 Sensor Analog Front End for Electrochemical sensor. The LMP91000EVM is
part of the Sensor AFE eval platform
The EVM contains one LMP91000, (See Table 1).
Table 1: Device and Package Configurations
DEVICE
IC
PACKAGE
U1 LMP91000SD LLP-14
The LMP91000EVM is provided with a 16 bit ADC (ADC161S626) in order to capture the output of the LMP91000.
The LMP91000EVM is not provided with any gas sensor. It supports 3-lead electrochemical cells and 2-lead
galvanic cell in potentiostat configuration.
2. Setup
This section describes the jumpers and connectors on the EVM as well and how to properly connect, set up
and use the LMP91000EVM in the Sensor AFE eval platform.
INSTRUMENTS
2 LMP91000EVM User’s Guide SNAU121-April 2012
2.1. Gas Sensor Connection
Both 3-lead and 2-lead gas sensor need to be placed in the Gas Sensor Fooptrint
Figure 1: Gas sensor’s footprint
2.1.1. Not Biased Gas sensor
Even if the LMP91000 is provided with an internal switch to short the RE and WE pin that can be enabled
when the device is in Deep sleep mode, it is possible to add an external JFET which makes the same feature
when the gas sensor is left connected to the board and the LMP91000 is turned off.
The JFET (Q1) should be a p-type FET. Recommended FETs are listed in the table below.
The gate resistance R12 can be populated with a 1kohm resistor.
Table 2: Recommended p-FETs for short circuiting RE and WE when LMP91000 is OFF
DEVICE
IC
DESCRIPTION
MANUFACTURER
Q1
PMBFJ177
P-channel Silicon Junction Field-
effect Transistor
NXP SEMICONDUCTOR
SOT23
SST177 VISHAY SILICONIX
MMBF177 Fairchild
2.2. Jumpers Configuration
2-WIRE is the jumper which shorts CE and RE pin when a 2-lead gas sensor is connected to the LMP91000.
2-WIRE
2-lead gas
sensor
2-WIRE
3-lead gas
sensor
Figure 2: 2-WIRE Jumper Settings
J_MENB configures the Module Enable of the LMP91000 either manual or controlled by external
microcontroller. In manual mode, the Module Enable of the LMP91000 is tied to GND. When the
LMP91000EVM is connected to the SPIO4 board pin 1-2 need to be shorted.
g
SNAU121-April 2012 LMP91000EVM User’s Guide 3
J_MENB
Manual
J_MENB
Microcontroller
Figure 3: J_MENB Jumper Settings
2.3. Connection of the LMP91000EVM to SPIO4 Board
The SPIO4 board is a data capture board required when the LMP91000 is used in the Sensor AFE eval
platform. The LMP91000EVM is connected to the SPIO4 board through the SPIO-GPSI16 connector.
The white arrows present on both LMP91000EVM and SPIO4 board need to be aligned in order to guaranty
the right connection.
Figure 4: Connection of the LMP91000EVM to SPIO4 board
2.4. LMP91000EVM as part of Sensor AFE eval platform
When the LMP91000EVM is part of the Sensor AFE eval platform it doesn’t require any external power
supply to properly work.
Before using the Sensor AFE eval platform make sure the following steps have been accomplished:
1. Install the Graphical User Interface of the LMP91000EVM
2. Connect the LMP91000EVM to the SPIO4 board
3. Connect the USB cable to SPIO-4 board
4. Connect the other end of the USB cable to an available USB port on the computer
5. Run the Graphical User Interface
The voltage at VDD pin of the LMP91000 (VDD test point) is 3.3V, the voltage at VREF pin of the LMP91000
(VREF test point) is 2.5V. The LMP91000EVM is ready to work.
2.5. LMP91000EVM In Standalone Operation (without ADC)
The LMP91000EVM can be used as a standalone board. In this case it requires the following voltages
2.5.1. Jumper/s setting
J_MENB - pin 2 and 3 shorted (manual mode), if on the I2C bus already exist a device with the same
address of the LMP91000, leave pin1 and 2 shorted.
2.5.2. Power supply
1. Remove R7 resistor
2. Connect a supply voltage (2.7V to 5.25V) between VDD test point and GND test point.
{'f TEXAS INSTRUMENTS
4 LMP91000EVM User’s Guide SNAU121-April 2012
2.5.3. Voltage reference
If the on board 2.5V voltage reference fits the requirements of the application, do not accomplish the
following steps.
1. Remove R6 resistor
2. Connect a reference voltage (1.5V to VDD) between VREF test point and GND test point.
2.5.4. I2C bus
The I2C bus requires two 10kohm pull-up resistors (R1, R2); the external microcontroller can be connected to the
SPIO-GPSI16 connector according to the following pin out:
SCL pin 12 of SPIO-GPSI16
SDA pin 11 of SPIO-GPSI16
GND pin 2 of SPIO-GPSI16
Refer to LMP91000’s datasheet for further details on I2C commands and registers.
The footprints of the pull-up resistors (R1, R2) are on the bottom side of the eval board.
2.5.5. Other
Remove the resistor R8 in order to disconnect the ADC’s input from LMP91000’s output.
{if TEXAS INSTRUMENTS o slam-595115 “ In ‘0 .4— : J; LMP9100059M6;6"T:
SNAU121-April 2012 LMP91000EVM User’s Guide 5
.
3. Board Layout
Figure 5, Figure 6 and Figure 7 show the board layout for the LMP91000EVM.
The EVM offers footprint for
- External JFET (Q1) to short RE and WE pin,
- Resistor (R3) and capacitor (C2) to apply external RTIA gain and filter
Figure 5: Top Layer Routing
Bill of Materials
6 LMP91000EVM User’s Guide SNAU121-April 2012
Figure 6: Bottom Layer Routing
" , 59, :8 ma $5.32 .5 .3? 2.. 23%: a... u... .565...- 28 3 .3 EEE 2. SEES 2. 5!, ass as... mass m: .53 .fl. .MEEEEE 2.55: 3 EEE n. 3 Bias. and; u... as, w: 35...... n $.53 a? is E. 5%.: Eva s 2.: 2. as... in? 3 .; SEES z. .gfinfiwwfifiésfisgg §)§E§.n22_s=§:e €835 Twas: 3 :58: 2.32.. a... a... "5.325%; s .3 EEE 2.... Efiasa 2. $2.2 5 mg, 52.5 is E a Sign is; a E 3%. an; a GEE-u. E is asasxfisg i. 2. ax... i3: 3 .5 ER: 2. ES. 2§Ssm58§ 3.332: ESE s§32§u§§fiizx€u§Bgfifizgisifié ‘5 TEXAS INSTRUMENTS
SNAU121-April 2012 LMP91000EVM User’s Guide 7
4. Schematic
Figure 7: LMP91000EVM Schematic
{'3 TEXAS INSTRUMENTS
Bill of Materials
8 LMP91000EVM User’s Guide SNAU121-April 2012
Table 3: LMP91000EVM Bill of Materials
COUNT
REF DES
DESCRIPTION
SIZE
MFR
PART NUMBER
1 2-wire
Header, TH, 100mil, 1x2, Gold
plated, 230 mil above insulator
0.100 x
2
Samtec Inc. TSW-102-07-G-S
12
3V3, 5V, SCL,
SDA, VDD,
TP_C1, TP_C2,
VOUT, CSB,
DOUT,SCLK,
VREF
Test Point, TH, Miniature, Red 40 mil Keystone
Electronics 5000
1 C1
CAP, CERM, 0.1uF, 10V, +/-
10%, X5R
402 MuRata
GRM155R61A104
KA01D
5
C5, C9, C11,
C13, C16
CAP, CERM, 0.1uF, 16V, +/-5%,
X7R
603 AVX 0603YC104JAT2A
1 C6
CAP, CERM, 56pF, 50V, +/-5%,
C0G/NP0
603 AVX 06035A560JAT2A
1 C7
CAP, TANT, 100uF, 10V, +/-
10%, 0.1 ohm
6032-28 AVX
TPSC107K010R01
00
1 C8
CAP, CERM, 470pF, 50V, +/-
5%, C0G/NP0
603 AVX 06035A471JAT2A
3 C10, C12, C14
CAP, TANT, 10uF, 16V, +/-10%,
0.45 ohm
6032-28
Vishay-
Sprague
593D106X9016C2
TE3
4
GND1, GND2,
GND3, GND4,
Test Point, TH, Miniature, Black 40 mil
Keystone
Electronics
5001
3
GAS_SENSOR
Gas sensor Hood
100mil
Cambion
450-3326-01-03-00
4 H1, H2, H3, H4
BUMPON HEMISPHERE .44X.20
BLACK
3M SJ-5003 (BLACK)
1 J_MENB
Header, TH, 100mil, 1x3, Gold
plated, 230 mil above insulator
0.100 x
3
Samtec Inc. TSW-103-07-G-S
2 R4, R8 RES, 20.0 ohm, 1%, 0.1W 603
Yageo
America
RC0603FR-
0720RL
2 R6, R7 RES, 0 ohm, 5%, 0.125W 805 Vishay-Dale
CRCW08050000Z0
EA
1 R10 RES, 27.4 ohm, 1%, 0.1W 603 Vishay-Dale CRCW060327R4F
KEA
1 SPIO-GPSI16 SPIO-GPSI16 Header, 8-Pin,
Dual row, Right Angle
0.100 x
8 dual
row
Sullins
Connector
Solutions PBC36DGAN
1 U1 LMP91000 LLP-14
Texas
Instruments
LMP91000SD
1 U2 IC ADC 16BIT 50-250KSPS
MSOP-
10
Texas
Instruments
ADC161S626CIM
M/NOPB
1 U3
Precision Micropower Low
Dropout Voltage Reference
SOT-23
Texas
Instruments
LM4120AIM5-2.5
1 U4 IC EEPROM 2KBIT 400KHZ TSSOP-
8
ON
Semiconductor
CAT24C01WI-GT3
*7, TEXAS INSTRUMENTS
SNAU121-April 2012 LMP91000EVM User’s Guide 9
www. .com/esh User Power/Frequency Use Obligations:
EVALUATION BOARD/KIT/MODULE (EVM) ADDITIONAL TERMS
Texas Instruments (TI) provides the enclosed Evaluation Board/Kit/Module (EVM) under the following conditions:
The user assumes all responsibility and liability for proper and safe handling of the goods. Further, the user
indemnifies TI from all claims arising from the handling or use of the goods.
Should this evaluation board/kit not meet the specifications indicated in the User’s Guide, the board/ kit may be
returned within 30 days from the date of delivery for a full refund. THE FOREGOING LIMITED WARRANTY IS THE
EXCLUSIVE WARRANTY MADE BY SELLER TO BUYER AND IS IN LIEU OF ALL OTHER WARRANTIES,
EXPRESSED, IMPLIED, OR STATUTORY, INCLUDING ANY WARRANTY OF MERCHANTABILITY OR FITNESS
FOR ANY PARTICULAR PURPOSE. EXCEPT TO THE EXTENT OF THE INDEMNITY SET FORTH ABOVE,
NEITHER PARTY SHALL BE LIABLE TO THE OTHER FOR ANY INDIRECT, SPECIAL, INCIDENTAL, OR
CONSEQUENTIAL DAMAGES.
Please read the User's Guide and, specifically, the Warnings and Restrictions notice in the User's Guide prior to
handling the product. This notice contains important safety information about temperatures and voltages. For
additional information on TI's environmental and/or safety programs, please visit www.ti.com/esh or contact TI.
No license is granted under any patent right or other intellectual property right of TI covering or relating to any
machine, process, or combination in which such TI products or services might be or are used. TI currently deals
with a variety of customers for products, and therefore our arrangement with the user is not exclusive. TI assumes
no liability for applications assistance, customer product design, software performance, or infringement of patents
or services described herein.
Mailing Address: Texas Instruments Post Office Box 655303 Dallas, Texas 75265
Copyright 2012, Texas Instruments Incorporated
REGULATORY COMPLIANCE INFORMATION
As noted in the EVM Users Guide and/or EVM itself, this EVM and/or accompanying hardware may or may not be
subject to the Federal Communications Commission (FCC) and Industry Canada (IC) rules.
For EVMs not subject to the above rules, this evaluation board/kit/module is intended for use for ENGINEERING
DEVELOPMENT, DEMONSTRATION OR EVALUATION PURPOSES ONLY and is not considered by TI to be a
finished end product fit for general consumer use. It generates, uses, and can radiate radio frequency energy and
has not been tested for compliance with the limits of computing devices pursuant to part 15 of FCC or ICES-003
rules, which are designed to provide reasonable protection against radio frequency interference. Operation of the
equipment may cause interference with radio communications, in which case the user at his own expense will be
required to take whatever measures may be required to correct this interference.
General Statement for EVMs including a radio
User Power/Frequency Use Obligations: This radio is intended for development/professional use only in legally
allocated frequency and power limits. Any use of radio frequencies and/or power availability of this EVM and its
development application(s) must comply with local laws governing radio spectrum allocation and power limits for
this evaluation module. It is the user’s sole responsibility to only operate this radio in legally acceptable frequency
space and within legally mandated power limitations. Any exceptions to this is strictly prohibited and unauthorized
by Texas Instruments unless user has obtained appropriate experimental/development licenses from local
regulatory authorities, which is responsibility of user including its acceptable authorization.
For EVMs annotated as FCC FEDERAL COMMUNICATIONS COMMISSION Part 15 Compliant
Caution
This device complies with part 15 of the FCC Rules. Operation is subject to the following two conditions: (1) This
device may not cause harmful interference, and (2) this device must accept any interference received, including
interference that may cause undesired operation.
Changes or modifications not expressly approved by the party responsible for compliance could void the user's
authority to operate the equipment.
FCC Interference Statement for Class A EVM devices
This equipment has been tested and found to comply with the limits for a Class A digital device, pursuant to part 15
of the FCC Rules. These limits are designed to provide reasonable protection against harmful interference when
the equipment is operated in a commercial environment. This equipment generates, uses, and can radiate radio
frequency energy and, if not installed and used in accordance with the instruction manual, may cause harmful
interference to radio communications. Operation of this equipment in a residential area is likely to cause harmful
interference in which case the user will be required to correct the interference at his own expense.
FCC Interference Statement for Class B EVM devices
This equipment has been tested and found to comply with the limits for a Class B digital device, pursuant to part 15
of the FCC Rules. These limits are designed to provide reasonable protection against harmful interference in a
residential installation. This equipment generates, uses and can radiate radio frequency energy and, if not installed
and used in accordance with the instructions, may cause harmful interference to radio communications. However,
there is no guarantee that interference will not occur in a particular installation. If this equipment does cause
harmful interference to radio or television reception, which can be determined by turning the equipment off and on,
the user is encouraged to try to correct the interference by one or more of the following measures:
Reorient or relocate the receiving antenna.
Increase the separation between the equipment and receiver.
Connect the equipment into an outlet on a circuit different from that to which the receiver is connected.
Consult the dealer or an experienced radio/TV technician for help.
For EVMs annotated as IC INDUSTRY CANADA Compliant
This Class A or B digital apparatus complies with Canadian ICES-003.
Changes or modifications not expressly approved by the party responsible for compliance could void the user’s
authority to operate the equipment.
Concerning EVMs including radio transmitters
This device complies with Industry Canada licence-exempt RSS standard(s). Operation is subject to the following
two conditions: (1) this device may not cause interference, and (2) this device must accept any interference,
including interference that may cause undesired operation of the device.
Concerning EVMs including detachable antennas
Under Industry Canada regulations, this radio transmitter may only operate using an antenna of a type and
maximum (or lesser) gain approved for the transmitter by Industry Canada. To reduce potential radio interference to
other users, the antenna type and its gain should be so chosen that the equivalent isotropically radiated power
(e.i.r.p.) is not more than that necessary for successful communication.
This radio transmitter has been approved by Industry Canada to operate with the antenna types listed in the user
guide with the maximum permissible gain and required antenna impedance for each antenna type indicated.
Antenna types not included in this list, having a gain greater than the maximum gain indicated for that type, are
strictly prohibited for use with this device.
~
Cet appareil numérique de la classe A ou B est conforme à la norme NMB-003 du Canada.
Les changements ou les modifications pas expressément approuvés par la partie responsable de la conformité ont
pu vider l’autorité de l'utilisateur pour actionner l'équipement.
Concernant les EVMs avec appareils radio
Le présent appareil est conforme aux CNR d'Industrie Canada applicables aux appareils radio exempts de licence.
L'exploitation est autorisée aux deux conditions suivantes : (1) l'appareil ne doit pas produire de brouillage, et (2)
l'utilisateur de l'appareil doit accepter tout brouillage radioélectrique subi, même si le brouillage est susceptible d'en
compromettre le fonctionnement.
Concernant les EVMs avec antennes détachables
Conformément à la réglementation d'Industrie Canada, le présent émetteur radio peut fonctionner avec une
antenne d'un type et d'un gain maximal (ou inférieur) approuvé pour l'émetteur par Industrie Canada. Dans le but
de réduire les risques de brouillage radioélectrique à l'intention des autres utilisateurs, il faut choisir le type
d'antenne et son gain de sorte que la puissance isotrope rayonnée équivalente (p.i.r.e.) ne dépasse pas l'intensité
nécessaire à l'établissement d'une communication satisfaisante.
Le présent émetteur radio a été approuvé par Industrie Canada pour fonctionner avec les types d'antenne
énumérés dans le manuel d’usage et ayant un gain admissible maximal et l'impédance requise pour chaque type
d'antenne. Les types d'antenne non inclus dans cette liste, ou dont le gain est supérieur au gain maximal indiqué,
sont strictement interdits pour l'exploitation de l'émetteur.
Important Notice for Users of this Product in Japan
This development kit is NOT certified as Confirming to Technical Regulations of Radio
Law of Japan!
If you use this product in Japan, you are required by Radio Law of Japan to follow the instructions below with
respect to this product:
(1) Use this product in a shielded room or any other test facility as defined in the notification #173 issued by
Ministry of Internal Affairs and Communications on March 28, 2006, based on Sub-section 1.1 of Article 6 of the
Ministry’s Rule for Enforcement of Radio Law of Japan,
(2) Use this product only after you obtained the license of Test Radio Station as provided in Radio Law of
Japan with respect to this product, or
(3) Use of this product only after you obtained the Technical Regulations Conformity Certification as
provided in Radio Law of Japan with respect to this product.
Also, please do not transfer this product, unless you give the same notice above to the transferee.
Please note that if you could not follow the instructions above, you will be subject to penalties of Radio Law of
Japan. Texas Instruments Japan Limited
(address) 24-1, Nishi-Shinjuku 6 chome, Shinjukku-ku, Tokyo, Japan
http://www.tij.co.jp
【ご使用にあたっての注意】
本開発キットは技術基準適合証明を受けておりません。
本製品のご使用に際しては、電波法遵守のため、以下のいずれかの措置を取っていただく必要がありますのでご注
意ください。
(1)電波法施行規則第6条第1項第1号に基づく平成18328日総務省告示第173号で定められた電波暗
室等の試験設備でご使用いただく。
(2)実験局の免許を取得後ご使用いただく。
(3)技術基準適合証明を取得後ご使用いただく
なお、本製品は、上記の「ご使用にあたっての注意」を譲渡先、移転先に通知しない限り、譲渡、移転できないも
のとします。
上記を遵守頂けない場合は、電波法の罰則が適用される可能性があることをご留意ください。
日本テキサス・インスツルメンツ株式会社
東京都新宿区西新宿6丁目24番1
西新宿三井ビル
http://www.tij.co.jp
EVALUATION BOARD/KIT/MODULE (EVM)
WARNINGS, RESTRICTIONS AND DISCLAIMERS
For Feasibility Evaluation Only, in Laboratory/Development Environments. Unless otherwise indicated, this
EVM is not a finished electrical equipment and not intended for consumer use. It is intended solely for use for
preliminary feasibility evaluation in laboratory/development environments by technically qualified electronics experts
who are familiar with the dangers and application risks associated with handling electrical mechanical components,
systems and subsystems. It should not be used as all or part of a finished end product.
Your Sole Responsibility and Risk. You acknowledge, represent and agree that:
1. You have unique knowledge concerning Federal, State and local regulatory requirements (including but not
limited to Food and Drug Administration regulations, if applicable) which relate to your products and which
relate to your use (and/or that of your employees, affiliates, contractors or designees) of the EVM for
evaluation, testing and other purposes.
2. You have full and exclusive responsibility to assure the safety and compliance of your products with all such
laws and other applicable regulatory requirements, and also to assure the safety of any activities to be
conducted by you and/or your employees, affiliates, contractors or designees, using the EVM. Further, you are
responsible to assure that any interfaces (electronic and/or mechanical) between the EVM and any human
body are designed with suitable isolation and means to safely limit accessible leakage currents to minimize the
risk of electrical shock hazard.
3. You will employ reasonable safeguards to ensure that your use of the EVM will not result in any property
damage, injury or death, even if the EVM should fail to perform as described or expected.
4. You will take care of proper disposal and recycling of the EVM’s electronic components and packing materials.
Certain Instructions. It is important to operate this EVM within TI’s recommended specifications and
environmental considerations per the user guidelines. Exceeding the specified EVM ratings (including but not
limited to input and output voltage, current, power, and environmental ranges) may cause property damage,
personal injury or death. If there are questions concerning these ratings please contact a TI field representative
prior to connecting interface electronics including input power and intended loads. Any loads applied outside of the
specified output range may result in unintended and/or inaccurate operation and/or possible permanent damage to
the EVM and/or interface electronics. Please consult the EVM User's Guide prior to connecting any load to the EVM
output. If there is uncertainty as to the load specification, please contact a TI field representative. During normal
operation, some circuit components may have case temperatures greater than 60oC as long as the input and output
are maintained at a normal ambient operating temperature. These components include but are not limited to linear
regulators, switching transistors, pass transistors, and current sense resistors which can be identified using the
EVM schematic located in the EVM User's Guide. When placing measurement probes near these devices during
normal operation, please be aware that these devices may be very warm to the touch. As with all electronic
evaluation tools, only qualified personnel knowledgeable in electronic measurement and diagnostics normally found
in development environments should use these EVMs.
Agreement to Defend, Indemnify and Hold Harmless. You agree to defend, indemnify and hold TI, its licensors
and their representatives harmless from and against any and all claims, damages, losses, expenses, costs and
liabilities (collectively, "Claims") arising out of or in connection with any use of the EVM that is not in accordance
with the terms of the agreement. This obligation shall apply whether Claims arise under law of tort or contract or
any other legal theory, and even if the EVM fails to perform as described or expected.
Safety-Critical or Life-Critical Applications. If you intend to evaluate the components for possible use in safety
critical applications (such as life support) where a failure of the TI product would reasonably be expected to cause
severe personal injury or death, such as devices which are classified as FDA Class III or similar classification, then
you must specifically notify TI of such intent and enter into a separate Assurance and Indemnity Agreement.
amglmer “Lam dataconvener,u.com dsgimom mterlacet om \ogwc. U cum gower '.com microcomro‘lem com www rhd com www.u.com/Igw www ti com/aud‘o om/aummuuve wwwl om/oghca‘network wwwlw Lam/security www.ll.com/le\eghuny om/vwdeo
IMPORTANT NOTICE
Texas Instruments Incorporated and its subsidiaries (TI) reserve the right to make corrections, modifications,
enhancements, improvements, and other changes to its products and services at any time and to discontinue any
product or service without notice. Customers should obtain the latest relevant information before placing orders and
should verify that such information is current and complete. All products are sold subject to TI’s terms and conditions
of sale supplied at the time of order acknowledgment.
TI warrants performance of its hardware products to the specifications applicable at the time of sale in accordance
with TI’s standard warranty. Testing and other quality control techniques are used to the extent TI deems necessary
to support this warranty. Except where mandated by government requirements, testing of all parameters of each
product is not necessarily performed.
TI assumes no liability for applications assistance or customer product design. Customers are responsible for their
products and applications using TI components. To minimize the risks associated with customer products and
applications, customers should provide adequate design and operating safeguards.
TI does not warrant or represent that any license, either express or implied, is granted under any TI patent right,
copyright, mask work right, or other TI intellectual property right relating to any combination, machine, or process in
which TI products or services are used. Information published by TI regarding third-party products or services does
not constitute a license from TI to use such products or services or a warranty or endorsement thereof. Use of such
information may require a license from a third party under the patents or other intellectual property of the third party,
or a license from TI under the patents or other intellectual property of TI. Reproduction of information in TI data
books or data sheets is permissible only if reproduction is without alteration and is accompanied by all associated
warranties, conditions, limitations, and notices.
Reproduction of this information with alteration is an unfair and deceptive business practice. TI is not responsible or
liable for such altered documentation. Resale of TI products or services with statements different from or beyond the
parameters stated by TI for that product or service voids all express and any implied warranties for the associated TI
product or service and is an unfair and deceptive business practice. TI is not responsible or liable for any such
statements.
TI products are not authorized for use in safety-critical applications (such as life support) where a failure of the TI
product would reasonably be expected to cause severe personal injury or death, unless officers of the parties have
executed an agreement specifically governing such use. Buyers represent that they have all necessary expertise in
the safety and regulatory ramifications of their applications, and acknowledge and agree that they are solely
responsible for all legal, regulatory and safety-related requirements concerning their products and any use of TI
products in such safety-critical applications, notwithstanding any applications-related information or support that may
be provided by TI. Further, Buyers must fully indemnify TI and its representatives against any damages arising out of
the use of TI products in such safety-critical applications.
TI products are neither designed nor intended for use in military/aerospace applications or environments unless the
TI products are specifically designated by TI as military-grade or "enhanced plastic." Only products designated by TI
as military-grade meet military specifications. Buyers acknowledge and agree that any such use of TI products which
TI has not designated as military-grade is solely at the Buyer's risk, and that they are solely responsible for
compliance with all legal and regulatory requirements in connection with such use.
TI products are neither designed nor intended for use in automotive applications or environments unless the specific
TI products are designated by TI as compliant with ISO/TS 16949 requirements. Buyers acknowledge and agree
that, if they use any non-designated products in automotive applications, TI will not be responsible for any failure to
meet such requirements.
Following are URLs where you can obtain information on other Texas Instruments products and application
solutions:
Products Applications
Amplifiers amplifier.ti.com Audio www.ti.com/audio
Data Converters dataconverter.ti.com Automotive www.ti.com/automotive
DSP dsp.ti.com Broadband www.ti.com/broadband
Interface interface.ti.com Digital Control www.ti.com/digitalcontrol
Logic logic.ti.com Military www.ti.com/military
Power Mgmt power.ti.com Optical Networking www.ti.com/opticalnetwork
Microcontrollers microcontroller.ti.com Security www.ti.com/security
RFID www.ti-rfid.com Telephony www.ti.com/telephony
Low Power www.ti.com/lpw Video & Imaging www.ti.com/video
Wireless Wireless www.ti.com/wireless
Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265
Copyright © 2007, Texas Instruments Incorporated

Products related to this Datasheet

EVAL BOARD FOR LMP91000