PIC18F1230,1330 Programming Spec Datasheet by Microchip Technology
View All Related Products | Download PDF Datasheet
Q
‘MICFIOCHIP PIC18F1230/1330
© 2009 Microchip Technology Inc. DS39752B-page 1
PIC18F1230/1330
1.0 DEVICE OVERVIEW
This document includes the programming specifications
for the following devices:
2.0 PROGRAMMING OVERVIEW
PIC18F1230/1330 devices can be programmed using
the high-voltage In-Circuit Serial Programming™
(ICSP™) method. This method can be done with the
device in the user’s system. This programming
specification applies to PIC18F1230/1330 devices in
all package types.
2.1 Hardware Requirements
In High-Voltage ICSP mode, PIC18F1230/1330
devices require two programmable power supplies:
one for VDD and one for MCLR/VPP/RA5/FLTA. Both
supplies should have a minimum resolution of 0.25V.
Refer to Section 6.0 “AC/DC Characteristics Timing
Requirements for Program/Verify Test Mode” for
additional hardware parameters.
2.2 Pin Diagrams
The pin diagrams for the PIC18F1230/1330 family are
shown in Figure 2-1, Figure 2-2 and Figure 2-3.
TABLE 2-1: PIN DESCRIPTIONS (DURING PROGRAMMING): PIC18F1230/1330
• PIC18F1230 • PIC18F1330
• PIC18F1330-ICD
Pin Name During Programming
Pin Name Pin Type Pin Description
MCLR/VPP/RA5/FLTA VPP P Programming Enable
VDD(1) VDD P Power Supply
VSS(1) VSS P Ground
RB6 PGC I Serial Clock
RB7 PGD I/O Serial Data
Legend: I = Input, O = Output, P = Power
Note 1: All power supply (VDD) and ground (VSS) pins must be connected.
Flash Microcontroller Programming Specification
PIC18F1230/1330
DS39752B-page 2 © 2009 Microchip Technology Inc.
FIGURE 2-1: PIC18F1230/1330 FAMILY PIN DIAGRAMS
18-Pin PDIP, SOIC
2
3
4
5
6
1
8
7
9
RA0/AN0/INT0/KBI0/CMP0
RA1/AN1/INT1/KBI1
RA4/T0CKI/AN2/VREF+
VSS/AVSS
RA2/TX/CK
RA3/RX/DT
RB0/PWM0
RB1/PWM1
PIC18F1X30
17
16
15
14
13
18
11
12
10
RB3/INT3/KBI3/CMP1/T1OSI(1)
RB2/INT2/KBI2/CMP2/T1OSO(1)
RA7/OSC1/CLKI/T1OSI(1)/FLTA(2)
RA6/OSC2/CLKO/T1OSO(1)/AN3
VDD/AVDD
RB7/PWM5/PGD
RB6/PWM4/PGC
RB5/PWM3
RB4/PWM2
20-Pin SSOP
2
3
4
5
6
1
8
7
9
RA0/AN0/INT0/KBI0/CMP0
RA1/AN1/INT1/KBI1
RA4/T0CKI/AN2/VREF+
MCLR/VPP/RA5/FLTA(2)
VSS
RA2/TX/CK
RA3/RX/DT
RB0/PWM0
RB1/PWM1
PIC18F1X30
17
16
15
14
13
18
11
12
10
RB3/INT3/KBI3/CMP1/T1OSI(1)
RB2/INT2/KBI2/CMP2/T1OSO(1)
RA7/OSC1/CLKI/T1OSI(1)/FLTA(2)
RA6/OSC2/CLKO/T1OSO(1)/AN3
RB7/PWM5/PGD
RB5/PWM3
RB4/PWM2
AVSS
RB6/PWM4/PGC
Note 1: Placement of T1OSI and T1OSO depends on the value of the Configuration bit, T1OSCMX of CONFIG3H.
2: Placement of FLTA depends on the value of the Configuration bit, FLTAMX of CONFIG3H.
20
19
VDD
AVDD
MCLR/VPP/RA5/FLTA(2)
uf.
ufv
ufv
ufv
ufv
ufv
ufv
© 2009 Microchip Technology Inc. DS39752B-page 3
PIC18F1230/1330
FIGURE 2-2: PIC18F1230/1330 FAMILY PIN DIAGRAMS
28-Pin QFN
PIC18F1X30
RA3/RX/DT
2
3
4
5
6
1
NC
VSS
NC
AVSS
NC
RA2/TX/CK 7
9
10
11
12
13
8
14
RB0/PWM0
RB1/PWM1
NC(2)
RB4/PWM2
RB5/PWM3
NC(2)
RA0/AN0/INT0/KBI0/CMP0
NC
RB3/INT3/KBI3/CMP1/T1OSI(1)
RB2/INT2/KBI2/CMP2/T1OSO(1)
NC
RA1/AN1/INT1/KBI1
27
25
24
23
28
22
26
RA7/OSC1/CLKI/T1OSI(1)/FLTA(3)
RA6/OSC2/CLKO/T1OSO(1)/AN3
VDD
NC
AVDD
RB7/PWM5/PGD
RB6/PWM4/PGC
20
19
18
17
16
21
15
Note 1: Placement of T1OSI and T1OSO depends on the value of the Configuration bit, T1OSCMX of CONFIG3H.
2: Pin feature is dependent on device configuration.
3: Placement of FLTA depends on the value of the Configuration bit, FLTAMX of CONFIG3H.
RA4/T0CKI/AN2/VREF+
MCLR/VPP/RA5/FLTA(3)

PIC18F1230/1330
DS39752B-page 4 © 2009 Microchip Technology Inc.
FIGURE 2-3: PIC18F1330-ICD DEVICE PIN DIAGRAM
28-Pin QFN
PIC18F1330-ICD
RA3/RX/DT
2
3
4
5
6
1
ICRST(2)/ICVPP(2)
VSS
NC
AVSS
NC
RA2/TX/CK 7
9
10
11
12
13
8
14
RB0/PWM0
RB1/PWM1
ICCK(2)/ICPGC(2)
RB4/PWM2
RB5/PWM3
ICDT(2)/ICPGD(2)
RA0/AN0/INT0/KBI0/CMP0
NC
RB3/INT3/KBI3/CMP1/T1OSI(1)
RB2/INT2/KBI2/CMP2/T1OSO(1)
NC
RA1/AN1/INT1/KBI1
27
25
24
23
28
22
26
RA7/OSC1/CLKI/T1OSI(1)/FLTA(3)
RA6/OSC2/CLKO/T1OSO(1)/AN3
VDD
NC
AVDD
RB7/PWM5/PGD
RB6/PWM4/PGC
20
19
18
17
16
21
15
Note 1: Placement of T1OSI and T1OSO depends on the value of the Configuration bit, T1OSCMX of CONFIG3H.
2: Pin feature is dependent on device configuration.
3: Placement of FLTA depends on the value of the Configuration bit, FLTAMX of CONFIG3H.
RA4/T0CKI/AN2/VREF+
MCLR/VPP/RA5/FLTA(3)
© 2009 Microchip Technology Inc. DS39752B-page 5
PIC18F1230/1330
2.3 Memory Maps
For the PIC18F1330 device, the code memory
space extends from 00000h to 01FFFh (8 Kbytes) in
two 4-Kbyte blocks. For the PIC18F1230 device, the
code memory space extends from 00000h to 00FFFh
(4 Kbytes) in two 2-Kbyte blocks. Addresses 00000h
through 07FFh, however, define a “Boot Block” region
that is treated separately from Block 0. All of these
blocks define code protection boundaries within the
code memory space.
The size of the Boot Block in PIC18F1230/1330
devices can be configured as 256, 512 or 1K words.
This is done through the BBSIZ<1:0> bits in the
Configuration register, CONFIG4L (see Table 5-1). It is
important to note that increasing the size of the Boot
Block decreases the size of Block 0.
TABLE 2-2: IMPLEMENTATION OF CODE
MEMORY
FIGURE 2-4: MEMORY MAP AND CODE MEMORY SPACE FOR THE PIC18F1230 DEVICE
Device Code Memory Size (Bytes)
PIC18F1230 00000h-00FFFh (4K)
PIC18F1330 00000h-01FFFh (8K)
000000h
01FFFFh
3FFFFFh
Note: Sizes of memory areas are not to scale.
* Boot Block size is determined by the BBSIZ<1:0> bits in CONFIG4L.
Code Memory
Unimplemented
Read as ‘0’
Configuration
and ID
Space
MEMORY SIZE/DEVICE
4Kbytes
(PIC18F1230) Address
Range
Boot Block 000000h
0001FFh* or 0003FFh*
Block 0 000200h* or 000400h
0007FFh
Block 1
000800h
000FFFh
Unimplemented
Read ‘0’s
001000h
01FFFFh
200000h

PIC18F1230/1330
DS39752B-page 6 © 2009 Microchip Technology Inc.
FIGURE 2-5: MEMORY MAP AND CODE MEMORY SPACE FOR THE PIC18F1330 DEVICE
000000h
01FFFFh
3FFFFFh
Note: Sizes of memory areas are not to scale.
* Boot Block size is determined by the BBSIZ<1:0> bits in CONFIG4L.
Code Memory
Unimplemented
Read as ‘0’
Configuration
and ID
Space
MEMORY SIZE/DEVICE
8Kbytes
(PIC18F1330) Address
Range
Boot Block 000000h
0001FFh* or 0003FFh* or 0007FFh*
Block 0 000200h* or 000400h or 000800h
000FFFh
Block 1
001000h
001FFFh
Unimplemented
Read ‘0’s
01FFFFh
200000h

© 2009 Microchip Technology Inc. DS39752B-page 7
PIC18F1230/1330
In addition to the code memory space, there are three
blocks in the Configuration and ID space that are
accessible to the user through table reads and table
writes. Their locations in the memory map are shown in
Figure 2-6.
Users may store identification information (ID) in eight ID
registers. These ID registers are mapped in addresses,
200000h through 200007h. The ID locations read out
normally, even after code protection is applied.
Locations 300000h through 30000Dh are reserved for
the Configuration bits. These bits select various device
options and are described in Section 5.0 “Configura-
tion Word”. These Configuration bits read out normally,
even after code protection.
Locations 3FFFFEh and 3FFFFFh are reserved for the
Device ID bits. These bits may be used by the program-
mer to identify what device type is being programmed
and are described in Section 5.0 “Configuration
Word”. These Device ID bits read out normally, even
after code protection.
2.3.1 MEMORY ADDRESS POINTER
Memory in the address space, 0000000h to 3FFFFFh,
is addressed via the Table Pointer register, which is
comprised of three pointer registers:
• TBLPTRU at RAM address 0FF8h
• TBLPTRH at RAM address 0FF7h
• TBLPTRL at RAM address 0FF6h
The 4-bit command, ‘0000’ (core instruction), is used to
load the Table Pointer prior to using many read or write
operations.
FIGURE 2-6: CONFIGURATION AND ID LOCATIONS FOR THE PIC18F1230/1330 DEVICES
TBLPTRU TBLPTRH TBLPTRL
Addr[21:16] Addr[15:8] Addr[7:0]
ID Location 1 200000h
ID Location 2 200001h
ID Location 3 200002h
ID Location 4 200003h
ID Location 5 200004h
ID Location 6 200005h
ID Location 7 200006h
ID Location 8 200007h
CONFIG1L 300000h
CONFIG1H 300001h
CONFIG2L 300002h
CONFIG2H 300003h
CONFIG3L 300004h
CONFIG3H 300005h
CONFIG4L 300006h
CONFIG4H 300007h
CONFIG5L 300008h
CONFIG5H 300009h
CONFIG6L 30000Ah
CONFIG6H 30000Bh
CONFIG7L 30000Ch
CONFIG7H 30000Dh
Device ID 1 3FFFFEh
Device ID 2 3FFFFFh
Note: Sizes of memory areas are not to scale.
000000h
1FFFFFh
3FFFFFh
01FFFFh Code Memory
Unimplemented
Read as ‘0’
Configuration
and ID
Space
2FFFFFh
PIC18F1230/1330
DS39752B-page 8 © 2009 Microchip Technology Inc.
2.4 High-Level Overview of the
Programming Process
Figure 2-7 shows the high-level overview of the
programming process. First, a Bulk Erase is performed.
Next, the code memory, ID locations and data
EEPROM are programmed (see Section 3.3 “Data
EEPROM Programming”). These memories are then
verified to ensure that programming was successful. If
no errors are detected, the Configuration bits are then
programmed and verified.
FIGURE 2-7: HIGH-LEVEL
PROGRAMMING FLOW
2.5 Entering and Exiting High-Voltage
ICSP Program/Verify Mode
As shown in Figure 2-8, the High-Voltage ICSP
Program/Verify mode is entered by holding PGC and
PGD low, and then raising MCLR/VPP/RA5/FLTA to
VIHH (high voltage). Once in this mode, the code mem-
ory, data EEPROM (see Section 3.3 “Data EEPROM
Programming”), ID locations and Configuration bits
can be accessed and programmed in serial fashion.
Figure 2-9 shows the exit sequence.
The sequence that enters the device into the Program/
Verify mode places all unused I/Os in the high-impedance
state.
FIGURE 2-8: ENTERING HIGH-VOLTAGE
PROGRAM/VERIFY MODE
FIGURE 2-9: EXITING HIGH-VOLTAGE
PROGRAM/VERIFY MODE
Start
Program Memory
Program IDs
Program Data EE
Verify Program
Verify IDs
Verify Data
Program
Configuration Bits
Verify
Configuration Bits
Done
Perform Bulk
Erase
P12
PGD
PGD = Input
VDD
D110
P13
P1
PGC
MCLR/VPP/
RA5/FLTA
MCLR/VPP/
P16
PGD
PGD = Input
PGC
VDD
D110
P17
P1
RA5/FLTA
© 2009 Microchip Technology Inc. DS39752B-page 9
PIC18F1230/1330
2.6 Serial Program/Verify Operation
The PGC pin is used as a clock input pin and the PGD
pin is used for entering command bits and data input/
output during serial operation. Commands and data are
transmitted on the rising edge of PGC, latched on the
falling edge of PGC and are Least Significant bit (LSb)
first.
2.6.1 4-BIT COMMANDS
All instructions are 20 bits, consisting of a leading 4-bit
command, followed by a 16-bit operand which depends
on the type of command being executed. To input a
command, PGC is cycled four times. The commands
needed for programming and verification are shown in
Table 2-3.
Depending on the 4-bit command, the 16-bit operand
represents 16 bits of input data, or 8 bits of input data
and 8 bits of output data.
Throughout this specification, commands and data are
presented as illustrated in Table 2-4. The 4-bit command
is shown Most Significant bit (MSb) first. The command
operand, or “Data Payload”, is shown <MSB><LSB>.
Figure 2-10 demonstrates how to serially present a
20-bit command/operand to the device.
2.6.2 CORE INSTRUCTION
The core instruction passes a 16-bit instruction to the
CPU core for execution. This is needed to set up
registers as appropriate for use with other commands.
TABLE 2-3: COMMANDS FOR
PROGRAMMING
TABLE 2-4: SAMPLE COMMAND
SEQUENCE
FIGURE 2-10: TABLE WRITE, POST-INCREMENT TIMING (1101)
Description 4-Bit
Command
Core Instruction
(shift in16-bit instruction)
0000
Shift out TABLAT Register 0010
Table Read 1000
Table Read, Post-Increment 1001
Table Read, Post-Decrement 1010
Table Read, Pre-Increment 1011
Table Write 1100
Table Write, Post-Increment by 2 1101
Table Write, Start Programming,
Post-Increment by 2
1110
Table Write, Start Programming 1111
4-Bit
Command Data
Payload Core Instruction
1101 3C 40 Table Write,
post-increment by 2
1234
P5
PGD = Input
5678 1234
P5A
910 11 13 15 161412
Fetch Next 4-Bit Command
1011
1234
nnnn
P3
P2 P2A
000000 010001111 0
04C3
P4
4-Bit Command 16-Bit Data Payload
P2B
PGC
PGD

PIC18F1230/1330
DS39752B-page 10 © 2009 Microchip Technology Inc.
2.7 28-Pin PIC18F1330-ICD Device
(Dedicated ICD Port)
The PIC18F1330-ICD 28-pin QFN device has a
dedicated ICSP/ICD port. The primary purpose of this
port is to provide an alternate In-Circuit Debugging
(ICD) option and free the pins (RB6, RB7 and MCLR)
that would normally be used for debugging the applica-
tion. In conjunction with ICD capability, however, the
dedicated ICSP/ICD port also provides an alternate
port for ICSP.
The dedicated ICSP/ICD port functions the same as
the default ICSP/ICD port; however, alternate pins are
used instead of the default pins. Table 2-5 identifies the
functionally equivalent pins for ICSP purposes.
The dedicated ICSP/ICD port is an alternate port. Thus,
ICSP is still available through the default port. When
the VIH is seen on the MCLR/VPP/RA5/FLTA pin prior to
applying VIH to the ICRST/ICVPP pin, then the state of
the ICRST/ICVPP pin is ignored. Likewise, when the
VIH is seen on ICRST/ICVPP prior to applying VIH to
MCLR/VPP/RA5/FLTA, then the state of the MCLR/VPP/
RA5/FLTA pin is ignored.
TABLE 2-5: ICSP™ EQUIVALENT PINS
Pin Name During Programming
Pin Name Pin Type Dedicated Pin Pin Description
MCLR/VPP/RA5/FLTA VPP P ICRST/ICVPP Programming Enable
RB6 PGC I ICCK/ICPGC Serial Clock
RB7 PGD I/O ICDT/ICPGD Serial Data
Legend: I = Input, O = Output, P = Power
© 2009 Microchip Technology Inc. DS39752B-page 11
PIC18F1230/1330
3.0 DEVICE PROGRAMMING
Programming includes the ability to erase or write the
various memory regions within the device.
In all cases, except high-voltage ICSP Bulk Erase, the
EECON1 register must be configured in order to
operate on a particular memory region.
When using the EECON1 register to act on code
memory, the EEPGD bit must be set (EECON1<7> = 1)
and the CFGS bit must be cleared (EECON1<6> = 0).
The WREN bit must be set (EECON1<2> = 1) to
enable writes of any sort (e.g., erases) and this must be
done prior to initiating a write sequence. The FREE bit
must be set (EECON1<4> = 1) in order to erase the
program space being pointed to by the Table Pointer.
The erase or write sequence is initiated by setting the
WR bit (EECON1<1> = 1). It is strongly recommended
that the WREN bit only be set immediately prior to a
program erase.
3.1 ICSP Erase
3.1.1 HIGH-VOLTAGE ICSP BULK ERASE
Erasing code or data EEPROM is accomplished by
configuring two Bulk Erase Control registers located at
3C0004h and 3C0005h. Code memory may be erased
portions at a time, or the user may erase the entire
device in one action. Bulk Erase operations will also
clear any code-protect settings associated with the
memory block erased. Erase options are detailed in
Table 3-1. If data EEPROM is code-protected
(CPD = 0), the user must request an erase of data
EEPROM (e.g., 0084h as shown in Table 3-1).
TABLE 3-1: BULK ERASE OPTIONS
The actual Bulk Erase function is a self-timed
operation. Once the erase has started (falling edge of
the 4th PGC after the NOP command), serial execution
will cease until the erase completes (parameter P11).
During this time, PGC may continue to toggle but PGD
must be held low.
The code sequence to erase the entire device is shown
in Table 3-2 and the flowchart is shown in Figure 3-1.
TABLE 3-2: BULK ERASE COMMAND
SEQUENCE
FIGURE 3-1: BULK ERASE FLOW
Description Data
(3C0005h:3C0004h)
Chip Erase 0F87h
Erase Data EEPROM(1) 0084h
Erase Boot Block 0081h
Erase Configuration Bits 0082h
Erase Code EEPROM Block 0 0180h
Erase Code EEPROM Block 1 0280h
Erase Code EEPROM Block 2 0480h
Erase Code EEPROM Block 3 0880h
Note 1: Selected devices only, see Section 3.3
“Data EEPROM Programming”.
Note: A Bulk Erase is the only way to reprogram
code-protect bits from an ON state to an
OFF state.
4-Bit
Command Data
Payload Core Instruction
0000
0000
0000
0000
0000
0000
1100
0000
0000
0000
0000
0000
0000
1100
0000
0000
0E 3C
6E F8
0E 00
6E F7
0E 05
6E F6
0F 0F
0E 3C
6E F8
0E 00
6E F7
0E 04
6E F6
87 87
00 00
00 00
MOVLW 3Ch
MOVWF TBLPTRU
MOVLW 00h
MOVWF TBLPTRH
MOVLW 05h
MOVWF TBLPTRL
Write 0Fh to 3C0005h
MOVLW 3Ch
MOVWF TBLPTRU
MOVLW 00h
MOVWF TBLPTRH
MOVLW 04h
MOVWF TBLPTRL
Write 8787h to 3C0004h
to erase entire
device.
NOP
Hold PGD low until
erase completes.
Start
Done
Write 8787h to
3C0004h to Erase
Entire Device
Write 0F0Fh
Delay P11 + P10
Time
to 3C0005h

PIC18F1230/1330
DS39752B-page 12 © 2009 Microchip Technology Inc.
FIGURE 3-2: BULK ERASE TIMING
3.1.2 ICSP ROW ERASE
For a PIC18F1230/1330 device, it is possible to erase
one row (64 bytes of data), provided the block is not
code or write-protected. Rows are located at static
boundaries, beginning at program memory address
000000h, extending to the internal program memory
limit (see Section 2.3 “Memory Maps”).
The Row Erase duration is externally timed and is
controlled by PGC. After the WR bit in EECON1 is set,
a NOP is issued, where the 4th PGC is held high for the
duration of the programming time, P9.
After PGC is brought low, the programming sequence
is terminated. PGC must be held low for the time
specified by parameter P10 to allow high-voltage
discharge of the memory array.
The code sequence to Row Erase a PIC18F1230/1330
device is shown in Table 3-3. The flowchart shown in
Figure 3-3 depicts the logic necessary to completely
erase a PIC18F1230/1330 device. The timing diagram
that details the Start Programming command and
parameters P9 and P10 is shown in Figure 3-5.
n
1234 121516 123
PGC
P5 P5A
PGD
PGD = Input
00011
P11
P10
Erase Time
000000
12
00
4
0
12 1516
P5
123
P5A
4
0000
n
4-Bit Command 4-Bit Command 4-Bit Command16-Bit
Data Payload
16-Bit
Data Payload 16-Bit
Data Payload
11
Note: The TBLPTR register can point to any byte
within the row intended for erase.

© 2009 Microchip Technology Inc. DS39752B-page 13
PIC18F1230/1330
TABLE 3-3: ERASE CODE MEMORY CODE SEQUENCE
FIGURE 3-3: SINGLE ROW ERASE CODE MEMORY FLOW
4-Bit
Command Data Payload Core Instruction
Step 1: Direct access to code memory and enable writes.
0000
0000
0000
8E A6
9C A6
84 A6
BSF EECON1, EEPGD
BCF EECON1, CFGS
BSF EECON1, WREN
Step 2: Point to first row in code memory.
0000
0000
0000
6A F8
6A F7
6A F6
CLRF TBLPTRU
CLRF TBLPTRH
CLRF TBLPTRL
Step 3: Enable erase and erase single row.
0000
0000
0000
88 A6
82 A6
00 00
BSF EECON1, FREE
BSF EECON1, WR
NOP – hold PGC high for time P9 and low for time P10.
Step 4: Repeat step 3, with Address Pointer incremented by 64 until all rows are erased.
Done
Start
Hold PGC Low
for Time P10
All
rows
done?
No
Yes
Addr = 0
Configure
Device for
Row Erases
Addr = Addr + 64
Start Erase Sequence
and Hold PGC High
for Time P9
PIC18F1230/1330
DS39752B-page 14 © 2009 Microchip Technology Inc.
3.2 Code Memory Programming
Programming code memory is accomplished by first
loading data into the write buffer and then initiating a
programming sequence. The write and erase buffer
sizes, shown in Table 3-4, can be mapped to any
location of the same size, beginning at 000000h. The
actual memory write sequence takes the contents of
this buffer and programs the proper amount of code
memory that contains the Table Pointer.
The programming duration is externally timed and is
controlled by PGC. After a Start Programming
command is issued (4-bit command, ‘1111’), a NOP is
issued, where the 4th PGC is held high for the duration
of the programming time, P9.
After PGC is brought low, the programming sequence
is terminated. PGC must be held low for the time
specified by parameter P10 to allow high-voltage
discharge of the memory array.
The code sequence to program a PIC18F1230/1330
device is shown in Table 3-5. The flowchart, shown in
Figure 3-4, depicts the logic necessary to completely
write a PIC18F1230/1330 device. The timing diagram
that details the Start Programming command and
parameters P9 and P10 is shown in Figure 3-5.
TABLE 3-4: WRITE AND ERASE BUFFER
SIZES
TABLE 3-5: WRITE CODE MEMORY CODE SEQUENCE
Note: The TBLPTR register must point to the
same region when initiating the program-
ming sequence as it did when the write
buffers were loaded.
Device Write Buffer
Size (bytes) Erase Buffer
Size (bytes)
PIC18F1230 864
PIC18F1330
4-Bit
Command Data Payload Core Instruction
Step 1: Direct access to code memory and enable writes.
0000
0000
8E A6
9C A6
BSF EECON1, EEPGD
BCF EECON1, CFGS
Step 2: Load write buffer.
0000
0000
0000
0000
0000
0000
0E <Addr[21:16]>
6E F8
0E <Addr[15:8]>
6E F7
0E <Addr[7:0]>
6E F6
MOVLW <Addr[21:16]>
MOVWF TBLPTRU
MOVLW <Addr[15:8]>
MOVWF TBLPTRH
MOVLW <Addr[7:0]>
MOVWF TBLPTRL
Step 3: Repeat for all but the last two bytes.
1101 <MSB><LSB> Write 2 bytes and post-increment address by 2.
Step 4: Load write buffer for the last two bytes.
1111
0000
<MSB><LSB>
00 00
Write 2 bytes and start programming.
NOP - hold PGC high for time P9 and low for time P10.
To continue writing data, repeat steps 2 through 4, where the Address Pointer is incremented by 2 at each iteration of the loop.
M U
W; H fllHlfl H H fi§wfl H H
fl; gV—‘g %#fl—’ W
© 2009 Microchip Technology Inc. DS39752B-page 15
PIC18F1230/1330
FIGURE 3-4: PROGRAM CODE MEMORY FLOW
FIGURE 3-5: TABLE WRITE AND START PROGRAMMING INSTRUCTION TIMING (1111)
Start Write Sequence
All
locations
done?
No
Done
Start
Yes
Hold PGC Low
for Time P10
Load 2 Bytes
to Write
Buffer at <Addr>
All
bytes
written?
No
Yes
and Hold PGC
High until Done
N = 1
LoopCount = 0
Configure
Device for
Writes
N = 1
LoopCount =
LoopCount + 1
N = N + 1
and Wait P9
1234 12 1516 123 4
PGC
P5A
PGD
PGD = Input
n
1111
34 65
P9
P10
Programming Time
nnn nn n n
00
12
0
00
16-Bit
Data Payload
0
3
0
P5
4-Bit Command 16-Bit Data Payload 4-Bit Command

PIC18F1230/1330
DS39752B-page 16 © 2009 Microchip Technology Inc.
3.2.1 MODIFYING CODE MEMORY
The previous programming example assumed that the
device had been Bulk Erased prior to programming
(see Section 3.1.1 “High-Voltage ICSP Bulk Erase”).
It may be the case, however, that the user wishes to
modify only a section of an already programmed
device.
The appropriate number of bytes required for the erase
buffer must be read out of code memory (as described
in Section 4.2 “Verify Code Memory and ID Loca-
tions”) and buffered. Modifications can be made on this
buffer. Then, the block of code memory that was read
out must be erased and rewritten with the modified data.
The WREN bit must be set if the WR bit in EECON1 is
used to initiate a write sequence.
TABLE 3-6: MODIFYING CODE MEMORY
4-Bit
Command Data Payload Core Instruction
Step 1: Direct access to code memory.
Step 2: Read and modify code memory (see Section 4.1 “Read Code Memory, ID Locations and Configuration Bits”).
0000
0000
8E A6
9C A6
BSF EECON1, EEPGD
BCF EECON1, CFGS
Step 3: Set the Table Pointer for the block to be erased.
0000
0000
0000
0000
0000
0000
0E <Addr[21:16]>
6E F8
0E <Addr[8:15]>
6E F7
0E <Addr[7:0]>
6E F6
MOVLW <Addr[21:16]>
MOVWF TBLPTRU
MOVLW <Addr[8:15]>
MOVWF TBLPTRH
MOVLW <Addr[7:0]>
MOVWF TBLPTRL
Step 4: Enable memory writes and set up an erase.
0000
0000
84 A6
88 A6
BSF EECON1, WREN
BSF EECON1, FREE
Step 5: Initiate erase.
0000
0000
82 A6
00 00
BSF EECON1, WR
NOP - hold PGC high for time P9 and low for time P10.
Step 6: Load write buffer. The correct bytes will be selected based on the Table Pointer.
0000
0000
0000
0000
0000
0000
1101
.
.
.
1111
0000
0E <Addr[21:16]>
6E F8
0E <Addr[8:15]>
6E F7
0E <Addr[7:0]>
6E F6
<MSB><LSB>
.
.
.
<MSB><LSB>
00 00
MOVLW <Addr[21:16]>
MOVWF TBLPTRU
MOVLW <Addr[8:15]>
MOVWF TBLPTRH
MOVLW <Addr[7:0]>
MOVWF TBLPTRL
Write 2 bytes and post-increment address by 2.
Repeat as many times as necessary to fill the write buffer
Write 2 bytes and start programming.
NOP - hold PGC high for time P9 and low for time P10.
To continue modifying data, repeat Steps 2 through 6, where the Address Pointer is incremented by the appropriate number of bytes
(see Table 3-4) at each iteration of the loop. The write cycle must be repeated enough times to completely rewrite the contents of
the erase buffer.
Step 7: Disable writes.
0000 94 A6 BCF EECON1, WREN
mm mm j m
WHWWHWHWWH; 5h
m w
© 2009 Microchip Technology Inc. DS39752B-page 17
PIC18F1230/1330
3.3 Data EEPROM Programming
Data EEPROM is accessed one byte at a time via an
Address Pointer (register pair, EEADRH:EEADR) and
a Data Latch (EEDATA). Data EEPROM is written by
loading EEADRH:EEADR with the desired memory
location, EEDATA with the data to be written and initiat-
ing a memory write by appropriately configuring the
EECON1 register. A byte write automatically erases the
location and writes the new data (erase-before-write).
When using the EECON1 register to perform a data
EEPROM write, both the EEPGD and CFGS bits must
be cleared (EECON1<7:6> = 00). The WREN bit must
be set (EECON1<2> = 1) to enable writes of any sort
and this must be done prior to initiating a write
sequence. The write sequence is initiated by setting the
WR bit (EECON1<1> = 1).
The write begins on the falling edge of the 4th PGC
after the WR bit is set. It ends when the WR bit is
cleared by hardware.
After the programming sequence terminates, PGC must
still be held low for the time specified by parameter P10
to allow high-voltage discharge of the memory array.
FIGURE 3-6: PROGRAM DATA FLOW
FIGURE 3-7: DATA EEPROM WRITE TIMING
Start
Start Write
Set Data
Done
No
Yes
Done?
Enable Write
Sequence
Set Address
WR bit
clear? No
Yes
n
PGC
PGD
PGD = Input
0000
BSF EECON1, WR
4-Bit Command
1234 121516
P5 P5A
P10
12
n
Poll WR bit, Repeat until Clear 16-Bit Data
Payload
1234 121516 123
P5 P5A
412 1516
P5 P5A
0000
MOVF EECON1, W, 04-Bit Command
0000
4-Bit Command Shift Out Data
MOVWF TABLAT
PGC
PGD
(see below)
(see Figure 4-4)
PGD = Input PGD = Output
Poll WR bit
P11A

PIC18F1230/1330
DS39752B-page 18 © 2009 Microchip Technology Inc.
TABLE 3-7: PROGRAMMING DATA MEMORY
4-Bit
Command Data Payload Core Instruction
Step 1: Direct access to data EEPROM.
0000
0000
9E A6
9C A6
BCF EECON1, EEPGD
BCF EECON1, CFGS
Step 2: Set the data EEPROM Address Pointer.
0000
0000
0000
0000
0E <Addr>
6E A9
OE <AddrH>
6E AA
MOVLW <Addr>
MOVWF EEADR
MOVLW <AddrH>
MOVWF EEADRH
Step 3: Load the data to be written.
0000
0000
0E <Data>
6E A8
MOVLW <Data>
MOVWF EEDATA
Step 4: Enable memory writes.
0000 84 A6 BSF EECON1, WREN
Step 5: Initiate write.
0000 82 A6 BSF EECON1, WR
Step 6: Poll WR bit, repeat until the bit is clear.
0000
0000
0000
0010
50 A6
6E F5
00 00
<MSB><LSB>
MOVF EECON1, W, 0
MOVWF TABLAT
NOP
Shift out data(1)
Step 7: Hold PGC low for time P10.
Step 8: Disable writes.
0000 94 A6 BCF EECON1, WREN
Repeat steps 2 through 8 to write more data.
Note 1: See Figure 4-4 for details on shift out data timing.

© 2009 Microchip Technology Inc. DS39752B-page 19
PIC18F1230/1330
3.4 ID Location Programming
The ID locations are programmed much like the code
memory. The ID registers are mapped in addresses
200000h through 200007h. These locations read out
normally even after code protection.
Table 3-8 demonstrates the code sequence required to
write the ID locations.
In order to modify the ID locations, refer to the
methodology described in Section 3.2.1 “Modifying
Code Memory”. As with code memory, the ID
locations must be erased before being modified.
TABLE 3-8: WRITE ID SEQUENCE
Note: The user only needs to fill the first 8 bytes
of the write buffer in order to write the ID
locations.
4-Bit
Command Data Payload Core Instruction
Step 1: Direct access to code memory and enable writes.
0000
0000
8E A6
9C A6
BSF EECON1, EEPGD
BCF EECON1, CFGS
Step 2: Load write buffer with 8 bytes and write.
0000
0000
0000
0000
0000
0000
1101
1101
1101
1111
0000
0E 20
6E F8
0E 00
6E F7
0E 00
6E F6
<MSB><LSB>
<MSB><LSB>
<MSB><LSB>
<MSB><LSB>
00 00
MOVLW 20h
MOVWF TBLPTRU
MOVLW 00h
MOVWF TBLPTRH
MOVLW 00h
MOVWF TBLPTRL
Write 2 bytes and post-increment address by 2.
Write 2 bytes and post-increment address by 2.
Write 2 bytes and post-increment address by 2.
Write 2 bytes and start programming.
NOP - hold PGC high for time P9 and low for time P10.

PIC18F1230/1330
DS39752B-page 20 © 2009 Microchip Technology Inc.
3.5 Boot Block Programming
The code sequence detailed in Table 3-5 should be
used, except that the address used in “Step 2” will be in
the range of 00000h to 007FFh.
3.6 Configuration Bits Programming
Unlike code memory, the Configuration bits are
programmed a byte at a time. The Table Write, Begin
Programming 4-bit command (‘1111’) is used, but only
8 bits of the following 16-bit payload will be written. The
LSB of the payload will be written to even addresses and
the MSB will be written to odd addresses. The code
sequence to program two consecutive Configuration
locations is shown in Table 3-9.
TABLE 3-9: SET ADDRESS POINTER TO CONFIGURATION LOCATION
FIGURE 3-8: CONFIGURATION PROGRAMMING FLOW
Note: The address must be explicitly written for
each byte programmed. The addresses
can not be incremented in this mode.
4-Bit
Command Data Payload Core Instruction
Step 1: Enable writes and direct access to configuration memory.
0000
0000
8E A6
8C A6
BSF EECON1, EEPGD
BSF EECON1, CFGS
Step 2: Set Table Pointer for configuration byte to be written. Write even/odd addresses.(1)
0000
0000
0000
0000
0000
0000
1111
0000
0000
0000
1111
0000
0E 30
6E F8
0E 00
6E F7
0E 00
6E F6
<MSB ignored><LSB>
00 00
0E 01
6E F6
<MSB><LSB ignored>
00 00
MOVLW 30h
MOVWF TBLPTRU
MOVLW 00h
MOVWF TBLPRTH
MOVLW 00h
MOVWF TBLPTRL
Load 2 bytes and start programming.
NOP - hold PGC high for time P9 and low for time P10.
MOVLW 01h
MOVWF TBLPTRL
Load 2 bytes and start programming.
NOP - hold PGC high for time P9 and low for time P10.
Note 1: Enabling the write protection of Configuration bits (WRTC = 0 in CONFIG6H) will prevent further writing of Configuration
bits. Always write all the Configuration bits before enabling the write protection for Configuration bits.
Load Even
Configuration
Start
Program Program
MSB
Delay P9 and P10
Time for Write
LSB
Load Odd
Configuration
Address Address
Done
Start
Delay P9 and P10
Time for Write
Done

© 2009 Microchip Technology Inc. DS39752B-page 21
PIC18F1230/1330
4.0 READING THE DEVICE
4.1 Read Code Memory, ID Locations
and Configuration Bits
Code memory is accessed one byte at a time via the
4-bit command, ‘1001’ (table read, post-increment).
The contents of memory pointed to by the Table Pointer
(TBLPTRU:TBLPTRH:TBLPTRL) are serially output on
PGD.
The 4-bit command is shifted in, LSb first. The read is
executed during the next 8 clocks, then shifted out on
PGD during the last 8 clocks, LSb to MSb. A delay of
P6 must be introduced after the falling edge of the 8th
PGC of the operand to allow PGD to transition from an
input to an output. During this time, PGC must be held
low (see Figure 4-1). This operation also increments
the Table Pointer by one, pointing to the next byte in
code memory for the next read.
This technique will work to read any memory in the
000000h to 3FFFFFh address space, so it also applies
to the reading of the ID and Configuration registers.
TABLE 4-1: READ CODE MEMORY SEQUENCE
FIGURE 4-1: TABLE READ POST-INCREMENT INSTRUCTION TIMING (1001)
4-Bit
Command Data Payload Core Instruction
Step 1: Set Table Pointer.
0000
0000
0000
0000
0000
0000
0E <Addr[21:16]>
6E F8
0E <Addr[15:8]>
6E F7
0E <Addr[7:0]>
6E F6
MOVLW Addr[21:16]
MOVWF TBLPTRU
MOVLW <Addr[15:8]>
MOVWF TBLPTRH
MOVLW <Addr[7:0]>
MOVWF TBLPTRL
Step 2: Read memory and then shift out on PGD, LSb to MSb.
1001 00 00 TBLRD *+
1234
PGC
P5
PGD
PGD = Input
Shift Data Out
P6
PGD = Output
5678 1234
P5A
910 11 13 15 161412
Fetch Next 4-Bit Command
1001
PGD = Input
LSb MSb123456
1234
nnnn
P14

PIC18F1230/1330
DS39752B-page 22 © 2009 Microchip Technology Inc.
4.2 Verify Code Memory and ID
Locations
The verify step involves reading back the code memory
space and comparing it against the copy held in the
programmer’s buffer. Memory reads occur a single byte
at a time, so two bytes must be read to compare
against the word in the programmer’s buffer. Refer to
Section 4.1 “Read Code Memory, ID Locations and
Configuration Bits” for implementation details of
reading code memory.
The Table Pointer must be manually set to 200000h
(base address of the ID locations) once the code
memory has been verified. The post-increment feature
of the table read 4-bit command may not be used to
increment the Table Pointer beyond the code memory
space. In an 8-Kbyte device, for example, a post-
increment read of address 01FFFh will wrap the Table
Pointer back to 00000h, rather than point to
unimplemented address, 02000h.
FIGURE 4-2: VERIFY CODE MEMORY FLOW
Read Low Byte
Read High Byte
Does
Word = Expect
Data? Failure,
Report
Error
All
code memory
verified?
No
Yes
No
Set TBLPTR = 0
Start
Set TBLPTR = 200000h
Yes
Read Low Byte
Read High Byte
Does
Word = Expect
Data? Failure,
Report
Error
All
ID locations
verified?
No
Yes
Done
Yes
No
with Post-Increment
with Post-Increment Increment
Pointer
with Post-Increment
with Post-Increment

© 2009 Microchip Technology Inc. DS39752B-page 23
PIC18F1230/1330
4.3 Verify Configuration Bits
A Configuration address may be read and output on
PGD via the 4-bit command, ‘1001’. Configuration data
is read and written in a byte-wise fashion, so it is not
necessary to merge two bytes into a word prior to a
compare. The result may then be immediately
compared to the appropriate configuration data in the
programmer’s memory for verification. Refer to
Section 4.1 “Read Code Memory, ID Locations and
Configuration Bits” for implementation details of
reading Configuration data.
4.4 Read Data EEPROM Memory
Data EEPROM is accessed one byte at a time via an
Address Pointer (register pair, EEADRH:EEADR) and a
Data Latch (EEDATA). Data EEPROM is read by loading
EEADRH:EEADR with the desired memory location and
initiating a memory read by appropriately configuring the
EECON1 register. The data will be loaded into EEDATA,
where it may be serially output on PGD via the 4-bit com-
mand, ‘0010’ (Shift Out Data Holding register). A delay
of P6 must be introduced after the falling edge of the 8th
PGC of the operand to allow PGD to transition from an
input to an output. During this time, PGC must be held
low (see Figure 4-4).
The command sequence to read a single byte of data
is shown in Table 4-2.
FIGURE 4-3: READ DATA EEPROM
FLOW
TABLE 4-2: READ DATA EEPROM MEMORY
Start
Set
Address
Read
Byte
Done
No
Yes
Done?
Move to TABLAT
Shift Out Data
4-Bit
Command Data Payload Core Instruction
Step 1: Direct access to data EEPROM.
0000
0000
9E A6
9C A6
BCF EECON1, EEPGD
BCF EECON1, CFGS
Step 2: Set the Data EEPROM Address Pointer.
0000
0000
0000
0000
0E <Addr>
6E A9
OE <AddrH>
6E AA
MOVLW <Addr>
MOVWF EEADR
MOVLW <AddrH>
MOVWF EEADRH
Step 3: Initiate a memory read.
0000 80 A6 BSF EECON1, RD
Step 4: Load data into the Serial Data Holding register.
0000
0000
0000
0010
50 A8
6E F5
00 00
<MSB><LSB>
MOVF EEDATA, W, 0
MOVWF TABLAT
NOP
Shift Out Data(1)
Note 1: The <LSB> is undefined. The <MSB> is the data.
PIC18F1230/1330
DS39752B-page 24 © 2009 Microchip Technology Inc.
FIGURE 4-4: SHIFT OUT DATA HOLDING REGISTER TIMING (0010)
4.5 Verify Data EEPROM
A data EEPROM address may be read via a sequence
of core instructions (4-bit command, ‘0000’) and then
output on PGD via the 4-bit command, ‘0010’ (TABLAT
register). The result may then be immediately
compared to the appropriate data in the programmer’s
memory for verification. Refer to Section 4.4 “Read
Data EEPROM Memory” for implementation details of
reading data EEPROM.
4.6 Blank Check
The term “Blank Check” means to verify that the device
has no programmed memory cells. All memories must
be verified: code memory, data EEPROM, ID locations
and Configuration bits. The Device ID registers
(3FFFFEh:3FFFFFh) should be ignored.
A “blank” or “erased” memory cell will read as a ‘1’.
Therefore, Blank Checking a device merely means to
verify that all bytes read as FFh except the
Configuration bits. Unused (reserved) Configuration
bits will read ‘0’ (programmed). Refer to Table 5-1 for
blank configuration expect data for the various
PIC18F1230/1330 devices.
Given that Blank Checking is merely code and data
EEPROM verification with FFh expect data, refer to
Section 4.4 “Read Data EEPROM Memory” and
Section 4.2 “Verify Code Memory and ID Locations”
for implementation details.
FIGURE 4-5: BLANK CHECK FLOW
1234
PGC
P5
PGD
PGD = Input
Shift Data Out
P6
PGD = Output
5678 1234
P5A
91011 13 15161412
Fetch Next 4-Bit Command
0100
PGD = Input
LSb MSb123456
1234
nnnn
P14
Yes
No
Start
Blank Check Device
Is
device
blank? Continue
Abort
© 2009 Microchip Technology Inc. DS39752B-page 25
PIC18F1230/1330
5.0 CONFIGURATION WORD
The PIC18F1230/1330 devices have several Configura-
tion Words. These bits can be set or cleared to select
various device configurations. All other memory areas
should be programmed and verified prior to setting
Configuration Words. These bits may be read out nor-
mally, even after read or code protection. See Table 5-1
for a list of Configuration bits and Device IDs and
Table 5-3 for the Configuration bit descriptions.
5.1 ID Locations
A user may store identification information (ID) in eight
ID locations, mapped in 200000h:200007h. It is
recommended that the most significant nibble of each
ID be Fh. In doing so, if the user code inadvertently tries
to execute from the ID space, the ID data will execute
as a NOP.
5.2 Device ID Word
The Device ID Word for the PIC18F1230/1330 devices
is located at 3FFFFEh:3FFFFFh. These bits may be
used by the programmer to identify what device type is
being programmed and read out normally, even after
code or read protection. See Table 5-2 for a complete
list of Device ID values.
FIGURE 5-1: READ DEVICE ID WORD
FLOW
TABLE 5-1: CONFIGURATION BITS AND DEVICE IDs
TABLE 5-2: DEVICE ID VALUE
Start
Set TBLPTR = 3FFFFE
Done
Read Low Byte
Read High Byte
with Post-Increment
with Post-Increment
File Name Bit 7 Bit 6 Bit 5 Bit 4 Bit 3 Bit 2 Bit 1 Bit 0 Default/
Unprogrammed
Value
300001h CONFIG1H IESO FCMEN —— FOSC3 FOSC2 FOSC1 FOSC0 00-- 0111
300002h CONFIG2L — — — BORV1 BORV0 BOREN1 BOREN0 PWRTEN ---1 1111
300003h CONFIG2H — — — WDTPS3 WDTPS2 WDTPS1 WDTPS0 WDTEN ---1 1111
300004h CONFIG3L — — — — HPOL LPOL PWMPIN —---- 111-
300005h CONFIG3H MCLRE — — —T1OSCMX——FLTAMX1--- 0--1
300006h CONFIG4L BKBUG XINST BBSIZ1 BBSIZ0 — — —STVREN1000 ---1
300008h CONFIG5L — — — — — —CP1CP0---- --11
300009h CONFIG5H CPD CPB — — — — — — 11-- ----
30000Ah CONFIG6L — — — — — — WRT1 WRT0 ---- --11
30000Bh CONFIG6H WRTD WRTB WRTC — — — — — 111- ----
30000Ch CONFIG7L — — — — — — EBTR1 EBTR0 ---- --11
30000Dh CONFIG7H —EBTRB— — — — — — -1-- ----
3FFFFEh DEVID1(1) DEV2 DEV1 DEV0 REV4 REV3 REV2 REV1 REV0 See Table 5-2
3FFFFFh DEVID2(1) DEV10 DEV9 DEV8 DEV7 DEEV6 DEV5 DEV4 DEV3 See Table 5-2
Legend: x = unknown, u = unchanged, - = unimplemented.Shaded cells are unimplemented, read as ‘0’.
Note 1: DEVID registers are read-only and cannot be programmed by the user.
Device Device ID Value
DEVID2 DEVID1
PIC18F1230 1Eh 000x xxxx
PIC18F1330 1Eh 001x xxxx
PIC18F1330-ICD 1Fh 111x xxxx
Note: The ‘x’s in DEVID1 contain the device revision code.

PIC18F1230/1330
DS39752B-page 26 © 2009 Microchip Technology Inc.
TABLE 5-3: PIC18F1230/1330 BIT DESCRIPTIONS
Bit Name Configuration
Words Description
IESO CONFIG1H Internal External Switchover bit
1 = Internal External Switchover mode enabled
0 = Internal External Switchover mode disabled
FCMEN CONFIG1H Fail-Safe Clock Monitor Enable bit
1 = Fail-Safe Clock Monitor enabled
0 = Fail-Safe Clock Monitor disabled
FOSC<3:0> CONFIG1H Oscillator Selection bits
11xx = External RC oscillator, CLKO function on RA6
101x = External RC oscillator, CLKO function on RA6
1001 = Internal RC oscillator, CLKO function on RA6, port function on RA7
1000 = Internal RC oscillator, port function on RA6, port function on RA7
0111 = External RC oscillator, port function on RA6
0110 = HS oscillator, PLL enabled (Clock Frequency = 4 x FOSC1)
0101 = EC oscillator, port function on RA6
0100 = EC oscillator, CLKO function on RA6
0011 = External RC oscillator, CLKO function on RA6
0010 = HS oscillator
0001 = XT oscillator
0000 = LP oscillator
BORV<1:0> CONFIG2L Brown-out Reset Voltage bits
11 =V
BOR set to 2.0V
10 =V
BOR set to 2.7V
01 =V
BOR set to 4.2V
00 =V
BOR set to 4.5V
BOREN<1:0> CONFIG2L Brown-out Reset Enable bits
11 = Brown-out Reset enabled in hardware only (SBOREN is disabled)
10 = Brown-out Reset enabled in hardware only and disabled in Sleep mode
(SBOREN is disabled)
01 = Brown-out Reset enabled and controlled by software (SBOREN is enabled)
00 = Brown-out Reset disabled in hardware and software
PWRTEN CONFIG2L Power-up Timer Enable bit
1 = PWRT disabled
0 = PWRT enabled
WDTPS<3:0> CONFIG2H Watchdog Timer Postscaler Select bits
1111 = 1:32,768
1110 = 1:16,384
1101 = 1:8,192
1100 = 1:4,096
1011 = 1:2,048
1010 = 1:1,024
1001 = 1:512
1000 = 1:256
0111 = 1:128
0110 = 1:64
0101 = 1:32
0100 = 1:16
0011 = 1:8
0010 = 1:4
0001 = 1:2
0000 = 1:1
Note 1: The BBSIZ<1:0> bits can not be changed once any of the following code-protect bits are enabled: CPB or
CP0, WRTB or WRT0, EBTRB or EBTR0.
For P‘C18F1330 devxce.
For P‘C18F1230 devxce.
© 2009 Microchip Technology Inc. DS39752B-page 27
PIC18F1230/1330
WDTEN CONFIG2H Watchdog Timer Enable bit
1 = WDT enabled
0 = WDT disabled (control is placed on SWDTEN bit)
HPOL CONFIG3L High Side Transistors Polarity bit (Odd PWM Output Polarity Control bit)
1 = PWM 1, 3 and 5 are active-high (default)
0 = PWM 1, 3 and 5 are active-low
LPOL CONFIG3L Low Side Transistors Polarity bit (Even PWM Output Polarity Control bit)
1 = PWM 0, 2 and 4 are active-high (default)
0 = PWM 0, 2 and 4 are active-low
PWMPIN CONFIG3L PWM Output Pins Reset State Control bit
1 = PWM outputs disabled upon Reset
0 = PWM outputs drive active states upon Reset
MCLRE CONFIG3H MCLR Pin Enable bit
1 =MCLR pin enabled, RA5 input pin disabled
0 = RA5 input pin enabled, MCLR pin disabled
T1OSCMX CONFIG3H T1OSC MUX bit
1 = T1OSC pins reside on RA6 and RA7
0 = T1OSC pins reside on RB2 and RB3
FLTAMX CONFIG3H FLTA MUX bit
1 = FLTA is multiplexed with RA5
0 = FLTA is multiplexed with RA7
BKBUG CONFIG4L Background Debugger Enable bit
1 = Background debugger disabled, RB6 and RB7 configured as general
purpose I/O pins
0 = Background debugger enabled, RB6 and RB7 are dedicated to In-Circuit
Debug
XINST CONFIG4L Extended Instruction Set Enable bit
1 = Instruction set extension and Indexed Addressing mode enabled
0 = Instruction set extension and Indexed Addressing mode disabled
(Legacy mode)
BBSIZ<1:0>(1) CONFIG4L Boot Block Size Select bits
For PIC18F1330 device:
11 = 1 kW Boot Block size
10 = 1 kW Boot Block size
01 = 512W Boot Block size
00 = 256W Boot Block size
For PIC18F1230 device:
11 = 512W Boot Block size
10 = 512W Boot Block size
01 = 512W Boot Block size
00 = 256W Boot Block size
STVREN CONFIG4L Stack Overflow/Underflow Reset Enable bit
1 = Reset on stack overflow/underflow enabled
0 = Reset on stack overflow/underflow disabled
CP1 CONFIG5L Code Protection bits (Block 1 code memory area)
1 = Block 1 is not code-protected
0 = Block 1 is code-protected
TABLE 5-3: PIC18F1230/1330 BIT DESCRIPTIONS (CONTINUED)
Bit Name Configuration
Words Description
Note 1: The BBSIZ<1:0> bits can not be changed once any of the following code-protect bits are enabled: CPB or
CP0, WRTB or WRT0, EBTRB or EBTR0.

PIC18F1230/1330
DS39752B-page 28 © 2009 Microchip Technology Inc.
CP0 CONFIG5L Code Protection bits (Block 0 code memory area)
1 = Block 0 is not code-protected
0 = Block 0 is code-protected
CPD CONFIG5H Code Protection bits (Data EEPROM)
1 = Data EEPROM is not code-protected
0 = Data EEPROM is code-protected
CPB CONFIG5H Code Protection bits (Boot Block memory area)
1 = Boot Block is not code-protected
0 = Boot Block is code-protected
WRT1 CONFIG6L Write Protection bits (Block 1 code memory area)
1 = Block 1 is not write-protected
0 = Block 1 is write-protected
WRT0 CONFIG6L Write Protection bits (Block 0 code memory area)
1 = Block 0 is not write-protected
0 = Block 0 is write-protected
WRTD CONFIG6H Write Protection bit (Data EEPROM)
1 = Data EEPROM is not write-protected
0 = Data EEPROM is write-protected
WRTB CONFIG6H Write Protection bit (Boot Block memory area)
1 = Boot Block is not write-protected
0 = Boot Block is write-protected
WRTC CONFIG6H Write Protection bit (Configuration registers)
1 = Configuration registers are not write-protected
0 = Configuration registers are write-protected
EBTR1 CONFIG7L Table Read Protection bit (Block 1 code memory area)
1 = Block 1 is not protected from table reads executed in other blocks
0 = Block 1 is protected from table reads executed in other blocks
EBTR0 CONFIG7L Table Read Protection bit (Block 0 code memory area)
1 = Block 0 is not protected from table reads executed in other blocks
0 = Block 0 is protected from table reads executed in other blocks
EBTRB CONFIG7H Table Read Protection bit (Boot Block memory area)
1 = Boot Block is not protected from table reads executed in other blocks
0 = Boot Block is protected from table reads executed in other blocks
DEV<10:3> DEVID2 Device ID bits
These bits are used with the DEV<2:0> bits in the DEVID1 register to
identify the part number.
DEV<2:0> DEVID1 Device ID bits
These bits are used with the DEV<10:3> bits in the DEVID2 register to
identify the part number.
TABLE 5-3: PIC18F1230/1330 BIT DESCRIPTIONS (CONTINUED)
Bit Name Configuration
Words Description
Note 1: The BBSIZ<1:0> bits can not be changed once any of the following code-protect bits are enabled: CPB or
CP0, WRTB or WRT0, EBTRB or EBTR0.

© 2009 Microchip Technology Inc. DS39752B-page 29
PIC18F1230/1330
5.3 Embedding Configuration Word
Information in the HEX File
To allow portability of code, a PIC18F1230/1330
programmer is required to read the Configuration Word
locations from the hex file. If Configuration Word
information is not present in the hex file, then a simple
warning message should be issued. Similarly, while
saving a hex file, all Configuration Word information
must be included. An option to not include the
Configuration Word information may be provided.
When embedding Configuration Word information in
the hex file, it should start at address 300000h.
Microchip Technology Inc. feels strongly that this
feature is important for the benefit of the end customer.
5.4 Embedding Data EEPROM
Information in the HEX File
To allow portability of code, a PIC18F1230/1330
programmer is required to read the data EEPROM
information from the hex file. If data EEPROM informa-
tion is not present, a simple warning message should
be issued. Similarly, when saving a hex file, all data
EEPROM information must be included. An option to
not include the data EEPROM information may be
provided. When embedding data EEPROM information
in the hex file, it should start at address F00000h.
Microchip Technology Inc. believes that this feature is
important for the benefit of the end customer.
5.5 Checksum Computation
The checksum is calculated by summing the following:
• The contents of all code memory locations
• The Configuration Word, appropriately masked
• ID locations
The Least Significant 16 bits of this sum are the
checksum.
Table 5-4 (pages 30 through 31) describes how to
calculate the checksum for each device.
Note: The checksum calculation differs depend-
ing on the code-protect setting. Since the
code memory locations read out differently
depending on the code-protect setting, the
table describes how to manipulate the
actual code memory values to simulate
the values that would be read from a
protected device. When calculating a
checksum by reading a device, the entire
code memory can simply be read and
summed. The Configuration Word and ID
locations can always be read.
Hem
Descmgtlon
PIC18F1230/1330
DS39752B-page 30 © 2009 Microchip Technology Inc.
TABLE 5-4: CHECKSUM COMPUTATION
Device Code-Protect Checksum Blank
Value
0xAA at 0
and Max
Address
PIC18F1230
None SUM(0000:01FF)+SUM(0200:FFF)+SUM(1000:1FFF)+(CONFIG0 & 0000)+
(CONFIG1 & 00CF)+(CONFIG2 & 001F)+(CONFIG3 & 001F)+
(CONFIG4 & 000E)+(CONFIG5 & 0089)+(CONFIG6 & 00F1)+
(CONFIG7 & 0000)+(CONFIG8 & 0003)+(CONFIG9 & 00C0)+
(CONFIG10 & 0003)+(CONFIG11 & 00E0)+(CONFIG12 & 0003)+
(CONFIG13 & 0040)
F33E F294
Boot 256W SUM(0200:FFF)+SUM(1000:1FFF)+(CONFIG0 & 0000)+(CONFIG1 & 00CF)+
(CONFIG2 & 001F)+(CONFIG3 & 001F)+(CONFIG4 & 000E)+
(CONFIG5 & 0089)+(CONFIG6 & 00F1)+(CONFIG7 & 0000)+
(CONFIG8 & 0003)+(CONFIG9 & 00C0)+(CONFIG10 & 0003)+
(CONFIG11 & 00E0)+(CONFIG12 & 0003)+(CONFIG13 & 0040)+SUM(IDs)
F521 F4C7
Boot 512W SUM(0400:FFF)+SUM(1000:1FFF)+(CONFIG0 & 0000)+(CONFIG1 & 00CF)+
(CONFIG2 & 001F)+(CONFIG3 & 001F)+(CONFIG4 & 000E)+
(CONFIG5 & 0089)+(CONFIG6 & 00F1)+(CONFIG7 & 0000)+
(CONFIG8 & 0003)+(CONFIG9 & 00C0)+(CONFIG10 & 0003)+
(CONFIG11 & 00E0)+(CONFIG12 & 0003)+(CONFIG13 & 0040)+SUM(IDs)
F732 F6D8
Boot/
Block 0
SUM(1000:1FFF)+(CONFIG0 & 0000)+(CONFIG1 & 00CF)+
(CONFIG2 & 001F)+(CONFIG3 & 001F)+(CONFIG4 & 000E)+
(CONFIG5 & 0089)+(CONFIG6 & 00F1)+(CONFIG7 & 0000)+
(CONFIG8 & 0003)+(CONFIG9 & 00C0)+(CONFIG10 & 0003)+
(CONFIG11 & 00E0)+(CONFIG12 & 0003)+(CONFIG13 & 0040)+SUM(IDs)
FB53 FAF9
All (CONFIG0 & 0000)+(CONFIG1 & 00CF)+(CONFIG2 & 001F)+
(CONFIG3 & 001F)+(CONFIG4 & 000E)+(CONFIG5 & 0089)+
(CONFIG6 & 00F1)+(CONFIG7 & 0000)+(CONFIG8 & 0003)+
(CONFIG9 & 00C0)+(CONFIG10 & 0003)+(CONFIG11 & 00E0)+
(CONFIG12 & 0003)+(CONFIG13 & 0040)+SUM(IDs)
F351 F34C
Legend: Item Description
CFGW = Configuration Word
SUM[a:b] = Sum of locations, a to b inclusive
SUM_ID = Byte-wise sum of lower four bits of all customer ID locations
+ = Addition
& = Bit-wise AND
Hem
Descmgtlon
© 2009 Microchip Technology Inc. DS39752B-page 31
PIC18F1230/1330
PIC18F1330
None SUM(0000:01FF)+SUM(0200:FFF)+SUM(1000:1FFF)+(CONFIG0 & 0000)+
(CONFIG1 & 00CF)+(CONFIG2 & 001F)+(CONFIG3 & 001F)+
(CONFIG4 & 000E)+(CONFIG5 & 0089)+(CONFIG6 & 00F1)+
(CONFIG7 & 0000)+(CONFIG8 & 0003)+(CONFIG9 & 00C0)+
(CONFIG10 & 0003)+(CONFIG11 & 00E0)+(CONFIG12 & 0003)+
(CONFIG13 & 0040)
E33E E294
Boot 256W SUM(0200:FFF)+SUM(1000:1FFF)+(CONFIG0 & 0000)+(CONFIG1 & 00CF)+
(CONFIG2 & 001F)+(CONFIG3 & 001F)+(CONFIG4 & 000E)+
(CONFIG5 & 0089)+(CONFIG6 & 00F1)+(CONFIG7 & 0000)+
(CONFIG8 & 0003)+(CONFIG9 & 00C0)+(CONFIG10 & 0003)+
(CONFIG11 & 00E0)+(CONFIG12 & 0003)+(CONFIG13 & 0040)+SUM(IDs)
E520 E4C6
Boot 512W SUM(0400:FFF)+SUM(1000:1FFF)+(CONFIG0 & 0000)+(CONFIG1 & 00CF)+
(CONFIG2 & 001F)+(CONFIG3 & 001F)+(CONFIG4 & 000E)+
(CONFIG5 & 0089)+(CONFIG6 & 00F1)+(CONFIG7 & 0000)+
(CONFIG8 & 0003)+(CONFIG9 & 00C0)+(CONFIG10 & 0003)+
(CONFIG11 & 00E0)+(CONFIG12 & 0003)+(CONFIG13 & 0040)+SUM(IDs)
E731 E6D7
Boot 1 kW SUM(0800:FFF)+SUM(1000:1FFF)+(CONFIG0 & 0000)+(CONFIG1 & 00CF)+
(CONFIG2 & 001F)+(CONFIG3 & 001F)+(CONFIG4 & 000E)+
(CONFIG5 & 0089)+(CONFIG6 & 00F1)+(CONFIG7 & 0000)+
(CONFIG8 & 0003)+(CONFIG9 & 00C0)+(CONFIG10 & 0003)+
(CONFIG11 & 00E0)+(CONFIG12 & 0003)+(CONFIG13 & 0040)+SUM(IDs)
E731 E6D7
Boot/
Block 0
SUM(1000:1FFF)+(CONFIG0 & 0000)+(CONFIG1 & 00CF)+
(CONFIG2 & 001F)+(CONFIG3 & 001F)+(CONFIG4 & 000E)+
(CONFIG5 & 0089)+(CONFIG6 & 00F1)+(CONFIG7 & 0000)+
(CONFIG8 & 0003)+(CONFIG9 & 00C0)+(CONFIG10 & 0003)+
(CONFIG11 & 00E0)+(CONFIG12 & 0003)+(CONFIG13 & 0040)+SUM(IDs)
F352 F2F8
All (CONFIG0 & 0000)+(CONFIG1 & 00CF)+(CONFIG2 & 001F)+
(CONFIG3 & 001F)+(CONFIG4 & 000E)+(CONFIG5 & 0089)+
(CONFIG6 & 00F1)+(CONFIG7 & 0000)+(CONFIG8 & 0003)+
(CONFIG9 & 00C0)+(CONFIG10 & 0003)+(CONFIG11 & 00E0)+
(CONFIG12 & 0003)+(CONFIG13 & 0040)+SUM(IDs)
E34B E34B
TABLE 5-4: CHECKSUM COMPUTATION (CONTINUED)
Device Code-Protect Checksum Blank
Value
0xAA at 0
and Max
Address
Legend: Item Description
CFGW = Configuration Word
SUM[a:b] = Sum of locations, a to b inclusive
SUM_ID = Byte-wise sum of lower four bits of all customer ID locations
+ = Addition
& = Bit-wise AND
Param
PIC18F1230/1330
DS39752B-page 32 © 2009 Microchip Technology Inc.
6.0 AC/DC CHARACTERISTICS TIMING REQUIREMENTS
FOR PROGRAM/VERIFY TEST MODE
Standard Operating Conditions
Operating Temperature: 25°C is recommended
Param
No. Sym Characteristic Min Max Units Conditions
D110 VIHH High-Voltage Programming Voltage on
MCLR/VPP/RA5/FLTA
VDD + 4.0 12.5 V (Note 2)
D110A VIHL Low-Voltage Programming Voltage on
MCLR/VPP/RA5/FLTA
2.00 5.50 V (Note 2)
D111 VDD Supply Voltage During Programming 2.00 5.50 V Externally timed,
row erases and all writes
3.00 5.50 V Self-timed,
bulk erases only (Note 3)
D112 IPP Programming Current on MCLR/VPP/RA5/FLTA —300μA(Note 2)
D113 IDDP Supply Current During Programming — 10 mA
D031 VIL Input Low Voltage VSS 0.2 VDD V
D041 VIH Input High Voltage 0.8 VDD VDD V
D080 VOL Output Low Voltage — 0.6 V IOL = 8.5 mA @ 4.5V
D090 VOH Output High Voltage VDD – 0.7 — V IOH = -3.0 mA @ 4.5V
D012 CIO Capacitive Loading on I/O pin (PGD) — 50 pF To meet AC specifications
P1 TRMCLR/VPP/RA5/FLTA Rise Time to Enter
Program/Verify mode
—1.0μs(Notes 1, 2)
P2 TPGC Serial Clock (PGC) Period 100 — ns VDD = 5.0V
1—μsV
DD = 2.0V
P2A TPGCL Serial Clock (PGC) Low Time 40 — ns VDD = 5.0V
400 — ns VDD = 2.0V
P2B TPGCH Serial Clock (PGC) High Time 40 — ns VDD = 5.0V
400 — ns VDD = 2.0V
P3 TSET1 Input Data Setup Time to Serial Clock ↓15 — ns
P4 THLD1 Input Data Hold Time from PGC ↓ 15 — ns
P5 TDLY1 Delay between 4-bit Command and Command
Operand
40 — ns
P5A TDLY1ADelay between 4-bit Command Operand and Next
4-bit Command
40 — ns
P6 TDLY2 Delay between Last PGC ↓ of Command Byte to
First PGC ↑ of Read of Data Word
20 — ns
P9 TDLY5 PGC High Time (minimum programming time) 1 — ms Externally Timed
P10 TDLY6 PGC Low Time after Programming
(high-voltage discharge time)
100 — μs
P11 TDLY7 Delay to allow Self-Timed Data Write or
Bulk Erase to Occur
5—ms
Note 1: Do not allow excess time when transitioning MCLR between VIL and VIHH; this can cause spurious program
executions to occur. The maximum transition time is:
1 TCY + TPWRT (if enabled) + 1024 TOSC (for LP, HS, HS/PLL and XT modes only) +
2 ms (for HS/PLL mode only) + 1.5 μs (for EC mode only)
where TCY is the instruction cycle time, TPWRT is the Power-up Timer period and TOSC is the oscillator period. For
specific values, refer to the Electrical Characteristics section of the device data sheet for the particular device.
2: This specification also applies to ICVPP for the PIC18F1330-ICD device.
3: At 0°C-50°C.
Param
© 2009 Microchip Technology Inc. DS39752B-page 33
PIC18F1230/1330
P11A TDRWT Data Write Polling Time 4 — ms
P12 THLD2 Input Data Hold Time from MCLR/VPP/RA5/FLTA ↑2—μs
P13 TSET2VDD ↑ Setup Time to MCLR/VPP/RA5/FLTA ↑100 — ns (Note 2)
P14 TVALID Data Out Valid from PGC ↑10 — ns
P15 TSET3PGM ↑ Setup Time to MCLR/VPP/RA5/FLTA ↑2—μs(Note 2)
P16 TDLY8 Delay between Last PGC ↓ and
MCLR/VPP/RA5/FLTA ↓
0—s
P17 THLD3MCLR/VPP/RA5/FLTA ↓ to VDD ↓—100ns
P18 THLD4MCLR/VPP/RA5/FLTA ↓ to PGM ↓0—s
6.0 AC/DC CHARACTERISTICS TIMING REQUIREMENTS
FOR PROGRAM/VERIFY TEST MODE (CONTINUED)
Standard Operating Conditions
Operating Temperature: 25°C is recommended
Param
No. Sym Characteristic Min Max Units Conditions
Note 1: Do not allow excess time when transitioning MCLR between VIL and VIHH; this can cause spurious program
executions to occur. The maximum transition time is:
1 TCY + TPWRT (if enabled) + 1024 TOSC (for LP, HS, HS/PLL and XT modes only) +
2 ms (for HS/PLL mode only) + 1.5 μs (for EC mode only)
where TCY is the instruction cycle time, TPWRT is the Power-up Timer period and TOSC is the oscillator period. For
specific values, refer to the Electrical Characteristics section of the device data sheet for the particular device.
2: This specification also applies to ICVPP for the PIC18F1330-ICD device.
3: At 0°C-50°C.

PIC18F1230/1330
DS39752B-page 34 © 2009 Microchip Technology Inc.
NOTES:
QUALITY MANAGEMENT SYSTEM
CERTIFIED BY DNV
= ISO/TS 16949:2002 =
© 2009 Microchip Technology Inc. DS39752B-page 35
Information contained in this publication regarding device
applications and the like is provided only for your convenience
and may be superseded by updates. It is your responsibility to
ensure that your application meets with your specifications.
MICROCHIP MAKES NO REPRESENTATIONS OR
WARRANTIES OF ANY KIND WHETHER EXPRESS OR
IMPLIED, WRITTEN OR ORAL, STATUTORY OR
OTHERWISE, RELATED TO THE INFORMATION,
INCLUDING BUT NOT LIMITED TO ITS CONDITION,
QUALITY, PERFORMANCE, MERCHANTABILITY OR
FITNESS FOR PURPOSE. Microchip disclaims all liability
arising from this information and its use. Use of Microchip
devices in life support and/or safety applications is entirely at
the buyer’s risk, and the buyer agrees to defend, indemnify and
hold harmless Microchip from any and all damages, claims,
suits, or expenses resulting from such use. No licenses are
conveyed, implicitly or otherwise, under any Microchip
intellectual property rights.
Trademarks
The Microchip name and logo, the Microchip logo, Accuron,
dsPIC, KEELOQ, KEELOQ logo, MPLAB, PIC, PICmicro,
PICSTART, rfPIC, SmartShunt and UNI/O are registered
trademarks of Microchip Technology Incorporated in the
U.S.A. and other countries.
FilterLab, Linear Active Thermistor, MXDEV, MXLAB,
SEEVAL, SmartSensor and The Embedded Control Solutions
Company are registered trademarks of Microchip Technology
Incorporated in the U.S.A.
Analog-for-the-Digital Age, Application Maestro, CodeGuard,
dsPICDEM, dsPICDEM.net, dsPICworks, dsSPEAK, ECAN,
ECONOMONITOR, FanSense, In-Circuit Serial
Programming, ICSP, ICEPIC, Mindi, MiWi, MPASM, MPLAB
Certified logo, MPLIB, MPLINK, mTouch, nanoWatt XLP,
PICkit, PICDEM, PICDEM.net, PICtail, PIC32 logo, PowerCal,
PowerInfo, PowerMate, PowerTool, REAL ICE, rfLAB, Select
Mode, Total Endurance, TSHARC, WiperLock and ZENA are
trademarks of Microchip Technology Incorporated in the
U.S.A. and other countries.
SQTP is a service mark of Microchip Technology Incorporated
in the U.S.A.
All other trademarks mentioned herein are property of their
respective companies.
© 2009, Microchip Technology Incorporated, Printed in the
U.S.A., All Rights Reserved.
Printed on recycled paper.
Note the following details of the code protection feature on Microchip devices:
• Microchip products meet the specification contained in their particular Microchip Data Sheet.
• Microchip believes that its family of products is one of the most secure families of its kind on the market today, when used in the
intended manner and under normal conditions.
• There are dishonest and possibly illegal methods used to breach the code protection feature. All of these methods, to our
knowledge, require using the Microchip products in a manner outside the operating specifications contained in Microchip’s Data
Sheets. Most likely, the person doing so is engaged in theft of intellectual property.
• Microchip is willing to work with the customer who is concerned about the integrity of their code.
• Neither Microchip nor any other semiconductor manufacturer can guarantee the security of their code. Code protection does not
mean that we are guaranteeing the product as “unbreakable.”
Code protection is constantly evolving. We at Microchip are committed to continuously improving the code protection features of our
products. Attempts to break Microchip’s code protection feature may be a violation of the Digital Millennium Copyright Act. If such acts
allow unauthorized access to your software or other copyrighted work, you may have a right to sue for relief under that Act.
Microchip received ISO/TS-16949:2002 certification for its worldwide
headquarters, design and wafer fabrication facilities in Chandler and
Tempe, Arizona; Gresham, Oregon and design centers in California
and India. The Company’s quality system processes and procedures
are for its PIC® MCUs and dsPIC® DSCs, KEELOQ® code hopping
devices, Serial EEPROMs, microperipherals, nonvolatile memory and
analog products. In addition, Microchip’s quality system for the design
and manufacture of development systems is ISO 9001:2000 certified.
Q
‘MICFIOCHIP
DS39752B-page 36 © 2009 Microchip Technology Inc.
AMERICAS
Corporate Office
2355 West Chandler Blvd.
Chandler, AZ 85224-6199
Tel: 480-792-7200
Fax: 480-792-7277
Technical Support:
http://support.microchip.com
Web Address:
www.microchip.com
Atlanta
Duluth, GA
Tel: 678-957-9614
Fax: 678-957-1455
Boston
Westborough, MA
Tel: 774-760-0087
Fax: 774-760-0088
Chicago
Itasca, IL
Tel: 630-285-0071
Fax: 630-285-0075
Cleveland
Independence, OH
Tel: 216-447-0464
Fax: 216-447-0643
Dallas
Addison, TX
Tel: 972-818-7423
Fax: 972-818-2924
Detroit
Farmington Hills, MI
Tel: 248-538-2250
Fax: 248-538-2260
Kokomo
Kokomo, IN
Tel: 765-864-8360
Fax: 765-864-8387
Los Angeles
Mission Viejo, CA
Tel: 949-462-9523
Fax: 949-462-9608
Santa Clara
Santa Clara, CA
Tel: 408-961-6444
Fax: 408-961-6445
Toronto
Mississauga, Ontario,
Canada
Tel: 905-673-0699
Fax: 905-673-6509
ASIA/PACIFIC
Asia Pacific Office
Suites 3707-14, 37th Floor
Tower 6, The Gateway
Harbour City, Kowloon
Hong Kong
Tel: 852-2401-1200
Fax: 852-2401-3431
Australia - Sydney
Tel: 61-2-9868-6733
Fax: 61-2-9868-6755
China - Beijing
Tel: 86-10-8528-2100
Fax: 86-10-8528-2104
China - Chengdu
Tel: 86-28-8665-5511
Fax: 86-28-8665-7889
China - Hong Kong SAR
Tel: 852-2401-1200
Fax: 852-2401-3431
China - Nanjing
Tel: 86-25-8473-2460
Fax: 86-25-8473-2470
China - Qingdao
Tel: 86-532-8502-7355
Fax: 86-532-8502-7205
China - Shanghai
Tel: 86-21-5407-5533
Fax: 86-21-5407-5066
China - Shenyang
Tel: 86-24-2334-2829
Fax: 86-24-2334-2393
China - Shenzhen
Tel: 86-755-8203-2660
Fax: 86-755-8203-1760
China - Wuhan
Tel: 86-27-5980-5300
Fax: 86-27-5980-5118
China - Xiamen
Tel: 86-592-2388138
Fax: 86-592-2388130
China - Xian
Tel: 86-29-8833-7252
Fax: 86-29-8833-7256
China - Zhuhai
Tel: 86-756-3210040
Fax: 86-756-3210049
ASIA/PACIFIC
India - Bangalore
Tel: 91-80-3090-4444
Fax: 91-80-3090-4080
India - New Delhi
Tel: 91-11-4160-8631
Fax: 91-11-4160-8632
India - Pune
Tel: 91-20-2566-1512
Fax: 91-20-2566-1513
Japan - Yokohama
Tel: 81-45-471- 6166
Fax: 81-45-471-6122
Korea - Daegu
Tel: 82-53-744-4301
Fax: 82-53-744-4302
Korea - Seoul
Tel: 82-2-554-7200
Fax: 82-2-558-5932 or
82-2-558-5934
Malaysia - Kuala Lumpur
Tel: 60-3-6201-9857
Fax: 60-3-6201-9859
Malaysia - Penang
Tel: 60-4-227-8870
Fax: 60-4-227-4068
Philippines - Manila
Tel: 63-2-634-9065
Fax: 63-2-634-9069
Singapore
Tel: 65-6334-8870
Fax: 65-6334-8850
Taiwan - Hsin Chu
Tel: 886-3-572-9526
Fax: 886-3-572-6459
Taiwan - Kaohsiung
Tel: 886-7-536-4818
Fax: 886-7-536-4803
Taiwan - Taipei
Tel: 886-2-2500-6610
Fax: 886-2-2508-0102
Thailand - Bangkok
Tel: 66-2-694-1351
Fax: 66-2-694-1350
EUROPE
Austria - Wels
Tel: 43-7242-2244-39
Fax: 43-7242-2244-393
Denmark - Copenhagen
Tel: 45-4450-2828
Fax: 45-4485-2829
France - Paris
Tel: 33-1-69-53-63-20
Fax: 33-1-69-30-90-79
Germany - Munich
Tel: 49-89-627-144-0
Fax: 49-89-627-144-44
Italy - Milan
Tel: 39-0331-742611
Fax: 39-0331-466781
Netherlands - Drunen
Tel: 31-416-690399
Fax: 31-416-690340
Spain - Madrid
Tel: 34-91-708-08-90
Fax: 34-91-708-08-91
UK - Wokingham
Tel: 44-118-921-5869
Fax: 44-118-921-5820
WORLDWIDE SALES AND SERVICE
02/04/09
Products related to this Datasheet
IC MCU 8BIT 4KB FLASH 18SOIC
IC MCU 8BIT 4KB FLASH 20SSOP
IC MCU 8BIT 4KB FLASH 18SOIC
IC MCU 8BIT 4KB FLASH 18DIP
IC MCU 8BIT 8KB FLASH 18SOIC
IC MCU 8BIT 4KB FLASH 18SOIC
IC MCU 8BIT 8KB FLASH 20SSOP
IC MCU 8BIT 4KB FLASH 28QFN
IC MCU 8BIT 8KB FLASH 20SSOP
IC MCU 8BIT 8KB FLASH 28QFN
IC MCU 8BIT 8KB FLASH 18DIP
IC MCU 8BIT 4KB FLASH 28QFN
IC MCU 8BIT 4KB FLASH 18DIP
IC MCU 8BIT 4KB FLASH 20SSOP
IC MCU 8BIT 4KB FLASH 28QFN
IC MCU 8BIT 4KB FLASH 18SOIC
IC MCU 8BIT 4KB FLASH 20SSOP
IC MCU 8BIT 8KB FLASH 18SOIC
IC MCU 8BIT 8KB FLASH 20SSOP
IC MCU 8BIT 8KB FLASH 28QFN
IC MCU 8BIT 8KB FLASH 28QFN
IC MCU 8BIT 8KB FLASH 18SOIC
IC MCU 8BIT 8KB FLASH 18DIP
IC MCU 8BIT 4KB FLASH 28QFN
IC MCU 8BIT 4KB FLASH 18DIP
IC MCU 8BIT 4KB FLASH 18SOIC
IC MCU 8BIT 4KB FLASH 20SSOP
IC MCU 8BIT 4KB FLASH 18SOIC