GPS-RTK2 Hookup Guide Datasheet by SparkFun Electronics
View All Related Products | Download PDF Datasheet
GPS-RTK2 Hookup G
GPS-RTK2 Hookup Guide
Introduction
The SparkFun GPS-RTK2 and GPS-RTK-SMA raises the bar for high-precision GPS. Utilizing the latest ZED-F9P
module from u-blox the RTK2 and RTK-SMA is capable of 10mm 3 dimensional accuracy. Yes, you read that right,
these boards can output your X, Y, and Z location that is roughly the width of your fingernail. With great power
comes a few requirements: high precision GPS requires a clear view of the sky (sorry, no indoor location) and a
stream of correction data from an RTCM source. We’ll get into this more in a later section but as long as you have
two ZED-F9P breakout boards, or access to an online correction source, your ZED-F9P can output lat, long, and
altitude with centimeter grade accuracy.
SparkFun GPS-RTK2 Board - ZED-F9P (Qwiic)
GPS-15136
I.
Suggested Reading
Before getting started, be sure to checkout our What is GPS RTK? tutorial and if you want to pre-read a bit have a
look at our Getting Started with U-Center.
Hardware Overview
One of the key differentiators between the ZED-F9P and almost all other low-cost RTK solutions is the ZED-F9P is
capable of receiving both L1 and L2 bands.
I2C
An introduction to I2C, one of the main embedded
communications protocols in use today.
Serial Basic Hookup Guide
Get connected quickly with this Serial to USB adapter.
What is GPS RTK?
Learn about the latest generation of GPS and GNSS
receivers to get 2.5cm positional accuracy!
Getting Started with U-Center for u-blox
Learn the tips and tricks to use the u-blox software tool
to configure your GPS receiver.
f
. m
23“ng
m
"“ <9 “‘33="" m="" °‘="" 5="" e="" e="" g="" ®="" a="" .4="" ‘="" z"="" s="" v="" m="" .="" g:="" ;="" .'="" zmmmsm="" x="" m="" g="" _="" 70500005137="" 2="" eg="" a="" muozmo.um="" n="" kg="" 8="" ~u="" —="" i="" am="" an="" soa="" m="" pm="" is!="" m="">9>Communication Ports
The ZED-F9P is unique in that it has five communication ports which are all active simultaneously. You can read
NMEA data over I C while you send configuration commands over the UART and vice/versa. The only limit is that
the SPI pins are mapped onto the I C and UART pins so it’s either SPI or I C+UART. The USB port is available at
all times.
SparkFun GPS-RTK2 Board SparkFun GPS-RTK-SMA Board
USB
The USB C connector makes it easy to connect the ZED-F9P to u-center for configuration and quick viewing of
NMEA sentences. It is also possible to connect a Raspberry Pi or other single board computer over USB. The
ZED-F9P enumerates as a serial COM port and it is a separate serial port from the UART interface. See Getting
Started with U-Center for more information about getting the USB port to be a serial COM port.
2
2 2
549 now-mg
a guy Haw
0mg: V
ZED-FVD‘DDB-OI as
so5ouaasvo7 w 40
‘ tomoanomam E ‘E‘
J— _J
ZED-F9P-005-02 22
F1 100:149‘02 19 so
The USB port and power GPS-RTK2 The USB port and power GPS RTK-SMA
A 3.3V regulator is provided to regulate the 5V USB down to 3.3V the module requires. External 5V can be applied
or a direct feed of 3.3V can be provided. Note that if you’re provide the board with 3.3V directly it should be a clean
supply with minimal noise (less than 50mV VPP ripple is ideal for precision locating).
The 3.3V regulator is capable of sourcing 600mA from a 5V input and the USB C connection is capable of
sourcing 2A.
I C (a.k.a DDC)
The u-blox ZED-F9P has a “DDC” port which is really just an I C port (without all the fuss of trademark issues).
These pins are shared with the SPI pins. By default, the I C pins are enabled. Be sure the DSEL jumper on the
rear of the board is open. The GPS-RTK2 and GPS-RTK-SMA from SparkFun also includes two Qwiic connectors
to make daisy chaining this GPS receiver with a large variety of I C devices. Checkout Qwiic for your next project.
2
2
2
2
@max'
ass—<13: vns-uu-sds="">13:>Highlighted I2C port and Qwiic connectors on the RTK2 and RTK-SMA
All features are accessible over the I C ports including reading NMEA sentences, sending UBX configuration
strings, piping RTCM data into the module, etc. We’ve written an extensive Arduino library showing how to
configure most aspects of the ZED-F9P making I C our preferred communication method on the ZED. You can get
the library through the Arduino library manager by searching ‘SparkFun Ublox’. Checkout the SparkFun U-blox
Library section for more information.
UART/Serial
The classic serial pins are available on the ZED-F9P but are shared with the SPI pins. By default, the UART pins
are enabled. Be sure the DSEL jumper on the rear of the board is open.
TX/MISO = TX out from ZED-F9P
RX/MOSI = RX into ZED-F9P
Serial pins on SparkFun ZED-F9P breakout boards highlighted
There is a second serial port (UART2) available on the ZED-F9P that is primarily used for RTCM3 correction data.
By default, this port will automatically receive and parse incoming RTCM3 strings enabling RTK mode on the
board. In addition to the TX2/RX2 pins we have added an additional ‘RTCM Correction’ port where we arranged
the pins to match the industry standard serial connection (aka the 'FTDI' pinout). This pinout is compatible with our
Bluetooth Mate and Serial Basic so you can send RTCM correction data from a cell phone or computer. Note that
RTCM3 data can also be sent over I C, UART1, SPI, or USB if desired.
2
2
2
uo mm;
mm:
». ~guu
E3)
“we"
[In-unw-
ZEDFQP-Oofirul 0! ‘ . ZED-FfiP-DDEDI 22
Fasooooany 1s 49 mm - museum: is =0
meiozooomm -» ‘ . 109102090.‘Dnz IV:
E ; W - ‘ @
.©‘.‘
u...,.... A
o.- Jinn-3:“ mu:
mun-.- ‘ -3111:
“r4“ -nml- ‘ ; 4.
w mm mm
up m
n... |—_|s m w
|—_|s mm V
I... r—jmm V
n...
5.».
m
I Man anfimgmil—
UART2 and RTCM Correction Port on the GPS-
RTK2
UART2 and RTCM Correction Port on the GPS-RTK-
SMA
The RTCM correction port (UART2) defaults to 38400bps serial but can be configured via software commands
(checkout our Arduino library) or over USB using u-center. Keep in mind our Bluetooth Mate defaults to
115200bps. If you plan to use Bluetooth for correction data (we found it to be easiest), we recommend you
increase this port speed to 115200bps using u-center. Additionally, but less often needed, the UART2 can be
configured for NMEA output. In general, we don’t use UART2 for anything but RTCM correction data, so we
recommend leaving the in/out protocols as RTCM.
If you’ve got the ZED-F9P setup for base station mode (also called survey-in mode) the UART2 will output RTCM3
correction data. This means you can connect a radio or wired link to UART2 and the board will automatically send
just RTCM bytes over the link (no NMEA data taking up bandwidth). Here is an example using the RTK2 but you
can also use the RTK-SMA using the same setup.
«was:
VNS-uu-w
Base station setup to send RTCM bytes out over Bluetooth
SPI
The ZED-F9P can also be configured for SPI communication. By default, the SPI port is disabled. To enable SPI
close the DSEL jumper on the rear of the board. Closing this jumper will disable the UART1 and I C interfaces
(UART2 will continue to operate as normal).
The SPI pins highlighted on the SparkFun RTK2 and RTK-SMA
Control Pins
The control pins are highlighted below.
2
ZEDFOP—ooam on
Fosononvn mu '
mmozaoomm E I? 5‘
“ ,", "m-n- .-
H III-1m- -
" mun- n
mun:
M. I." -nm I l N
ZED-FfiP-DDEDZ 22
F1 100045102 19/30
1091020001002 sz
LO©garm
5‘4“““mm: .11:
mm, 0393113]:
F... manta]:
.LNCKMJL
.
Highlighted control pins of the SparkFun GPS-RTK2 Highlighted control pins of the SparkFun GPS-RTK-SMA
These pins are used for various extra control of the ZED-F9P:
FENCE: Geofence output pin. Configured with U-Center. Will go high or low when a geofence is setup.
Useful for triggering alarms and actions when the module exits a programmed perimeter.
RTK: Real Time Kinematic output pin. Remains high when module is in normal GPS mode. Begins blinking
when RTCM corrections are received and module enters RTK float mode. Goes low when module enters
RTK fixed mode and begins outputting cm-level accurate locations.
PPS: Pulse-per-second output pin. Begins blinking at 1Hz when module gets basic GPS/GNSS position
lock.
RST: Reset input pin. Pull this line low to reset the module.
SAFE: Safeboot input pin. This is required for firmware updates to the module and generally should not be
used or connected.
INT: Interrupt input/output pin. Can be configured using U-Center to bring the module out of deep sleep or to
output an interrupt for various module states.
Note: For those that need to connect a SMA connector to the PPS pin, the RTK-SMA includes a footprint so
that you can manually solder the connector to the board for your application. The PPS output is helpful as a
clock source correction when synchronizing equipment (not 1 Hz but in many MHz). The PPS output can be
configured to output a very accurate clock which scientists use to correct less accurate, but much faster
clocks. To configure, you can use the u-center to adjust The NEO-F9P's setting under View > Conviguration
View > TP (TimePulse).
moan-003.01 on
Fasouaosnv 13/48 >
“momma”: E Ex
O©1
. an" N?
I until: “1.7
nxhtlF
zi:=‘n
ZED-FfiP-DDEDZ 22
F1 100045102 19/30
Mm.
mun/u
Antenna
The ZED-F9P requires a good quality GPS or GNSS (preferred) antenna. A U.FL connector is provided. Note:
U.FL connectors are rated for only a few mating cycles (about 30) so we recommend you set it and forget it. You
may need to secure the u.FL to SMA cable depending on your application. Otherwise, you could use the RTK-
SMA version.
U.FL antenna connector and SMA cut-out on the GPS RTK2 SMA antenna connector on the GPS-SMA
A cutout for the SMA bulkhead is available for those who want an extra sturdy connection. We recommended
installing the SMA into the board only when the board is mounted in an enclosure. Otherwise, the cable runs the
risk of being damaged when compressed (for example, students carrying the board loose in a backpack). ac
SMA Connector
WRL-00593
0000000000
Hump-nos m
Fosocooa7a7
as
I8 a9
msmzaoo mam E 3
.©
' fl
000000000
ZE asap-005.02
su‘uauns‘az
msmzoan 1002
A U.FL to SMA cable threaded through the mounting hole provides a robust connection that is also easy to
disconnect at the SMA connection if needed. Check below in Connecting an Antenna for more information.
Low-cost magnetic GPS/GNSS antennas can be used (checkout the ublox white paper) but a 4” / 10cm metal disc
is required to be placed under the antenna as a metal ground plane.
LEDs
The board includes four status LEDs as indicated in the image below.
mm- mg
m»... W 8'3
vws-nuu-sde
onl-u
Status LEDs on the GPS-RTK2 Status LEDs on the GPS-SMA
PWR: The power LED will illuminate when 3.3V is activated either over USB or via the Qwiic bus.
PPS: The pulse per second LED will illuminate each second once a position lock has been achieved.
RTK: The RTK LED will be illuminated constantly upon power up. Once RTCM data has been successfully
received it will begin to blink. This is a good way to see if the ZED-F9P is getting RTCM from various
sources. Once an RTK fix is obtained, the LED will turn off.
FENCE: The FENCE LED can be configured to turn on/off for geofencing applications.
Jumpers
There are five jumpers used to configure the GPS-RTK2.
User jumpers on the SparkFun RTK2 and RTK-SMA
Closing DSEL with solder enables the SPI interface and disables the UART and I C interfaces. USB will still
function.
Cutting the I C jumper will remove the 2.2k Ohm resistors from the I C bus. If you have many devices on your I C
bus you may want to remove these jumpers. Not sure how to cut a jumper? Read here!
Cutting the JP1, JP2, JP3 jumpers on the RTK2 will disconnect of the various status LEDs from their associated
pins. These have been labeled on the RTK-SMA version. We have included a jumper for the PPS on the top and
bottom of the RTK-SMA.
Backup Battery
The MS621FE rechargeable battery maintains the battery backed RAM (BBR) on the GNSS module. This allows
for much faster position locks (a.k.a. hot start). The BBR is also used for module configuration retention. The
battery is automatically trickle charged when power is applied and should maintain settings and GNSS orbit data
for up to two weeks without power.
2
22 2
uni-3
~ I I If! you
damn
ZED-FVP-DDE-m . zaurwnooam
Fosouncavu - n mumsmz
mmozooo mo:
_0l .© ‘
-0)
The backup battery on the SparkFun RTK2 The backup battery on the SparkFun RTK-SMA
Connecting an Antenna
U.FL connectors are very good but they are a designed to be implemented inside a small embedded application
like a laptop. Exposing a U.FL connector to the wild risks it getting damaged. To prevent damaging the U.FL
connection on the GPS-RTK2 we recommend threading the U.FL cable through the stand-off hole, then attach the
U.FL connectors. This will provide a great stress relief for the antenna connection. Now attach your SMA antenna
of choice.
Be Careful! U.FL connectors are easily damaged. Make sure the connectors are aligned, flush face to
face (not at an angle), then press down using a rigid blunt edge such as the edge of a PCB or point of a small
flat head screwdriver. For more information checkout our tutorial Three Quick Tips About Using U.FL.
Additionally, a bulkhead cut-out is provided to screw the SMA onto the PCB if desired.
While this method decreases stress from the U.FL connector it is only recommended when the board has been
permanently mounted. If the board is not mounted, the cable on the U.FL cable is susceptible to being kinked
causing impedance changes that may decrease reception quality.
If you are using the the RTK-SMA, there is no need to worry about this since there is a SMA connector soldered
on the board providing a sturdy connection.
Three Quick Tips About Using U.FL
DECEMBER 28, 2018
Quick tips regarding how to connect, protect, and disconnect U.FL connectors.
If you’re indoors you must run a SMA extension cable long enough to locate the antenna where it has a clear view
of the sky. That means no trees, buildings, walls, vehicles, or concrete metally things between the antenna and the
sky. Be sure to mount the antenna on a 4”/10cm metal ground plate to increase reception.
Board Dimensions
The overall board dimensions for each board is ~1.70" x ~1.70" (~43.18mm x ~43.18mm). Keep in mind the
connectors are not flush with the board, which adds additional length to the board. Make sure to take that into
account when mounting and placing the board in an enclosure.
Board Dimensions for RTK2 Board Dimensions for RTK-SMA
Connecting the ZED-F9P to a Correction Source
Before you go out into the field it’s good to understand how to get RTCM data and how to pipe it to the GPS-RTK2
and GPS-RTK-SMA. We recommend you read Connecting a Correction Source section of the original GPS-RTK
tutorial. This will give you the basics of how to get a UNAVCO account and how to identify a Mount Point within
10km of where your ZED-F9P rover will be used. This section builds upon these concepts.
>< mm!="" mm.="" mm="" n5="" cmmm="">GPS RTK Hookup Guide: Connecting a Correction Source
For this example, we will show how to get correction data from the UNAVCO network and pull that data in using
the Android app called NTRIP Client. The correction data will then be transmitted from the app over Bluetooth to
the ZED-F9P using the SparkFun Bluetooth Mate.
Required Materials
1x GPS-RTK2 or GPS-RTK-SMA
1x GPS or GNSS Antenna
1x Metal Plate of 4” or larger
1x SMA extension cable (if needed to get a clear view of the sky)
1x USB C 2.0 Cable
1x Bluetooth Mate
1x male and female header pair
GNSS antenna sitting on a metal ground plate elevated with clear view of the sky
Now setup your GPS receiver such that you can work from your desk but have the antenna outdoors with a clear
view of the sky.
Required Software
Credentials with a free RTCM provider such as UNAVCO
U-Center
Get the NTRIP By Lefebure app from Google Play. There seem to be NTRIP apps for iOS but we have not
been able to verify any one app in particular. If you have a favorite, please let us know.
First, we need to attach the Bluetooth Module to the ZED-F9P's breakout board. Solder a female header to the
Bluetooth Mate so that it hangs off the end.
On the GPS-RTK2 or GPS_RTK-SMA board we recommend soldering the right-angle male header underneath the
board. This will allow the Bluetooth module to be succinctly tucked under the board.
When attaching the Bluetooth Mate to board be sure to align the pins so that the GND indicator align on both
boards. Once Bluetooth has been installed attach your GNSS antenna and connect the board over USB. This will
power the board and the Bluetooth Mate.
Where the male and female headers go is personal preference. For example, here are two Bluetooth Mates; one
with male headers, one with female.
a» 55mm mm
m-
mm
mm
”a.
mu
m
Soldering a female header to a Bluetooth Mate makes it easier to add Bluetooth to boards that have a 'FTDI' style
connection like our OpenScale, Arduino Pro, or Simultaneous RFID Reader. Whereas, soldering a male header to
the Bluetooth Mate makes it much easier to use in a breadboard. It's really up to you!
The Bluetooth Mate defaults to 115200bps whereas the ZED-F9P is expecting serial over UART2 to be
38400bps. To fix this we need to open u-center and change the port settings for UART2. If you haven’t already, be
sure to checkout the tutorial Getting Started with U-Center to get your bearings.
Open the Configure window and navigate to the PRT (Ports) section. Drop down the target to UART2 and set the
baud rate to 115200. Finally, click on the ‘Send’ button.
By this time you should have a valid 3D GPS lock with ~1.5m accuracy. It’s about to get a lot better.
We are going to assume you’ve read the original RTK tutorial and obtained your UNAVCO credentials including
the following:
Username
Password
IP Address for UNAVCO (69.44.86.36 at time of writing)
Caster Port (2101 at time of writing)
Data Stream a.k.a. Mount Point (‘P041_RTCM3’ if you want the one near Boulder, CO - but you should
really find one nearest your rover location)
The Bluetooth Mate should be powered up. From your phone, discover the Bluetooth Mate and pair with it. The
module used in this tutorial was discovered as RNBT-E0DC where E0DC is the last four characters of the MAC
address of the module and should be unique to your module.
Once you have your UNAVCO credentials and you’ve paired with the Bluetooth module open the NTRIP client.
IO
Receiver Settings
Receiver Connection
i ii i i i , i
Blueiooih Dewce
P ' ii i
Bluelooih Conneclion Method
i- , , ri iiii'
Au‘toVEnable Blueiooth ‘ D
117 i i»' iim
Auto-Configure Receiver
ii i i' i‘i i i
Anienna Heighi
Li 1
Save GPS Data to File E]
Save NTRIP Dala to File [3
GPS Mock Locations
i iiiiir . i‘ C]
'iwr 1‘ Mi“
Verify that the Receiver Connection is set to Bluetooth then select Bluetooth Device and select the Bluetooth
module you just paired with. Next, open NTRIP settings and enter your credentials including mounting point (a.k.a.
Data Stream).
'0
NTRIP Settings
Network Protocol
L . ‘ M
Caster IP
Caster Port
Username
Password
Data Sueam
} >- V 'J
Reported Locallon
V! ~x~ \mm
E Saved Profiles
This example demonstrates how to obtain correction data from UNAVCO’s servers but you could similarly setup
your own base station using another ZED-F9P and RTKLIB to broadcast the correction data. This NTRIP app
would connect to your RTKLIB based server giving you some amazing flexibility (the base station could be
anywhere there’s a laptop and Wifi within 10km of your rover).
Ok. You ready? This is the fun part. Return to the main NTRIP window and click Connect. The app will connect to
the Bluetooth module. Once connected, it will then connect to your NTRIP source. Once data is flowing you will
see the number of bytes increase every second.
0
[I] NTRIP Cllen
No Data Age: 73
0.0 MPH
03 26 09 Sen/Ice Started
03 2609 Dewce RNBTVEODC
03.26 ()9 Trying 10 Connect .
03 2613 Bluetooth Devwce Connected
03:2614 Network Connecung.
03 2614 NTRIP, Connected to caster
Within a few seconds you should see the RTK LED on the ZED-F9P's breakout board turn off. This indicates you
have an RTK fix. To verify this, open u-center on your computer. The first thing to notice is that Fix Mode in the left
hand black window has changed from 3D to 3D/DGNSS/FIXED.
Navigate to the UBX-NAV-HPPOSECEF message. This will show you a high-precision 3D accuracy estimate. We
were able to achieve 17mm accuracy using a low-cost GNSS antenna with a metal plate ground plane and we
were over 10km from the correction station.

Congrats! You now know where you are within the diameter of a dime!
SparkFun U-blox Library
Note: This example assumes you are using the latest version of the Arduino IDE on your desktop. If this is
your first time using Arduino, please review our tutorial on installing the Arduino IDE. If you have not
previously installed an Arduino library, please check out our installation guide.
The SparkFun Ublox Arduino library enables the reading of all positional datums as well as sending binary UBX
configuration commands over I C. This is helpful for configuring advanced modules like the ZED-F9P but also the
NEO-M8P-2, SAM-M8Q and any other Ublox module that use the Ublox binary protocol.
The SparkFun U-blox Arduino library can be downloaded with the Arduino library manager by searching
'SparkFun Ublox' or you can grab the zip here from the GitHub repository:
SPARKFUN U-BLOX ARDUINO LIBRARY (ZIP)
Once you have the library installed checkout the various examples.
Example1: Read NMEA sentences over I C using Ublox module SAM-M8Q, NEO-M8P, etc
Example2: Parse NMEA sentences using MicroNMEA library. This example also demonstrates how to
overwrite the processNMEA function so that you can direct the incoming NMEA characters from the Ublox
module to any library, display, radio, etc that you prefer.
Example3: Get latitude, longitude, altitude, and satellites in view (SIV). This example also demonstrates
how to turn off NMEA messages being sent out of the I C port. You’ll still see NMEA on UART1 and USB,
but not on I C. Using only UBX binary messages helps reduce I C traffic and is a much lighter weight
protocol.
Example4: Displays what type of a fix you have the two most common being none and a full 3D fix. This
sketch also shows how to find out if you have an RTK fix and what type (floating vs. fixed).
Example5: Shows how to get the current speed, heading, and dilution of precision.
Example6: Demonstrates how to increase the output rate from the default 1 per second to many per
second; up to 30Hz on some modules!
Example7: Older modules like the SAM-M8Q utilize an older protocol (version 18) whereas the newer
modules like the ZED-F9P depricate some commands using the latest protocol (version 27). This sketch
shows how to query the module to get the protocol version.
Example8: Ublox modules use I C address 0x42 but this is configurable via software. This sketch will allow
you to change the module’s I C address.
Example9: Altitude is not a simple measurement. This sketch shows how to get both the ellipsoid based
altitude and the MSL (mean sea level) based altitude readings.
Example10: Sometimes you just need to do a hard reset of the hardware. This sketch shows how to set
your Ublox module back to factory default settings.
NEO-M8P
NEO-M8P Example1: Send UBX binary commands to enable RTCM sentences on U-blox NEO-
M8P-2 module. This example is one of the steps required to setup the NEO-M8P as a base station.
For more information have a look at the Ublox manual for setting up an RTK link.
NEO-M8P Example2: This example extends the previous example sending all the commands to the
NEO-M8P-2 to have it operate as a base. Additionally the processRTCM function is exposed. This
allows the user to overwrite the function to direct the RTCM bytes to whatever connection the user
would like (radio, serial, etc).
2
2
2
2 2
2
2

NEO-M8P Example3: This is the same example as NEO-M8P's Example2. However, the data is sent
to a serial LCD via I C.
ZED-F9P
ZED-F9P Example1: This module is capable of high precision solutions. This sketch shows how to
inspect the accuracy of the solution. It’s fun to watch our location accuracy drop into the millimeter
scale.
ZED-F9P Example2: The ZED-F9P uses a new Ublox configuration system of
VALGET/VALSET/VALDEL. This sketch demonstrates the basics of these methods.
ZED-F9P Example3: Setting up the ZED-F9P as a base station and outputting RTCM data.
ZED-F9P Example4: This is the same example as ZED-F9P's Example3. However, the data is sent
to a serial LCD via I C.
This SparkFun Ublox library really focuses on I C because it's faster than serial and supports daisy-chaining. The
library also uses the UBX protocol because it requires far less overhead than NMEA parsing and does not have
the precision limitations that NMEA has.
Setting the ZED-F9P as a Correction Source
If you’re located further than 20km from a correction station you can create your own station using the ZED-F9P.
Ublox provides a setup guide within the ZED-F9P Integration Manual showing the various settings needed via U-
Center. We’ll be covering how to setup the ZED-F9P using I C commands only. This will enable a headless
(computerless) configuration of a base station that outputs RTCM correction data.
Before getting started we recommend you configure the module using U-Center. Checkout our tutorial on using U-
Center then read section 3.5.8 Base Station Configuration of the Ublox Integration Manual for getting the ZED-
F9P configured for RTK using U-Center. Once you’ve been successful controlling the module in the comfort of
your lab using U-Center, then consider heading outdoors.
For this exercise we’ll be using the following parts:
1x SparkFun GPS-RTK2 Board or RTK-SMA Board
1x U.FL to SMA Cable for the RTK2
1x SparkFun BlackBoard makes I C easy
1x USB C 2.0 Cable if you need one
1x Two Qwiic Cables
1x 20x4 SerLCD with Qwiic Adapter soldered on
1x Antenna GNSS 3-5V Magnetic Mount
1x GPS Antenna Ground Plate
1x 20+ft SMA extension can be handy when first experimenting with base stations so you can sit indoors
with a laptop and analyze the output of the GPS-RTK
1x A standard camera tripod
The ZED-F9P can be configured using Serial, SPI, or I C. We’re fans of the daisy chain-ability of I C so we’ll be
focusing on the Qwiic system. For this exercise we’ll be connecting the an LCD and GPS-RTK2 to a BlackBoard
using two Qwiic cables. You can also use the RTK-SMA as an alternative.
2
2
2
2
2
2 2
For the antenna, you’ll need a clear view of the sky. The better your antenna position the better your accuracy and
performance of the system. We designed the GPS Antenna Ground Plate to make this setup easy. The plate has a
¼” threaded hole that threads directly onto a camera tripod. The plate thickness was chosen to be thick enough so
that the threaded screw is flush with the plate so it won’t interfere with the antenna. Not sure why we’re using a
ground plate? Read the Ublox white paper on using low-cost GNSS antennas with RTK. Mount your magnetic
mount antenna and run the SMA cable to the U.FL to SMA cable to the GPS-RTK2 board. If you have the RTK-
SMA, you just need to run the SMA cable to the board's connector.
There are only three steps to initiating a base station:
Enable Survey-In mode for 1 minute (60 seconds)
Enable RTCM output messages
Being Transmitting the RTCM packets over the backhaul of choice
Be sure to grab the SparkFun Arduino Library for Ublox. You can easily install this via the library manager by
searching ‘SparkFun Ublox’. Once installed click on File -> Examples -> SparkFun_Ublox_Arduino_Library.
The ZED-F9P subfolder houses a handful of sketches specific to its setup. Example3 of the library demonstrates
how to send the various commands to the ZED-F9P to enable Survey-In mode. Let’s discuss the important bits of
code.

response = myGPS.enableSurveyMode(60, 5.000); //Enable Survey in, 60 seconds, 5.0m
The library is capable of sending UBX binary commands with all necessary headers, packet length, and CRC
bytes over I C. The enableSurveyMode(minimumTime, minimumRadius) command does all the hard work to tell the
module to go into survey mode. The module will begin to record lock data and calculate a 3D standard deviation.
The survey-in process ends when both the minimum time and minimum radius are achieved. Ublox recommends
60 seconds and a radius of 5m. With a clear view of the sky, with a low cost GNSS antenna mounted to a ground
plate we’ve seen the survey complete at 61 seconds with a radius of around 1.5m.
response &= myGPS.enableRTCMmessage(UBX_RTCM_1005, COM_PORT_I2C, 1); //Enable message 1005 to ou
tput through I2C port, message every second
response &= myGPS.enableRTCMmessage(UBX_RTCM_1074, COM_PORT_I2C, 1);
response &= myGPS.enableRTCMmessage(UBX_RTCM_1084, COM_PORT_I2C, 1);
response &= myGPS.enableRTCMmessage(UBX_RTCM_1094, COM_PORT_I2C, 1);
response &= myGPS.enableRTCMmessage(UBX_RTCM_1124, COM_PORT_I2C, 1);
response &= myGPS.enableRTCMmessage(UBX_RTCM_1230, COM_PORT_I2C, 10); //Enable message every 10
seconds
These six lines enable the six RTCM output messages needed for a second ZED-F9P to receive correction data.
Once these sentences have been enabled (and assuming a survey process is complete) the ZED-F9P base
module will begin outputting RTCM data every second after the NMEA sentences (the RTCM_1230 sentence will
be output once every 10 seconds). You can view an example of what this output looks like here.
The size of the RTCM correction data varies but in general it is approximately 2000 bytes every second (~2500
bytes every 10th second when 1230 is transmitted).
//This function gets called from the SparkFun Ublox Arduino Library.
//As each RTCM byte comes in you can specify what to do with it
//Useful for passing the RTCM correction data to a radio, Ntrip broadcaster, etc.
void SFE_UBLOX_GPS::processRTCM(uint8_t incoming)
{
//Let's just pretty-print the HEX values for now
if (myGPS.rtcmFrameCounter % 16 == 0) Serial.println();
Serial.print(" ");
if (incoming < 0x10) Serial.print("0");
Serial.print(incoming, HEX);
}
If you have a ‘rover’ in the field in need of correction data you’ll need to get the RTCM bytes to the rover. The
SparkFun Ublox library automatically detects the difference between NMEA sentences and RTCM data. The
processRTCM() function allows you to ‘pipe’ just the RTCM correction data to the channel of your choice. Once the
base station has completed the survey and has the RTCM messages enabled, your custom processRTCM()
function can pass each byte to any number of channels:
A wireless system such as LoRa or Cellular
Posting the bytes over the internet using WiFi or wired ethernet over an Ntrip caster
Over a wired solution such as RS485
The power of the processRTCM() function is that it doesn’t care; it presents the user with the incoming byte and is
agnostic about the back channel.
2

Heads up! We’ve been experimenting with various LoRa solutions and the bandwidth needed for the best
RTCM (~500 bytes per second) is right at the usable byte limit for many LoRa setups. It’s possible but you
may need to adjust your LoRa settings to reach the throughput necessary for RTK.
What about configuring the rover? Ublox designed the ZED-F9P to automatically go into RTK mode once RTCM
data is detected on any of the ports. Simply push the RTCM bytes from your back channel into one of the ports
(UART, SPI, I C) on the rover's ZED-F9P and the location accuracy will go from meters to centimeters. The rover's
NMEA messages will contain the improved Lat/Long data and you'll know where you are with mind-bending
accuracy. It’s a lot of fun to watch!
Can I Really Use NMEA with a High Precision GPS Receiver?
Yes! Except that NMEA sentences are right on the edge of enough precision. NMEA sentences look something
like this:
$GNGGA,012911.00,4003.19080,N,10416.95542,W,1,12,0.75,1647.1,M,-21.3,M,,*4F
NMEA outputs coordinates in the ddmm.mmmmm format. So what is the weight of the least significant digit? Said
differently, what is the impact of one digit change?
104 16.95542
vs
104 16.95543
If we know 1 degree of latitude is 111.3km at the equator, we can glean the change of a fraction of a minute:
1 degree = 60 minutes
1 minute = 1 degree/60 = 111.32km / 60 = 1.855km
1 minute = 1855m
0.1min = 185.5m
0.01min = 18.55m
0.001min = 1.855m
0.0001min = .1855m = 185.5mm
0.00001min = 0.0185m = 18.55mm = 1.855cm
Using the NMEA sentence, the ZED-F9P will only be able to communicate a change of ~1.5cm location change for
each digit in the 5th position. This is pretty close to the 1.0cm accuracy of the module. If you want additional
precision, you should consider using the UBX protocol which can output up to 8 digits of precision in dd.dddddddd
format which will get you down to 1.11mm of precision! Be sure to checkout the examples in the SparkFun Ublox
Arduino Library. We have various examples outputting the full 8 digits of precision over I C without the burden of
parsing NMEA sentences.
Resources and Going Further
2
2
Have fun with your new found super power: sub decimeter grade GPS! For more on the GPS-RTK2 and RTK-
SMA, check out the links below:
SparkFun GPS-RTK2
Schematic (PDF)
Eagle Files (ZIP)
Board Dimensions
SparkFun GPS-RTK-SMA
Schematic (PDF)
Eagle Files (ZIP)
Board Dimensions
ZED-F9P Datasheet (PDF)
ZED-F9P UBX and NMEA Protocol Manual
ZED-F9P Integration Manual including setting up the module for base station using u-center
ZED-F9P Product Summary
ZED-F9P FW1.00 Release Notes
U-blox ECCN notice
Example RTCM output from the ZED-F9P
GitHub
Arduino Library
Ready to get hands-on with GPS?
We've got a page just for you! We'll walk you through the basics of how GPS
works, the hardware needed, and project tutorials to get you started.
TAKE ME THERE!
I.
I.
Product Repo
GPS-RTK2
GPS-RTK-SMA
SFE Product Showcase
Need some inspiration? Check out some of these related tutorials:
Building an Autonomous Vehicle: The Batmobile
Documenting a six-month project to race autonomous
Power Wheels at the SparkFun Autonomous Vehicle
Competition (AVC) in 2016.
What is GPS RTK?
Learn about the latest generation of GPS and GNSS
receivers to get 2.5cm positional accuracy!
GPS-RTK Hookup Guide
Find out where you are! Use this easy hook-up guide to
get up and running with the SparkFun high precision
GPS-RTK NEO-M8P-2 breakout board.
Getting Started with U-Center for u-blox
Learn the tips and tricks to use the u-blox software tool
to configure your GPS receiver.
Products related to this Datasheet
GPS-RTK2 BOARD - ZED-F9P (QWIIC)