Micro:Climate Kit Experiment Guide Datasheet by SparkFun Electronics
View All Related Products | Download PDF Datasheet
Page 1 of36
micro:climate Kit Experiment Guide
micro:climate Kit Experiment Guide
Introduction to the Micro:Climate Kit
Introduction
We have seen a huge amount of excitement from hobbyists, students and
scientists around building a DIY weather station to track what is going on
around us on Planet Earth on a daily basis.
We have seen just as much excitement around the BBC’s newly released
micro:bit, which made its debut in the United Kingdom and is now available
in the United States through SparkFun.
And then it dawned on us…why not combine the two? So, here it is: a
weather station kit that is built on top of the inexpensive, easy-to-use
micro:bit and Microsoft MakeCode. We have also written seven
experiments that walk you through how to use each and every component
of the kit and how to use them with the micro:bit and Microsoft MakeCode.
What’s Included in the Kit?
Below is all the parts included in the SparkFun micro:climate kit.
The kit comes with everything you need to build a fully featured weather
station for the micro:bit. All you need to supply is, well, the micro:bit!
SparkFun micro:climate kit
KIT-14217
Page 1 of 3
6
Page 2 of36
The kit includes the following parts:
•SparkFun weather:bit — The carrier board for the micro:bit and the
central component to building a weather station
•Weather Meter — Wind speed, direction and rain gauge that
connects to the SparkFun weather:bit
•SparkFun Soil Moisture Sensor — A simple probe for measuring
soil moisture
•Waterproof Temperature Sensor — Waterproof temperature
sensor with a long wire
•SparkFun OpenLog — A small widget that logs any data sent to it
over a serial connection to a microSD card
•10-Pack of M/M 12" Jumper Wires — Jumper wires for connecting
things
•SparkFun Screwdriver — Great for tightening screws and screw
terminals
How to Use This Guide
Please note that this guide is designed to get you started with the
weather:bit board and the SparkFun micro:climate kit in a simple,
straightforward way. We demonstrate each component’s functionality and
the corresponding code to make it work.
While you explore this guide, we urge you to take your time and tinker with
the sensors, code and ideas shared to build something tailored to your
application. Our goal is to get you enough information and know-how to
make you dangerous and then release you into the wild, weather station in
hand, to do whatever you do with a weather station.
Be sure to share your projects with us via Twitter or Facebook! We are
excited to see you get creative and Start Something!
Suggested Reading
Before continuing with this guide, we recommend you be somewhat familiar
with the concepts in the following tutorials:
micro:bit Board
DEV-14208
Page 2 of 3
6
Page 3 of36
Open Source!
All of our experiments and guides are licensed under the Creative
Commons Attribution Share-Alike 4.0 Unported License. Feel free to remix
and reuse our work. But please, share the love and give us attribution for
our hard work!
To view a copy of this license visit this link, or write: Creative Commons,
171 Second Street, Suite 300, San Francisco, CA 94105, USA.
About the weather:bit
The weather:bit is a carrier board for the micro:bit. Similar to an Arduino
shield, it is designed to add functionality to the micro:bit without the hassle
of a number of other boards, components and all of those jumper wires.
In this case, the weather:bit takes your normal run-of-the-mill micro:bit and
turns it into a full-blown weather station with a few extra parts, which you
can use to measure the following:
• Air Temperature
• Relative Humidity
• Barometric Pressure
• Wind Speed
• Wind Direction
• Rain Fall
What is a Circuit
?
Every electrical project starts with a
circuit. Don't know what a circuit is?
We're here to help.
Getting Started with the
micro:bit
The micro:bit is a compact, powerful
programming tool that requires no
software installation. Read on to
learn how to use it YOUR way!
SparkFun weather:bit
DEV-14214
Page 3 of 3
6
Page 4 0f36
11wm~:=m-w. \ '\ mm \'
• Soil Moisture
• Soil Temperature
Phewwwww! That is a lot of data for such a tiny computer! Let’s take a
closer look at this board and check it out for ourselves.
Edge Connector
The weather:bit connects to the micro:bit via an edge pin connector. This
makes it handy to swap out micro:bits for programming, but also gives
reliable connections to all of the different pins on the micro:bit.
BME280 Barometric Pressure Sensor
The weather:bit has a BME280 barometric pressure sensor onboard, which
can measure air temperature, humidity, barometric pressure and altitude. It
communicates with the micro:bit via I C, and the data from this sensor is
easily accessible using the SparkFun weather:bit package for MakeCode.
Weather Meter Sockets
There are two RJ11 jacks at the bottom of the weather:bit. These are used
to connect our weather meters to the weather:bit.
2
Page 4 of 3
6
Page 5 of36
O
‘I‘I'I‘I*1':*;‘»v:“m i mm
' ' 11:.
‘ - 'Pnn
These meters enable you to measure the wind speed and direction, as well
as rain fall.
Again, these are easily accessible in MakeCode via our SparkFun
weather:bit package.
Soil Moisture and Temperature
Between the two RJ11 jacks are two sets of screw terminals sets.
The one on the left is used to hook up a soil moisture sensor. You can use
either longer jumper wires or wires cut to whatever length works for your
project.
Page 5 of 3
6
Page 6 0f36
‘1‘i‘i‘2‘ will‘uhimii
wwmimli
inn 0
L
—.a‘ _ nnxs My:
_ ‘l‘i‘i‘E‘M"ill‘ummi1
The set on the right is the soil temperature sensor. It is set up to use our
waterproof temperature sensor. This sensors wire is rather long and is
great for monitoring the temperature of the soil in your garden so that you
know the exact moment the ground is ready for planting those tomatoes!
Serial Port
We have populated the serial port pins with a standard FTDI format to
make it easy for you to plug in a serial widget of your choice, such as an
OpenLog or Serial LCD display, or to just monitor data through an FTDI
breakout and USB cable.
IC Port
2
Page 6 of 3
6
a Gun:
Images
0 Pin
a;— Serial
l Cumml
0 Add Package
u...“
Page 7 0f36
For those of you who are more adventurous and demand a way to hook up
other sensors of your choice, we have added an I C port that can be
soldered to directly — or you can add headers for plug-and-play use of your
I C sensors and actuators.
Installing the weather:bit Package in
MakeCode
To make the most out of the weather:bit with the least amount of coding,
use the MakeCode package we wrote for the weather:bit board.
Packages?
If you have used Arduino before, you probably know about a thing called a
library; which is a collection of code that extends the functionality of the
core programming language. MakeCode packages work the same way.
There are some amazing differences between Arduino libraries and
MakeCode packages. One of them is that MakeCode packages include
JavaScript functions, which you can use when programming in text, as well
as all of the blocks you need to program using the block method. This
makes learning and using new packages straightforward and shortens the
time to awesome when setting out to build the project of your dreams.
Installing a MakeCode Package
To install or add a new package to your MakeCode toolbox (the list of
different block groups), click on “Advanced” and then on “Add Package.”
From here you can search for “SparkFun weather-bit,” and it should show
up as a public package in the list. Go ahead and click on it.
2
2
Page 7 of 3
6
Page 8 of36
C
22 Logic
E Vanab‘es
E Ma‘h
v Weathcrbit
A Advanced
55 Arrays
This will add all of the blocks to your toolbox. In general, this is a bit tricky
as, depending on how the package was written, it may either have its own
toolbox or just add blocks to the existing ones. Take a look at your toolbox;
for the weather:bit you should see…
Great! You have now installed the weather:bit package and are ready to
use the board as well as the components that come in the micro:climate kit.
As a side note, for every new MakeCode project that you make, you will
have to load packages over again. Not a big deal, but noteworthy! Now,
let’s put this package to good use!
Experiment 1: Reading the
Temperature, Humidity and Pressure
Introduction
What comes to mind first when you hear the term “Atmospheric
Conditions”? Well, other than the weatherman on the news, you probably
think about temperature — maybe humidity and even barometric pressure if
you are a weather nerd like many of us at SparkFun. In this first experiment
we will explore measuring those conditions using a micro:bit and the
weather:bit carrier board.
Parts Needed
•1x micro:bit board (Not included)
•1x weather:bit carrier board
•1x micro-B USB cable (Not included)
micro:bit Board
DEV-14208
USB Micro-B Cable - 6"
CAB-13244
Page 8 of 3
6
Page 9 0f36
wwwm’.1,.“
Suggested Reading
• Getting Started with the micro:bit — Basic hookup and programming
of the micro:bit
Introduction to the BME280
The BME280 Atmospheric Sensor is an easy way to measure aspects of
the atmosphere around you, including pressure, humidity and air
temperature. All of this is combined into a petite package that resides on
the weather:bit.
The sensor operates on 3.3V and is super power-efficient, using as little as
5µA (that’s 1/1,000,000 of an amp!) when idling and less than 1mA when
it’s taking measurements. This means you can operate the board on a
battery, with little thought to major power issues.
In this experiment, you will work with the BME280 to read the temperature,
pressure, and humidity of the room as well as your altitude based off of the
atmospheric pressure.
Hardware Hookup
Since the BME280 is already on the weather:bit board, this should be pretty
straightforward; you have one step in hooking everything up. Insert the
micro:bit into the weather:bit carrier board with the LED array facing up as
shown in the image below.
SparkFun weather:bit
DEV-14214
Page 9 of 3
6
Page 10 of36
b Simu‘ator I: B‘ocks (2» JavaScnpt M
\oacmg project
3.,
Download
Note: The edge connector for the micro:bit is not keyed, so there is
the potential for the micro:bit to be inserted backward. Be sure to
check the orientation of the board and micro:bit before plugging it in!
Running Your Script
We are going to use Microsoft MakeCode to program the micro:bit. Please
open a browser window and navigate to https://makecode.microbit.org. This
should open the MakeCode environment that you used to install the
weather:bit package.
Be sure to add the weather:bit package as instructed in the Installing the
weather:bit Package in MakeCode section of this tutorial.
Now, you can either download the following example script and drag and
drop it onto your micro:bit, or use it as an example and build it from scratch
in MakeCode.
Note: If this is your first time programming a micro:bit, please be sure
to see our Getting Started with the micro:bit tutorial on how to get the
MakeCode program onto your micro:bit.
Code to Note
Download
Page 10 of 3
6
Page 11 of36
Start Weather Monitoring
When the script starts, we use this block to start or initiate the BME280
sensor and get it ready to take readings. Anytime you want to use the
temperature, humidity, pressure or altitude blocks, you need to have this
block in your on start block.
Set Item To
We use a variable called item to keep track of which data are being
displayed on the LED array. If item is equal to 0, it shows the temperature;
if 1, it shows the humidity; if 2, the pressure. If the variable goes over 2, we
reset it to 0. We increment the variable by pressing the A button.
Temperature (°C)
This variable returns a number that you then have to divide by 100 to get
the temperature in Celsius.
Humidity
This variable returns a number that you need to divide by 1,024 to get the
relative humidity.
Pressure
This variable returns a number that you divide by 25,600 to get the
atmospheric pressure in hPa.
Why All of the Math?
This is a good question! It all comes down to accuracy of the data that you
receive. MakeCode cannot handle floating point numbers (numbers with
decimal points) yet. Which can be troublesome for getting really accurate
readings from the BME280 with a single variable block. So, to as accurate
of values as possible you have to do some math in the programming
environment. We know, not fun! But, hey now you might pay attention in
math class a bit more now.
What You Should See
Once your code is loaded, you should start to see numbers scroll across
the LED array on your micro:bit, beginning with the temperature in Celsius.
If you press the left button on your micro:bit, the number will change to
percent humidity; press it again, and it will be pressure. Pretty cool…well,
hmmm…maybe warm?
Page 11 of 3
6
Page 12 of36
Troubleshooting
•weather:bit blocks not showing up — Make sure you have a
network connection and have added the package to your MakeCode
environment.
•micro:bit not showing up — Try unplugging the USB cable and
plugging it back in. Also, be sure that you have the cable inserted all
the way into your micro:bit.
•atmospheric data seems odd — Make sure that the BME280 is
free from contact with sources of heat and/or moisture (for example,
having your finger over the top of it).
Experiment 2: Reading the Light Level
Introduction
Light conditions are a huge part of the weather. The great thing is that the
weather:bit doesn’t have a light sensor. No, we didn’t miss a typo! The
weather:bit doesn’t have a light sensor. Why not? Because the micro:bit
has one already! In this experiment you will measure the light around you
and have the micro:bit “graph” it
Parts Needed
For this experiment you actually don’t need the weather:bit carrier board, so
we left it out. But feel free to leave it attached to your micro:bit if you so
choose.
•1x micro:bit board (Not included)
•1x micro-B USB cable (Not included)
micro:climate kit: Exp1
Page 1
2
of 3
6
I)
V SImu‘ator ('y Javascnm B‘
>800)X
\oadmg
I! i. > ‘
Nmoso Efods WownlcadMA
m (9 [mm level
0 mm bar- gmph or
up to 255
L
Page 13 of36
Suggested Reading
• Using LEDs as Light Sensors — That’s correct! You can use LEDs
as light sensors. In fact, that is how the micro:bit does it.
Hardware Hookup
Again, the hardware hookup here is minimal! Plug your micro:bit into your
computer with the USB cable, and you are good to go!
Running Your Script
Please open a browser window and navigate to makecode.microbit.org.
This should open the MakeCode environment that you used to install the
weather:bit package.
Code to Note
Set lightVal To
We read the light level in the area using the light level block and store it
in a variable called lightVal . This is the value that we can compare
against the calibration value you captured at the beginning of your script.
micro:bit Board
DEV-14208
USB Micro-B Cable - 6
"
CAB-13244
Download
Blocks
Page 1
3
of 3
6
Page 14 of36
Plot Bar Graph Of
This block is fun! It accepts two values: the value of what you want to graph
and a maximum value of that variable. In this case we want to graph
lightVal , and it has a maximum value of 255 . This will create a “bar
graph” of the light value on your micro:bit.
What You Should See
You should see the LED array light up as a graph based on how bright it is
wherever you are. Turn out the lights or pass your hand over the array, and
the graph should react. Pretty sweet! You now have a way to measure the
light value as well as another way to display data with the micro:bit.
Troubleshooting
•odd light readings — Make sure you are not leaning over the
micro:bit, your shadow will impact the sensor reading.
•The arrows threshold is odd — Try resetting the micro:bit while you
are not leaning over it or casting a shadow on it.
Experiment 3: Reading the Soil
Moisture
Introduction
How wet is the ground? It is actually an important question to ask if you are
thinking about growing plants, digging a hole, or even walking across your
yard. Enter the soil moisture sensor. In this experiment you will hook up the
soil moisture sensor and use it. You will display different images on your
micro:bit based on the moisture level of the soil.
Parts Needed
•1x micro:bit board (Not included)
•1x weather:bit carrier board
•1x micro-B USB cable (Not included)
•3x 12" M/M jumper wires
micro:climate kit: Exp2
Page 1
4
of 3
6
Page 15 of36
DEVVNZOE
01543244 osvrvam
•1x SparkFun Soil Moisture Sensor
Suggested Reading
• Soil Moisture Sensor Hookup Guide — How does the moisture
sensor work?
• Voltage Dividers — The moisture sensor works as a voltage divider.
Dig in and see what makes it tick!
About the Moisture Sensor
micro:bit Board
DEV-14208
SparkFun Soil Moisture
Sensor
SEN-13322
USB Micro-B Cable - 6"
CAB-13244
SparkFun weather:bit
DEV-14214
Jumper Wires Premium 12"
M/M Pack of 10
PRT-09387
Page 1
5
of 3
6
Page 16 of 36
The SparkFun Soil Moisture Sensor is a simple breakout board for
measuring the moisture in soil and similar materials. The soil moisture
sensor is straightforward to use. The two large, exposed pads function as
probes for the sensor, together acting as a variable resistor. The more
water that is in the soil, the better the conductivity between the pads will be,
which will result in a lower resistance and a higher SIG (output voltage).
To get the SparkFun Soil Moisture Sensor functioning with your weather:bit,
all you need to do is connect the VCC, GND and SIG pins to the
weather:bits VCC, GND and SIG screw terminals. You will receive a SIG
out, which will depend on the amount of water in the soil. Oh, and you’ll
also need a bit of dirt in a pot to test it all out!
One commonly known issue with soil moisture sensors is their short life
span when exposed to a moist environment. To combat this, we’ve had the
PCB coated in gold finishing (ENIG, or Electroless Nickel Immersion Gold).
Hardware Hookup
Hooking the moisture sensor up to the weather:bit is relatively easy. You
will need a screwdriver with a small bit, preferably a jeweler’s screwdriver or
our pocket screwdriver.
Pocket Screwdriver Set
TOL-12891
Page 1
6
of 3
6
I)
y Simmamr 1-. mocks () JavaSmipv
VCIWX
Ioading project
0 i V &
chvosoflMgfikleCods TeDQWfllGadm/am
W.‘
Page 17 of36
Start by using the screwdriver to open the three screw terminals on the
moisture sensor enough that you can insert the ends of the jumper wires
into them. Next, insert three jumper wires into the screw terminals using
Red for VCC, Black for GND and Yellow for SIG. Tighten the screws down
so that the wires will not come loose.
Next, do the same thing for the screw terminals for the moisture sensor port
on the weather:bit. Open the screws enough that you can insert the jumper
wires with Red to VCC, Black to GND and Yellow to SIG. Tighten the
screws enough to hold the wires in place.
With that, you are done hooking the moisture sensor up!
Running Your Script
Please open a browser window and navigate to
https://makecode.microbit.org. This should open the MakeCode
environment that you used to install the weather:bit package.
Code to Note
Download
Page 1
7
of 3
6
cm sum
.vezmm mamtuv‘wg
g5 furmcr
show \(nn D
show mm D
Page 18 0f36
Soil Moisture
The Soil Moisture block returns an analog value range of 0 - 1023 (a 10
bit number). The lower the number is the less moisture the sensor detects.
The “dryness” and “wetness” level depends on your climate, humidity, etc.
so we cannot give you a concrete range of what is wet and dry, that is
something you will have to fiddle with yourself.
If / Else If / Else
We used an if then block to create some logic that changes based on the
soil moisture detected by the sensor. If the moisture value is low the LED
array shows an angry face, if just right a smiley face and if too wet and
frown.
To add more else / else if options to your if statement click on the small
gear and build your state tree using the block interface presented.
Show Icon
The Show Icon block is really useful when you want to display a simple
image or icon on the LED array. You can select from a number of premade
images from the pull down menu in the block.
What You Should See
Based on our extensive testing (me pouring water into a pot of soil with the
sensor stuck in it), we defined dry, damp and wet states. The image below
shows the experiment powered up to test the plant’s soil.
When you insert your sensor into a potted plant of your own and run your
script, you will see an icon show up on your micro:bit. If you get an angry
face, your soil is too dry; a sad face means it is too wet; and finally, a happy
face is “moist” and just right. Water as needed to keep your plants “happy.”
Page 18 of 3
6
Page 19 of36
$31
You may need to adjust the numbers in your code to match the state of
preference for your house plants!
Troubleshooting
•Odd readings — Make sure your wiring is correct, if you wire the
sensor backwards it will give backwards results.
•I never get a “happy” face — Try playing around with the threshold
values in your if statements to find a range that works for your
application.
•It still doesn’t work — Drop us a line, we would love to help you
figure it out!
Experiment 4: Reading the Soil
Temperature
Introduction
When you are looking to put plants in the ground in spring, plant seed, or
even track the temperature of your koi pond, you need a temperature
sensor. But not just any temperature sensor…a waterproof one! In this
experiment you will explore using the waterproof temperature sensor to
measure ground temperature in a garden or pot.
Parts Needed
•1x micro:bit board (Not included)
•1x weather:bit carrier board
•1x micro-B USB cable (Not included)
•1x Waterproof Temperature Sensor
micro:climate kit: Exp3
Page 1
9
of 3
6
Page 20 of 36
Suggested Reading
• Temperature Sensor Datasheet - The nitty gritty details on the water
proof temperature sensor
• Simple Sketch Video - Video demonstrating the use with Arduino
Hardware Hookup
The hookup of this sensor is much easier with the weather:bit carrier board
than with any other microcontroller. We have done a lot of the leg work for
you!
Find the screw terminals for the soil temperature on the weather:bit. Using
your screwdriver, open the screw terminals a bit and insert the wires as
shown in the photo below with the wires from left to right:
• Red to VCC
• White to SIG
•Black to GND
Running Your Script
Temperature Sensor -
Waterproof (DS18B20)
SEN-11050
micro:bit Board
DEV-14208
USB Micro-B Cable - 6"
CAB-13244
SparkFun weather:bit
DEV-14214
Page 20 of 3
6
Page 21 0f36
p slmu‘alor t E‘ocks () Javascrlpl D"
FCIWX
foading project
a 1. > .t
chvasoflMgheCode TEDQWIIlGadru/aq
Please open a browser window and navigate to
https://makecode.microbit.org. This should open the MakeCode
environment that you used to install the weather:bit package.
Code to Note
Soil Temperature
The Soil Temperature block returns the soil a value that you need to
divide by 100 to get the temperature in Celcius. Like the data from the
BME280 sensor in Experiment 1, this is to get you the most accurate
temperature possible.
Set Item To
In this Set Item To block we use a boolean variable of true . You can
then flip flop that variables to false when needed
Not
We use the not block to flip flop a boolean variable when needed. In this
case when a button is pressed.
Show String
The Show String Block enables you to display a scrolling string of
character across the LED array.
Show Number
As in previous experiments we use the show number block to display the
temperature data from the soil temperature sensor.
What You Should See
As soon as you power up your micro:bit, you should see the ground
temperature from the temperature sensor scrolling across the LED array in
Celcius. If you press the A button, it will change what is scrolling to a “Plant”
or “Don’t Plant” depending on the temperature of the ground making it a
useful tool for when to figure out when it is time to plant your tomato crop.
Download
Page 21 of 3
6
Page 22 of 36
Note: The actual temperature sensor is at the end of the long wire.
Make sure that is in place where you want to take temperature
readings; otherwise you may get odd values.
Troubleshooting
•Odd temperature — Make sure you are measuring with the end of
the temperature sensor, that is where the actual sensor is.
•Really odd temperature — Double check your wiring and hookup!
•Numbers still seem odd — Check your math blocks! You may be
missing an order of operation.
Experiment 5: Reading the Wind
Direction and Speed
Introduction
The winds are a-blowin'! The question is, which direction and how hard? In
this experiment you will assemble, hook up and program your weather:bit to
read the weather meters — more specifically, the wind anemometer (wind
speed) and directional vane. We will again use the micro:bit’s LED array to
display the wind speed or the direction.
Parts Needed
•1x micro:bit board (Not included)
•1x weather:bit carrier board
•1x micro-B USB cable (Not included)
•1x Weather Meter
micro:climate kit: Exp4
Page 2
2
of 3
6
Page 23 of 36
Suggested Reading
• Reed Switch — A tutorial about how a reed switch works.
• Weather Meter Datasheet — The nitty-gritty details on the weather
meter.
Introducing the Weather Meter (Anemometer and Vane)
The anemometer on the weather meter is the propeller-looking thing that
got lost in a ping-pong ball factory.
It has three cups that catch the wind, which then cause it to spin. As the
head spins, a magnet at the center of the hub travels over a reed switch
that closes the circuit to the pin that the sensor is connected to for a brief
moment. The faster the wind is, the faster the anemometer spins and the
faster and more often the reed switch is triggered.
We count the number of times that the reed switch is triggered every
second, and we can calculate the wind speed from that (1 click per second
is roughly 1.5mph).
We did the hard work on this one in terms of simplifying all of this for you.
All you need to know is that an anemometer is a wind-speed sensor.
The wind vane is the arrow-looking thing that spins.
Weather Meters
SEN-08942
micro:bit Board
DEV-14208
USB Micro-B Cable - 6"
CAB-13244
SparkFun weather:bit
DEV-14214
Page 2
3
of 3
6
Page 24 of 36
When the wind blows, it catches the vane, which points in the direction that
the wind is coming from. As the vane moves around, it closes a series of
switches inside, which produce a different resistance at 16 different
locations around the hub. Each direction has a specific value that we have
mapped to the cardinal directions once you have it set in the location you
want it. In the makeCode package the Wind Direction block will return
N,NE,E,SE,S,SW,W,NE directions as a string.
Hardware Hookup
To help you out in the assembly of your weather meter we have created
this step by step assembly guide.
Note: Once you have assembled your weather meter we highly
recommend labeling the two cables for the wind and rain sensors. This
will make your life much easier in the long run!
Once you have completed the assembly of the weather meter, find the
cable for the wind sensors and plug it into the RJ-11 connector on the
weather:bit labeled “wind”.
Weather Meter Hookup Guid
e
J
ULY 20, 201
7
How to assemble your very own weather meter!
Page 2
4
of 3
6
Page 25 of 36
p slmwalor t E‘ocks () Javascrlpl D"
FCIWX
Foading project.
a 1. > .t
chvosoflMgheCode Tewwllleadnvaq
With that you are ready to roll!
Running Your Script
Please open a browser window and navigate to
https://makecode.microbit.org/. This should open the MakeCode
environment that you used to install the weather:bit package in.
Code to Note
Start Wind Monitoring
The Start Wind Monitoring block starts all of the necessary processes to
use the wind sensors that plug into the weather:bit. This block show be
placed in the On Start block as it only needs to be called once at the very
beginning of the program.
Show Number
The Show Number block displays/scrolls whatever number is placed inside
of it across the LED array. We use it to display the wind speed in this
example.
Wind Speed
The Wind Speed block is a variable block that returns the calculated wind
speed from the anemometer. It is updated every 2 seconds!
Show String
The Show String block is similar to the Show Number block in that it
displays/scrolls whatever string that it is passed. In this case we use it to
display the wind direction.
Wind Direction
Last but not least, the Wind Direction block is a variable block that returns
a string value of a cardinal direction that the wind vane is pointing.
What You Should See
Download
Page 2
5
of 3
6
lll
Page 26 of 36
Once you power up the micro:bit, spin the anemometer with your hand or
place it in front of a fan. The speed in miles per hour should start to scroll
across the LED array. If you press the A button on your micro:bit, it will
change the readout to print the direction the vane is pointing as the
direction the wind is coming from.
Note: Be sure to set your vane so that N on the micro:bit reading is
true north for this reading to be accurate.
Troubleshooting
•odd readings — Make sure your wiring is correct, make sure the
correct sensors are plugged into the correct RJ11 jack.
•What is north? — The directions produced by the weather:bit are
based off of readings from the vane, you have to personally line up
the orientation of your vane to north.
•It still doesn’t work — Drop us a line, we would love to help you
figure it out!
Experiment 6: Reading the Rain Gauge
Introduction
Rain, rain, go away; come again another day! In this experiment you will
add the rain gauge to your weather meter and use it to track the amount of
rain that falls. In the end you will use the micro:bit to keep track of the
amount of rain, print it out over the LED array when a button is pressed and
then use another button press to reset that value to 0. Ready to get wet?
Us too…
Parts Needed
•1x micro:bit board (Not included)
•1x weather:bit carrier board
•1x micro-B USB cable (Not included)
micro:climate kit: Exp5
Page 2
6
of 3
6
Page 27 of 36
•1x Weather Meter
Suggested Reading
• Weather Meter Datasheet — The nitty-gritty details on the weather
meter.
Introducing the Weather Meter (Rain Gauge)
In the previous experiment you met the wind sensors on the weather meter.
Here you meet the rain gauge!
The rain gauge is actually quite an ingenious design. Inside of the box is a
tiny bucket. When that bucket is full (0.011" of rain) it tips over, both
triggering a switch and dumping out the water that is in the bucket, which
then allows the bucket to come back to upright. So, for every switch press
there is 0.011" of rain. In software we count these triggers and increment
the rainfall value.
Hardware Hookup
If you didn’t assembly your weather meter in the previous experiment we
created this step by step assembly guide for you to follow!
Weather Meters
SEN-08942
micro:bit Board
DEV-14208
USB Micro-B Cable - 6"
CAB-13244
SparkFun weather:bit
DEV-14214
Page 2
7
of 3
6
Page 28 of 36
b Simu‘ator 1 Blocks U JavaScrip\ 2'
>300)X
loading pvojem.
N .t ' .t
Note: Once you have assembled your weather meter we highly
recommend labeling the two cables for the wind and rain sensors. This
will make your life much easier in the long run!
Once you have completed the assembly of the weather meter, find the
cable for the rain gauge and plug it into the RJ-11 connector on the
weather:bit labeled “rain”.
Hope you have an umbrella!
Running Your Script
Please open a browser window and navigate to
https://makecode.microbit.org. This should open the MakeCode
environment that you used to install the weather:bit package.
Weather Meter Hookup Guid
e
J
ULY 20, 201
7
How to assemble your very own weather meter!
Page 28 of 3
6
Page 29 of 36
Code to Note
Start Rain Monitoring
To use the rain gauge you need to add the Start Rain Monitoring block
to your On Start Block for it to be able to function correctly. It sets up the
micro:bit hardware correctly to be able to read the rain gauge correctly.
Rain
The rain block returns the number of inches of rain that the gauge has
measured as a whole number. This variable block stores that value until
your micro:bit is reset or power cycled (turned off and on again).
Show LEDs
We used the Show LEDs block to draw an image of the sun. If MakeCode
doesn’t have just the right icon for you pre-drawn you can make your own
using this method.
Reset
The reset block resets the code that you have on your micro:bit. This is
the same as pressing the reset button on the back of the micro:bit, but at
times it is useful to be able to do this in software. A great example would be
that you couldn’t reach the back of the micro:bit for some reason.
What You Should See
Once you power up your micro:bit, you should see a sun show up on the
LED array. Once the amount of rain fallen goes over 1" the LED array will
display an umbrella and every 10 seconds the number of inches of rain fall
since you started your program.
micro:climate kit: Exp6
Page 2
9
of 3
6
Page 30 of36
To restart the counter, press the A button or, if you can reach it, the reset
button on the back of the micro:bit.
Troubleshooting
•I am getting a lot or rain? — Every time the bucket tip, it is
measured as rainfall. If you bump into the sensor or if it is vibrated it
may trigger the sensor and you get a false reading.
•Getting an Odd reading?! — Make sure the rain gauge is plugged
into the proper RJ11 jack and there is a “click” when you insert it all
the way.
•It still doesn’t work — Drop us a line, we would love to help you
figure it out!
Experiment 7: Logging to the MicroSD
Card
Introduction
We are almost done with our whirlwind series of weather experiments. In
this final experiment we will look at how to log all of this amazing weather
data to a microSD card using the OpenLog.
Parts Needed
•1x micro:bit board (Not included)
•1x weather:bit carrier board
•1x micro-B USB cable (Not included)
•1x OpenLog (with headers)
•1x microSD card (NOT INCLUDED WITH THIS KIT)
SparkFun OpenLog
DEV-13712
micro:bit Board
DEV-14208
USB Micro-B Cable - 6"
CAB-13244
SparkFun weather:bit
DEV-14214
Page 30 of 3
6
Page 31 0f36
O O O D o
OpenLoqu
RENEW“
nu,
..
..
..
..
..
”2
..
.
....
..‘
..-
GQN DXI YXO UCC EN
0
m
r.
x
Suggested Reading
• OpenLog Hookup Guide — The ups and downs of how to use the
OpenLog
Introducing the SparkFun OpenLog
The OpenLog Data Logger is a simple-to-use open source solution for
logging serial data from your projects. The OpenLog provides a simple
serial interface to log data from a project to a microSD card.
The primary interface with the OpenLog is the FTDI header on the board
edge. This header is designed to plug directly into the weather:bit carrier
board’s serial port, which allows the micro:bit to send data over a serial
connection to the OpenLog.
There are two status LEDs on the OpenLog to help you with
troubleshooting.
MicroSD Card with Adapter -
8GB
COM-11609
Page 31 of 3
6
Page 32 of 36
I :- aunmmuu I
Van-nu...“
•STAT1 — This blue indicator LED toggles on/off when a new
character is received. This LED blinks when serial communication is
functioning.
•STAT2 — This green LED is connected to Arduino D13 (SPI Serial
Clock Line/ATmega328 PB5). This LED only blinks when the SPI
interface is active. You will see it flash when the OpenLog records
512 bytes to the microSD card.
Hardware Hookup
You are going to love this! First thing is that you need to insert a microSD
card into the OpenLog with the text side “up” as shown in the image below.
Make sure the card “clicks” into place and stays in place.
Next insert the OpenLog’s pins into the serial port on the weather:bit carrier
board as shown below. Make sure that all of the pins are aligned and
inserted correctly. Offsetting these pins could end in damaging your
OpenLog or micro:bit. Finally, if you haven’t already, plug your micro:bit into
the weather:bit. With that you should be good to go!
Page 3
2
of 3
6
I)
V Simunatnr
I}.
r/maso’
1-, mm; (} JavaSnript
max
\oadmg project
' .t
kéfods “gnownlcamw
F)!
Page 33 of36
Running Your Script
Please open a browser window and navigate to
https://makecode.microbit.org. This should open the MakeCode
environment that you used to install the weather:bit package.
Code to Note
Serial Redirect To
We use the Serial Port on the weather:bit board to write data to the
SparkFun OpenLog. To do this we need to do some setup for the micro:bit
to use it correctly. We do this through the Serial Redirect To block
placed in our On Start block.
In the Serial Redirect To block we set the transmit (TX) and receive (RX)
pins. In this case we use pins 15 and 14. We also set the baud rate which is
the rate at which two devices “agree” to communicate at. The OpenLog is
preprogrammed to communicate at 9600 baud, so that is what we will set it
at.
Join
The join block is one of the most useful blocks out there. You use it to
join pieces of data together to build a long string that you then store in a
variable. For example for our header we stored comma separated names
Download
Page 3
3
of 3
6
Page 34 of 36
as a single variable called header . The join blocks standard size is 2
slots. To add more slots click on the gear button and drag more slots in
place as you have with the if / else if statements in previous experiments.
Serial Write Line
To send data to the OpenLog we use the Serial Write Line block. This
command sends whatever data you attach to it over the serial lines you
have specified in your Serial Redirect to block with a carriage return at
the end of it.
Running Time(ms)
The running time block returns the number of milliseconds that the
micro:bit has been powered up and running the current program. We are
using it as a timestamp for data logging since there is no access to a
realtime clock.
What You Should See
When you power your micro:bit, you will eventually see an “X” on the LED
array. Press the A button to start logging data every 30 seconds. A check
mark will be displayed on your LED array. Let the program run for a couple
of minutes and press the A button again. You will see an “X” again. It is now
safe to remove the microSD card from the OpenLog.
Now, using the microSD card slot on your computer or an adapter, open up
the microSD card on your computer. You should see two files. One is a
config file, which you can ignore. The other, which has a file name of
“LOGXXXXX.txt,” is what you are looking for; go ahead and open it.
The data in this text file is a Comma Separated Value (CSV) set of the data
you sent it. The format is that the first line is the “header,” which is the
name of each “column.” You see that our header is the following:
time,temperature,humidity,pressure,altitude
The header is followed by lines of values associated with each reading.
In fact, if you are a user of Google Sheets you can import this text file as a
CSV and then graph these values pretty easily. We recommend this quick
guide from Google on how to import a .txt file as a CSV into sheets.
Troubleshooting
•Doesn’t seem to be logging — Make sure your openLog is oriented
correctly in the Serial port
•The log has weird characters —Make sure you have the serial
baud rate set to 9600!
•It still doesn’t work — Drop us a line, we would love to help you
Page 3
4
of 3
6
Page 35 of36
figure it out!
Resources and Going Further
We produce a number of other kits and carrier boards that you can hook up
to your micro:bit to help take your projects to the next level. Here is some
further reading that may help you along in learning more about the world of
electronics.
For more information on our micro:bit ecosystem, check out these tutorials:
For more Internet-connected weather fun, check out our these other
weather data tutorials.
SparkFun Inventor's Kit for
micro:bit Experiment Guide
This guide contains all the
information you will need to explore
the twelve circuits of the SparkFun
Inventors Kit for micro:bit.
micro:bot Kit Experiment
Guide
Get started with the moto:bit, a
carrier board for the micro:bit that
allows you to control motors, and
create your own robot using this
experiment guide for the micro:bot
kit.
micro:arcade Kit Experiment
Guide
We love games! We love writing
games, building games and yes,
even building game consoles. So we
w
ant to introduce to you the
micro:arcade kit for the micro:bit!
micro:bit Breakout Board
Hookup Guide
How to get started with the micro:bit
breakout board.
Weather Station Wirelessly
Connected to
Wunderground
Build your own open-source, official
Wunderground weather station that
connects over WiFi via an Electric
Imp.
Photon Weather Shield
Hookup Guide V11
Create Internet-connected weather
projects with the SparkFun Weather
Shield for the Photon.
Page 3
5
of 3
6
er 5
12
1c
11
Page 36 of36
9// 7
A
rduino Weather Shield
Hookup Guide V1
2
Read humidity, pressure and
luminosity quickly and easily. Add
w
ind speed, direction and rain
gauge for full weather station
capabilities.
ESP32 Environment Sensor
Shield Hookup Guide
SparkFun's ESP32 Environment
Sensor Shield provides sensors and
hookups for monitoring
environmental conditions. This
tutorial will show you how to connect
your sensor suite to the Internet and
post weather data online.
Page 3
6
of 3
6
9
/
11
/
201
7
https://learn.sparkfun.com/tutorials/microclimat
e
-kit-experiment-guide/al
l
Products related to this Datasheet
MICRO CLIMATE KIT