Tmmi 2Platfann 5min:
AD\-\NTECH
User Manual
AIMB-258
Intel® GM45 µFC-PGA 478
CoreTM2 Duo Mini ITX
Motherboard with VGA, DVI,
LVDS, 6 COM, Dual GbE, 8 USB,
2 SATA II, PCIe x 16
Ver.1.00

AIMB-258 User Manual ii
Safety Information
Electrical safety
!To prevent electrical shock hazard, disconnect the power cable from the electri-
cal outlet before relocating the system.
!When adding or removing devices to or from the system, ensure that the power
cables for the devices are unplugged before the signal cables are connected. If
possible, disconnect all power cables from the existing system before you add a
device.
!Before connecting or removing signal cables from the motherboard, ensure that
all power cables are unplugged.
!Seek professional assistance before using an adapter or extension cord. These
devices could interrupt the grounding circuit.
!Make sure that your power supply is set to the correct voltage in your area. If
you are not sure about the voltage of the electrical outlet you are using, contact
your local power company.
!If the power supply is broken, do not try to fix it by yourself. Contact a qualified
service technician or your retailer.
Operation safety
!Before installing the motherboard and adding devices on it, carefully read all the
manuals that came with the package.
!Before using the product, make sure all cables are correctly connected and the
power cables are not damaged. If you detect any damage, contact your dealer
immediately.
!To avoid short circuits, keep paper clips, screws, and staples away from connec-
tors, slots, sockets and circuitry.
!Avoid dust, humidity, and temperature extremes. Do not place the product in
any area where it may become wet.
!Place the product on a stable surface.
!If you encounter technical problems with the product, contact a qualified service
technician or your retailer.
Part No. 2006025801 Edition 2
Printed in Taiwan June 2009
Caution! The symbol of the crossed out wheeled bin indicates that the product
(electrical and electronic equipment) should not be placed in municipal
waste. Check local regulations for disposal of electronic products.
FCC
iii AIMB-258 User Manual
Certifications
This device complies with the requirements in part 15 of the FCC rules: Operation is
subject to the following two conditions:
!This device may not cause harmful interference,
!This device must accept any interference received, including interference that
may cause undesired operation.
This equipment has been tested and found to comply with the limits for a Class A dig-
ital device, pursuant to Part 15 of the FCC Rules. These limits are designed to pro-
vide reasonable protection against harmful interference when the equipment is
operated in a commercial environment. This equipment generates, uses, and can
radiate radio frequency energy and, if not installed and used in accordance with the
instruction manual, may cause harmful interference to radio communications. Opera-
tion of this device in a residential area is likely to cause harmful interference in which
case the user will be required to correct the interference at his/her own expense. The
user is advised that any equipment changes or modifications not expressly approved
by the party responsible for compliance would void the compliance to FCC regula-
tions and therefore, the user's authority to operate the equipment.
Caution! There is a danger of a new battery exploding if it is incorrectly installed.
Do not attempt to recharge, force open, or heat the battery. Replace the
battery only with the same or equivalent type recommended by the man-
ufacturer. Discard used batteries according to the manufacturer's
instructions.

AIMB-258 User Manual iv
Technical Support
If a problem arises with your system and no solution can be obtained from the user’s
manual, please contact your place of purchase or local distributor. Alternatively,
please try the following help resources for further guidance. Visit the Advantech web-
site for FAQ, technical guide, BIOS updates, driver updates, and other information:
http://support.advantech.com.tw/Support/default.aspx
Packing List
Before you begin installing your single board, please make sure that the following
materials have been shipped:
!1 x AIMB-258 Intel® µFC-PGA 478 Core 2 Duo Mini ITX Motherboard
!2 x SATA HDD cable
!2 x SATA Power cable
!1 x Serial port cable 1 to 4
!1 x I/O port bracket
!1 x Startup manual
!1 x Driver CD
!1 x Warranty card
If any of the above items is damaged or missing, please contact your retailer.

v AIMB-258 User Manual
Contents
Chapter 1 Product Introduction ...........................1
1.1 Before You Proceed.................................................................................. 2
1.2 Motherboard Overview.............................................................................. 2
1.2.1 Placement Direction...................................................................... 2
1.2.2 Screw Holes.................................................................................. 3
1.3 Motherboard Layout .................................................................................. 4
Figure 1.1 Motherboard Layout ................................................... 4
1.4 Specifications ............................................................................................ 5
1.5 Operating System support list ................................................................... 6
1.6 Board Diagram .......................................................................................... 7
1.7 Ordering Information ................................................................................. 8
1.8 Riser Card ................................................................................................. 8
1.9 Bracket View ............................................................................................. 8
1.10 Accessories............................................................................................... 8
1.11 Layout Content List ................................................................................... 9
Table 1.1: Jumper Setting List..................................................... 9
Table 1.2: JSETCOM1: COM1/+5 V/+12 V Selection ................. 9
Table 1.3: JSETCOM2: COM2 RS232/422/485 Mode Selection 9
Table 1.4: CMOS1: Clear CMOS .............................................. 10
Table 1.5: J1:LCD Power 3.3 V/5.5 V Selection........................ 10
Table 1.6: PSON1: ATX, AT Mode Selection ............................ 10
Table 1.7: JWDT1: Watchdog Timer Output Option.................. 11
Table 1.8: JOBS: HW monitor ................................................... 11
1.12 Central Processing Unit (CPU) for AIMB-258 ......................................... 11
1.12.1 Installing the CPU ....................................................................... 12
1.12.2 Installing the CPU Heatsink and Fan .......................................... 14
1.12.3 Uninstalling the CPU Heatsink and Fan...................................... 16
1.13 System Memory ...................................................................................... 17
1.13.1 DIMM Sockets Location.............................................................. 17
1.13.2 System Memory.......................................................................... 17
1.13.3 Memory Support List................................................................... 18
Table 1.9: SODIMM DDR3 ........................................................ 18
1.14 Connectors.............................................................................................. 19
1.14.1 Rear Panel Connectors............................................................... 19
Table 1.10:Rear Panel Connectors ............................................ 19
Table 1.11:LEDs......................................................................... 19
1.14.2 CPU Fan Connector (CPUFAN1) ............................................... 20
1.14.3 System Fan Connector (SYSFAN1, SYSFAN2)......................... 21
1.14.4 Serial Port Connector 3456 (COM3456)..................................... 22
1.14.5 Front Headphone Connector (HD1)............................................ 22
1.14.6 Front Panel Connector (JFP1/JFP2/JFP3) ................................. 23
1.14.7 ATX soft power switch (JFP1 / PWR_SW) ................................. 23
1.14.8 Reset (JFP1 / RESET)................................................................ 23
1.14.9 HDD LED (JFP2 / HDDLED)....................................................... 23
1.14.10External speaker (JFP2 / SPEAKER) ......................................... 23
1.14.11Power LED and keyboard lock connector
(JFP3 / PWR_LED&KEY LOCK) ................................................ 24
Table 1.12:ATX power supply LED status
(No support for AT power)........................................ 24
1.14.12USB 2.0 Connector (USB56, USB78)......................................... 24
1.14.13ATX Power Connector (ATX1).................................................... 25
1.14.14LCD Inverter Connector (VP1).................................................... 26
1.14.15LVDS Connector (LVDS1) .......................................................... 26
1.14.16Digital I/O Connector (DIO_CN1)................................................ 27

AIMB-258 User Manual vi
1.14.17Serial ATA Connector 1 & 2 (SATA1, SATA2) ........................... 27
1.14.18PCIe x 16 Slot (PCIE X 16)......................................................... 28
1.14.19SPI Flash Connector(SPI_CN1) ................................................. 28
1.14.20Memory Connector Channel A/B(DIMM1/2) ............................... 29
1.14.21SPDIF1 out connector(SPDIF1) ................................................. 29
1.14.22CF connector .............................................................................. 30
Chapter 2 BIOS Operation ................................. 31
2.1 BIOS Introduction.................................................................................... 32
2.2 BIOS Setup ............................................................................................. 32
2.2.1 Main Menu.................................................................................. 33
2.2.2 Standard CMOS Features .......................................................... 34
2.2.3 Advanced BIOS Features........................................................... 35
2.2.4 Advanced Chipset Features ....................................................... 36
2.2.5 Integrated Peripherals ................................................................ 37
2.2.6 USE Device Setting .................................................................... 39
2.2.7 Power Management Setup ......................................................... 40
2.2.8 PnP/PCI Configurations.............................................................. 42
2.2.9 PC Health Status ........................................................................ 42
2.2.10 Load Setup Defaults ................................................................... 43
2.2.11 Set Password.............................................................................. 43
Chapter 3 Chipset Software Install Utility ........ 45
3.1 Before you Begin .................................................................................... 46
3.2 Introduction ............................................................................................. 46
3.3 Windows Vista/XP Driver Setup.............................................................. 47
Chapter 4 VGA Setup ......................................... 49
4.1 Introduction ............................................................................................. 50
4.2 Windows Vista/XP Driver Setup.............................................................. 50
Chapter 5 LAN Configuration ............................ 51
5.1 Introduction ............................................................................................. 52
5.2 Features.................................................................................................. 52
5.3 Installation............................................................................................... 52
5.4 Windows Vista/XP Driver Setup (Realtek RTL8111C)............................ 52
Appendix A Programming the Watchdog Timer .55
A.1 Programming the Watchdog Timer ......................................................... 56
A.1.1 Watchdog timer overview ........................................................... 56
A.1.2 Programming the Watchdog Timer............................................. 56
Table A.1: Watchdog Timer Registers....................................... 58
A.1.3 Example Program ....................................................................... 59
Appendix B Pin Assignments............................... 63
B.1 USB Connector (USB56,USB78)............................................................ 64
Table B.1: USB5/USB6 Connector (USB56) ............................. 64
B.2 VGA Connector (VGA1A) ....................................................................... 64
Table B.2: VGA Connector (VGA1A)......................................... 64

vii AIMB-258 User Manual
B.3 DVI Connector (VGA1B) ......................................................................... 64
Table B.3: DVI Connector (VGA1B)........................................... 64
B.4 RS-232 Serial Port (COM1~COM2)........................................................ 65
Table B.4: RS-232 Serial Port (COM1~COM2) ......................... 65
B.5 RS-232 Serial Port (COM3 ~ COM6)...................................................... 66
Table B.5: RS-232 Serial Port (COM23).................................... 66
B.6 PS/2 Keyboard/ Mouse Connector (KBMS1) .......................................... 67
Table B.6: PS/2 Keyboard/ Mouse Connector (KBMS1) ........... 67
B.7 CPU Fan Power Connector (CPUFAN1) ................................................ 67
Table B.7: CPU Fan Power Connector (CPUFAN1).................. 67
B.8 Power LED & Keyboard Lock Connector (JFP3) .................................... 68
Table B.8: Power LED and Keylock Connector (JFP3) ............ 68
B.9 HDD LED and External Speaker Connector
(JFP2/HDD LED and SPEAKER)............................................................ 68
Table B.9: External Speaker Connector (JFP2/SPEAKER)....... 68
B.10 ATX Soft Power Switch and Reset Connector
(JFP1/ PWR-SW and RESET) ................................................................ 69
Table B.10:Audio Front Panel Connector (JFP1/ RESET) ......... 69
B.11 Audio Front Panel Connector (FPAUD1) ................................................ 69
Table B.11:Audio front panel connector (FPAUD1).................... 69
B.12 GPIO Pin Header (GPIO1)...................................................................... 70
Table B.12:GPIO Pin Header (GPIO1) ....................................... 70
B.13 LVDS Connector (LVDS1) ...................................................................... 71
Table B.13:LVDS Connector (LVDS1)........................................ 71
B.14 LVDS Power Jumper (J1) ....................................................................... 72
Table B.14:LVDS Power Jumper (J1)......................................... 72
B.15 LVDS Invert (VP1)................................................................................... 72
Table B.15:LVDS Invert (VP1) .................................................... 72
B.16 System I/O Ports ..................................................................................... 73
Table B.16:System I/O Ports ...................................................... 73
B.17 DMA Channel Assignments .................................................................... 73
Table B.17:DMA Channel Assignments...................................... 73
B.18 Interrupt Assignments ............................................................................. 74
Table B.18:Interrupt Assignments............................................... 74
B.19 1st MB Memory Map ............................................................................... 74
Table B.19:1st MB Memory Map ................................................ 74

AIMB-258 User Manual viii

Chapter 1
1Product Introduction
This chapter describes the main
board features and the new tech-
nologies it supports.

AIMB-258 User Manual 2
1.1 Before You Proceed
Take note of the following precautions before you install motherboard components or
change any motherboard settings.
1.2 Motherboard Overview
Before you install the motherboard, study the configuration of your chassis to ensure
that the motherboard fits into it. Refer to the chassis documentation before installing
the motherboard.
1.2.1 Placement Direction
When installing the motherboard, make sure that you place it into the chassis in the
correct orientation. The edge with external ports goes to the rear part of the chassis.
Caution!
!
Unplug the power cord from the wall socket before touching any
component.
!
Use a grounded wrist strap or touch a safely grounded object or a
metal object, such as the power supply case, before handling com-
ponents to avoid damaging them due to static electricity
!
Hold components by the edges to avoid touching the ICs on them.
!
Whenever you uninstall any component, place it on a grounded
antistatic pad or in the bag that came with the component.
!
Before you install or remove any component, ensure that the ATX
power supply is switched off or the power cord is detached from the
power supply. Failure to do so may cause severe damage to the
motherboard, peripherals, and/or components.
Warning! Make sure to unplug the power cord before installing or removing the
motherboard. Failure to do so can cause you physical injury and dam-
age motherboard components.
3 AIMB-258 User Manual
Chapter 1 Product Introduction
1.2.2 Screw Holes
Place four (4) screws into the holes indicated by circles to secure the motherboard to
the chassis.
Caution! Do not over tighten the screws! Doing so can damage the motherboard.
Place this side towards the rear
of the chassis.
FSOM
JOBS!
LANZ LANI VGA1A
Aumot U5334 usa12 vsma comz KBMS1
,; o
:22; a o CE
0 n"n°n°n°w C‘ ‘
””1 j *JSETCOM1
SPD‘F1 : , —JSETCOM2
me17 W Z coms‘ase
D‘MM‘ so 3
D‘MMZ p:
, ; —AT><1 eee‘="" a="" mfl="" fl="" lfc1="" g::="" ’7‘="" ba“="" ”="" isysfam="" e§§="" ‘="" —sysfan2="" cmos1="" *="" co="" c="" pc‘ejsx="" ii="" cpu!="" uss7a="" q="" .,="" u)="" usbsg="" is:="" :1="" w="" 1»;="" j="" u="" m="" '="" o="" 0="" l7="" ,ejfljejejwijejeflljw.="" .="" .="" x="" d="" —lyc="" ““zargwicd="" |="" ‘="" ‘="" \="" \="" \="" \="" sata1="" j1="" lvds1="" vp1="" cpu="" d‘oficni="" splcn1="" fan1="" sataz="" figgg="" j="" leed‘="" 0="" jfps="" o="" o="" wrjedakevl="" m="" oqcc)="">1>AIMB-258 User Manual 4
1.3 Motherboard Layout
Figure 1.1 Motherboard Layout
PWR-SW RESET
SPEAKER
1234
2468
1357
12 345

5 AIMB-258 User Manual
Chapter 1 Product Introduction
1.4 Specifications
Processor Sys-
tem
CPU (45 nm
µFC-PGA 478)
Intel® Core™2 Duo Intel Celeron M
Max. Speed T9400 2.53 GHz 575 2.0 GHz
Front Side Bus 667/800/1066 MHz 667 MHz
L2 Cache 6 MB 1 MB
Chipset GM45 + ICH9M
BIOS Award 16 Mbit, SPI
Expansion Slot
PCI -
Mini-PCI -
PCIe x 16 4 GB/s per direction, 1 slot
Memory
Technology DDR3 800/1066 MHz SDRAM
Max. Capacity 4 GB
Socket 2 x 204-pin SODIMM
Graphics
Controller Intel GM45 GMCH integrated Graphics Media Accelerator X4500
VRAM Shared system memory up to 384 MB video memory
LVDS Single channel 18/24-bit/Dual channel 36/48-bit LVDS
DVI-D Yes (if DVI is used, PCIe x16 is automatically disable)
Dual Display VGA + DVI; VGA + LVDS; DVI + LVDS
*Dual Display
Mode
Extended Mode, Clone Mode, Twin Mode
Ethernet
Interface 10/100/1000Base-T
Controller GbE LAN1: Realtek RTL8111C; GbE LAN2: Realtek RTL8111C
Connector RJ-45 x 2
SATA
Max Data Trans-
fer Rate
300 MB/s
Channel 2
SSD Compact Flash Compact Flash Supports compact flash type I/II
Rear I/O
VGA 1
DVI 1
Ethernet 2
USB 4 (USB 2.0 compliant)
Serial 2 (1 of RS-232, 1 of RS-232/422/485)
PS/2 2 (1 x keyboard and 1 x mouse)
Internal
Connector
LVDS 1
USB 4 (USB 2.0 compliant)
Serial 4 (RS-232)
IDE -
SATA 2
Audio 3 (Mic-in, Line-in, Line-out)
Compact Flash 1
Parallel -
IrDA -
FDD -
DIO 16-bit General Purpose I/O for digital signal input/output
Watchdog
Timer
Output Interrupt, system reset
Interval Programmable 1 ~ 255 sec/ min

AIMB-258 User Manual 6
*Dual Display Clone uses both display pipes to drive the same content at the same
resolution and color depth to two different displays. This configuration allows for dif-
ferent refresh rates on each display.
Dual Display Twin uses one of the display pipes to drive the same content, at the
same resolution, color depth, and refresh rates to two different displays.
Extended Desktop uses both display pipes to drive different content, at potentially
different resolutions, refresh rates, and color depths, to two different displays. This
configuration allows for a larger Windows desktop by using both displays as one
work surface.
1.5 Operating System support list
Power
Requirement
Power On 5 V 3.3 V 12 V 5 Vsb -12 V
0 . 9 9 A 2 . 6 7 A 2 . 0 7 A 0 . 1 7 A 0 . 0 8 A
Environment Operating Non-Operating
Temperature 0 ~ 60°C (32 ~ 140°F) -20 ~ 70°C (-4 ~ 158°F)
Physical
Characteristics
Dimensions 170 mm x 170 mm (6.69’ x 6.69’)
Operation System AIMB-258
Windows Vista Ultimate edition
(32-bit/64-bit)
Support
Windows XP professional edition
(32-bit/64-bit)
Support
XP embedded Support
Linux (Fedora) Only OS installation and limited I/O functionality are
validated
QNX Only OS installation and limited I/O functionality are
validated
WinCE 6.0 Require OEM BIOS. Please contact with Advantech
FAE
7 AIMB-258 User Manual
Chapter 1 Product Introduction
1.6 Board Diagram
Intel GM45n
GMCH
CRT
BIOS
NXP 9555
16-bit GPIO
Super IO
Winbond
W83627UHG
Direct Media Interface
2GB/s bandwidth
ICH9M
1066/800/667
MHzFSB
VGA
PCI3 x 16
DDR3 800/1066
Channel A
LVDS
Dual Channel
24-bit LVDS
GbE-LAN1: Realtek 8111C
SPI
DVI
PCI3 x 16 slot
LPC
SM Bus
JMB368
2SATAports
8USBPorts
Realtek ALC888
300MB/s
PCIe x 1
CF IDE
PCIe x 1
PCIe x 1
USB2.0/1.1
HD Audio
Intel Socket 478
Core 2 Duo Processor
DDR3 800/1066
Channel A
GbE-LAN2:Realtek 8111C
AIMB-258 User Manual 8
1.7 Ordering Information
1.8 Riser Card
1.9 Bracket View
1.10 Accessories
Part Number Display GbE SATA Serial CF
AIMB-258G2-00A1E VGA/ DVI/ LVDS Dual 2 6 1
Part Number Description
AIMB-R430P-03A1E 2U riser card with 3 PCI slot expansion
Part Number Description
1700003195 USB cable with four ports, 17.5 cm
1700002204 USB cable with four ports, 27 cm
1700002314 USB cable with four ports, 30.5 cm
6005
4003
m
6005
2001
m
6
4003
9 AIMB-258 User Manual
Chapter 1 Product Introduction
1.11 Layout Content List
Table 1.1: Jumper Setting List
Label Function
JSETCOM1 COM1/+5 V/+12 V Selection
JSETCOM2 COM2 RS232/422/485 Mode Selection
CMOS1 Clear CMOS
J1 LCD Power 3.3 V/5.5 V Selection
PSON1 ATX, AT Mode Selection
JWDT1 Watchdog Timer Output Option
JOBS1 Hardware Monitor
Table 1.2: JSETCOM1: COM1/+5 V/+12 V Selection
COM1 (Default)
+5 V
+12 V
Table 1.3: JSETCOM2: COM2 RS232/422/485 Mode Selection
Users can use JSETCOM2 to select among RS 232/422/485 modes for COM2. The default
setting is RS 232.
Table 1
ETCOMZ: COMZ R5232
171513119
O O
RS-232 Configuration
(default) 0 O
18 16 14 12 10
17 15 13 11 9 7 5
O O O
RS—422 Configuration
0 O O
18 16 14 12 10 8 6
17 15 13 11 9 7 5
O O O
RS—485 Configuration
0 O 0
18161412108 6
Table 1.4: CMOS1: Clear CMOS
Pins Result
1—2‘ Keep CMOS data‘
2—3 Clear CMOS data
'Default
1 1
no
Table 1.5: J1 :LCD Power 3.3 V/5.5 V Selection
Closed Pins Result
1—2‘ 3.3 V“
2—3 5 V
'Default
1 1
-m
Table 1.6: PSON1: ATX, AT Mode Selection
Closed Pins Result
1—2 AT Mode
2—3‘ ATX Mode‘
'Default
1
DZ
AIME-258 User Manual 10
AIMB-258 User Manual 10
Table 1.4: CMOS1: Clear CMOS
Pins Result
1-2* Keep CMOS data*
2-3 Clear CMOS data
*Default
Table 1.5: J1:LCD Power 3.3 V/5.5 V Selection
Closed Pins Result
1-2* 3.3 V*
2-3 5 V
*Default
Table 1.6: PSON1: ATX, AT Mode Selection
Closed Pins Result
1-2 AT Mode
2-3* ATX Mode*
*Default
Table 1.3: JSETCOM2: COM2 RS232/422/485 Mode Selection
RS-232 Configuration
(default)
RS-422 Configuration
RS-485 Configuration
11
Keep CMOS data Clear CMOS
11
3.3 V, 1-2 closed 5 V, 2-3 closed
11
AT Mode, 1-2 closed ATX Mode, 2-3 closed
Table 1.8: JOBS: HW monitor
Closed Pins Result
1-2' Close: Enable OBS Alarm [Default]
1-2 Open: Disable OBS Alarm
'Default
M
Close Open
1.12 Central Processing Unit (CPU) for AlMB-2
The motherboard AIME-258 comes with a surface mount 478-pin Ze
Force (ZIF) socket designed for the Intel® Pentium® M / Celeron® M
(Supports mPGA478M, Micro-FCPGA).
11 AIME-258
11 AIMB-258 User Manual
Chapter 1 Product Introduction
1.12 Central Processing Unit (CPU) for AIMB-258
The motherboard AIMB-258 comes with a surface mount 478-pin Zero Insertion
Force (ZIF) socket designed for the Intel® Pentium® M / Celeron® M processor
(Supports mPGA478M, Micro-FCPGA).
Table 1.7: JWDT1: Watchdog Timer Output Option
Closed Pins Result
1-2 NC
2-3* System Reset*
*Default
Table 1.8: JOBS: HW monitor
Closed Pins Result
1-2* Close: Enable OBS Alarm [Default]
1-2 Open: Disable OBS Alarm
*Default
11
NC, 1-2 closed System Reset, 2-3 closed
Close Open
12 12
Take one of the marked corner (with gold
triangle) on the CPU. This mark should
match a specific corner on the socket to
ensure correct installation.
Note!
!
Make sure the AC power is off before you install the CPU.
!
If installing a dual-core CPU, connect the CPU fan cable to the
CPUFAN1 connector to ensure system stability.
Gold Mark
6 33333;.
x coaoccocou I
AIMB-258 User Manual 12
1.12.1 Installing the CPU
Caution!
!
Intel® socket 478 Pentium M/ Celeron M CPU with 90nm process
package should come with installation instructions for the CPU,
heatsink, and the retention mechanism. If the instructions in this
section do not match the CPU documentation, follow the latter.
!
Upon purchase of the motherboard, make sure that the PnP cap is
on the socket and the socket contacts are not bent. Contact your
retailer immediately if the PnP cap is missing, or if you see any
damage to the PnP cap/socket contacts/motherboard components.
Your place of purchase or local distributor will shoulder the cost of
repair only if the damage is shipment/transit-related.
!
Keep the cap after installing the motherboard. Your place of pur-
chase or local distributor will process Return Merchandise Authori-
zation (RMA) requests only if the motherboard comes with the cap
on the socket.
!
The product warranty does not cover damage to the socket con-
tacts resulting from incorrect CPU installation/removal, or misplace-
ment/loss/ incorrect removal of the PnP cap.
1. Locate the CPU socket on
the motherboard.
Note! Before installing the CPU, make sure that the socket box is facing towards you.
1
Gold trlangular
mark
‘ MJ ‘3
E
m
E fiiéé
E WEED
E §§§§§§§§l§§§
W V
fifigm
]
]
13 AIMB-258 User Manual
Chapter 1 Product Introduction
2. The processor socket comes with
a screw to secure the processor,
please unlock the screw first.
3. Position the CPU above the
socket and the gold triangular
mark on the CPU must align with
pin 1 of the CPU socket.
4. Carefully insert the CPU into the
socket until it fits in place ‘Gold
mark’.
5. Turn the screw to the lock
position.
Warning! The CPU fits in only one correct orientation. DO NOT force the CPU into
the socket to prevent bending the connectors on the socket and damag-
ing the CPU.
AIMB-258 User Manual 14
1.12.2 Installing the CPU Heatsink and Fan
The Intel® Pentium® M / Celeron® M processor (supports mPGA478M, Micro-
FCPGA) requires a specially designed heatsink and fan assembly to ensure optimum
thermal condition and performance.
Warning! After installation, make sure to plug-in the ATX power cable to the moth-
erboard.
Caution! If you purchased a separate CPU heatsink and fan assembly, make
sure that you have properly applied Thermal Interface Material to the
CPU heatsink or CPU before you install the heatsink and fan assembly.
1. Place the heatsink on top of the
installed CPU, making sure that
the four screws match the holes
on the motherboard.
Motherboard Hole
Note! Orient the heatsink and fan assembly such that the CPU fan cable is
closest to the CPU fan connector.
2. Connect the CPU fan cable to the connector on the motherboard labelled
CPUFAN1.
emu-J
100903000470 K
filooooooo
Sense
+12V—
GND—
1
15 AIMB-258 User Manual
Chapter 1 Product Introduction
Caution!
!
Do not forget to connect the fan cables to the fan connectors. Insuf-
ficient air flow inside the system may damage the motherboard
components, and hardware monitoring errors can occur if you fail
to plug this connector.
!
These are not jumpers! DO NOT place jumper caps on the fan con-
nectors.
AIMB-258 User Manual 16
1.12.3 Uninstalling the CPU Heatsink and Fan
1. Disconnect the CPU fan cable
from the connector on the
motherboard.
2. Rotate each screw counter- clock-
wise.
3. Carefully remove the heatsink and
fan assembly from the mother-
board.
Note! Refer to the documentation in the boxed or stand-alone CPU fan pack-
age for detailed information on CPU fan installation.
Mm .m u L
_ u
17 AIMB-258 User Manual
Chapter 1 Product Introduction
1.13 System Memory
1.13.1 DIMM Sockets Location
The motherboard comes with two 204-pin Double Data Rate 3 (DDR3) Dual Inline
Memory Modules (DIMM) sockets. The following figure illustrates the location of the
sockets:
1.13.2 System Memory
The AIMB-258 has two sockets for 204-pin SODIMMx2.
All these sockets use 1.5 V unbuffered double data rate synchronous DRAMs (DDR
SDRAM). They are available in capacities of 256, 512, and 1024 MB. The sockets
can be filled in any combination with SODIMMs of any size, giving a total memory
size between 256 MB and 2 GB. AIMB-258 does NOT support ECC (error checking
and correction).
1.13.2.1 Memory Installation Procedures
To install SODIMMs, first make sure the two handles of the SODIMM socket are in
the.open. position. i.e., the handles lean outward. Slowly slide the SODIMM module
along the plastic guides on both ends of the socket. Then press the SODIMM module
right down into the socket, until you hear a click. This is when the two handles have
automatically locked the memory module into the correct position of the SODIMM
socket. To remove the memory module, just push both handles outward, and the
memory module will be ejected by the mechanism.
1.13.2.2 Cache Memory
The AIMB-258 supports a CPU with one of the following built-in full speed L2 caches:
2048 MB for Intel Core 2 Duo CPU
The built-in second-level cache in the processor yields much higher performance
than conventional external cache memories.

AIMB-258 User Manual 18
1.13.3 Memory Support List
Table 1.9: SODIMM DDR3
SODIMM DDR3
Brand Size Speed Type ECC Vendor PN Advantech
PN
Memory
Transcend 1GB DDR3
1066
SODIMM
DDR3
NTS128MSK
64V1U
96SD3-
1G1066NN-
TR
SEC K4B1G0846D-
HCF8(128x8)
2GB DDR3
1066
SODIMM
DDR3
NTS256MSK
64V1U
96SD3-
2G1066NN-
TR
SEC K4B1G0846D-
HCF8(128x8)
Apacer RAM
Apacer 1GB DDR3
1066
SODIMM
DDR3
N NA NA ELPIDA J1108BABG-
DJ-E 084909DE7
2GB DDR3
1066
SODIMM
DDR3
N NA NA ELPIDA J1108BABG-
DJ-E 084909D8T
19 AIMB-258 User Manual
Chapter 1 Product Introduction
1.14 Connectors
1.14.1 Rear Panel Connectors
Table 1.10: Rear Panel Connectors
No. Label Function Description
1 KBMS1 PS/2 mouse connector The standard PS/2 mouse DIN connec-
tor is for a PS/2 mouse.
2 COM1(Top) Serial port connector x 1 D-sub 9-pin, male
3 COM2(Bottom) Serial port connector x 1 D-sub 9-pin, male
4,5 LAN1_USB12/
LAN2_USB34
LAN (RJ-45) connector This port allows Gigabit connection to a
Local Area Network (LAN) through a
network hub. Refer to the table 1.11 for
the LAN port LED indications. The
optional 10/100 Mbps LAN controller
allows 10/100 Mbps connection to a
Local Area Network (LAN) through a
network hub.
6 Audio1 3 ports audio connector Mic-in, Line-in, Line-out
7 VGA VGA port Analog graphical output
8 DVI-D DVI port Digital graphical output
Table 1.11: LEDs
ACT / LINK LED SPEED LED
Status Description Status Description
OFF No link OFF 10 Mbps connection
Green Linked ORANGE 100 Mbps connection
Blinking Data activity GREEN 1 Gbps connection
12, 3 784, 5 6
D00
noooooocoo
aooaaocuao
AIMB-258 User Manual 20
1.14.2 CPU Fan Connector (CPUFAN1)
Caution!
!
Do not forget to connect the fan cables to the fan connectors. Insuf-
ficient air flow inside the system may damage the motherboard
components, and hardware monitoring errors can occur if you fail
to plug this connector.
!
These are not jumpers! DO NOT place jumper caps on the fan
connectors.
D00
fignooaoooioiflv
fijooiooooouglflw.
21 AIMB-258 User Manual
Chapter 1 Product Introduction
1.14.3 System Fan Connector (SYSFAN1, SYSFAN2)
Caution!
!
Do not forget to connect the fan cables to the fan connectors. Insuf-
ficient air flow inside the system may damage the motherboard
components, and hardware monitoring errors can occur if you fail
to plug this connector.
!
These are not jumpers! DO NOT place jumper caps on the fan con-
nectors.
900‘
mow”
Q .7 Jifi‘ Q "2”29
wmhm‘y
$3 J
COM3_#DCD DO CUM3_#DSR
c0M3,er oo con/lung
COM3_SOUT oo commas
COM3_#DTR oo COM3_#RI
GND 00 GND
CUMUDCD oo COMUDSR
com 5m 00 com #RTS
COM4_SOUT oo COM4 ms
cor/143mm oo COMAJRI
GND 00 GND
COM5_#DCD oo OMSJDSR
COM5751N CO CDMSJtRTS
coms_sou‘r oo commas
COM5_#DTR oo COMSJRI
GND 00 GND
COM6_#DCD oo COM6_#DSR
COM6_SI'N oo COMURTS
COM6_SOUT oo commas
COMGjDTR oc COMURI
GND 00 GND
CNLOUT_R
O5V
.
GND 00 (y-CNLOUT_L
Fionl_MIC 000 5- LOUTL
1_ | |
GND JDD
LOUTR
AIMB-258 User Manual 22
1.14.4 Serial Port Connector 3456 (COM3456)
1.14.5 Front Headphone Connector (HD1)
This connector is for a chassis-mounted front panel audio I/O module that supports
either HD Audio. Connect one end of the front panel audio I/O module cable to this
connector.
23 AIMB-258 User Manual
Chapter 1 Product Introduction
1.14.6 Front Panel Connector (JFP1/JFP2/JFP3)
There are several external switches to monitor and control the AIMB-258.
1.14.7 ATX soft power switch (JFP1 / PWR_SW)
If your computer case is equipped with an ATX power supply, you should connect the
power on/off button on your computer case to (JFP1/PWR_SW). This connection
enables you to turn your computer on and off.
1.14.8 Reset (JFP1 / RESET)
Many computer cases offer the convenience of a reset button. Connect the wire for
the reset button.
1.14.9 HDD LED (JFP2 / HDDLED)
You can connect an LED to connector (JFP2/HDDLED) to indicate when the HDD is
active.
1.14.10 External speaker (JFP2 / SPEAKER)
(JFP2 / SPEAKER) is a 4-pin connector for an external speaker. If there is no exter-
nal speaker, the AIMB-258 provides an onboard buzzer as an alternative. To enable
the buzzer, set pins 3-4 as closed.
Note! For motherboards with the optional HD Audio feature, we recommend
that you connect a high-definition front panel audio module to this con-
nector to avail of the motherboard’s high definition audio capability.
'3 53:92, O
0 fig?) 0
mm a a
W uss+sv
— 6ND
USB+5V
USB¢5V —GND
USBeSV
[PB
AIMB-258 User Manual 24
1.14.11 Power LED and keyboard lock connector (JFP3 /
PWR_LED&KEY LOCK)
(JFP3 / PWR_LED&KEY LOCK) is a 5-pin connector for the power on LED and Key
Lock function. Refer to Appendix B for detailed information on the pin assignments.
The Power LED cable should be connected to pin 1-3. The key lock button cable
should be connected to pin 4-5.
There are 3 modes for the power supply connection. The first is “ATX power mode”,
system is on/off by a tentative power button. The second is “AT Power Mode”, system
is on/off by the switch of the Power supply. The third is another “AT Power Mode”
which is using the front panel power switch. The power LED status is indicated as fol-
lowing table:
1.14.12 USB 2.0 Connector (USB56, USB78)
These connectors are for USB 2.0 ports. Connect the USB module cable to any of
these connectors, then install the module to a slot opening at the back of the system
chassis. These USB connectors comply with USB 2.0 specification that supports up
to 480 Mbps connection speed.
Table 1.12: ATX power supply LED status (No support for AT power)
Power Mode LED (ATX Power Mode)
(On/Off by tentative
button)
LED (AT Power Mode)
(On/Off by switching
power supply)
LED (AT Power Mode)
(On/Off by front panel
switch)
PSON1
(On Back plane)
Jumper Setting
2-3 pin closed 1-2 pin closed Connect 1-2 pin cable
with switch
System On On On On
System Status Fast flashes Fast flashes Fast flashes
System Off Slow flashes Off Off
USB56
USB78
r J—L :L
C 0 23:}
O finial C 2‘”:
ms: 3
o +12v «5v
3 «svsa «5v
3 Powel 0K 5V
2 sun 6ND
+5v sun
3 GND cup
’ 6V PS on
em) sun
.3v .12v
+av .3v
25 AIMB-258 User Manual
Chapter 1 Product Introduction
1.14.13 ATX Power Connector (ATX1)
This connector is for an ATX Micro-Fit power supply. The plugs from the power sup-
ply are designed to fit these connectors in only one orientation. Find the proper orien-
tation and push down firmly until the connectors completely fit.
Important notes on the Motherboard Power Requirements
Caution! Never connect a 1394 cable to the USB connectors. Doing so will dam-
age the motherboard!
Note! The USB module is purchased separately.
Note!
!
Make sure that your ATX 12 V power supply can provide 6 A on the
+12 V lead and at least 1A on the +5-volt standby lead (+5 VSB).
The minimum recommended wattage is 180 W for a fully config-
ured system. The system can become unstable and might experi-
ence difficulty powering up if the power supply is inadequate.
!
You must install a Power Supply with a higher power rating if you
intend to install additional devices.
$v$vq
HZV
6ND
3" 83283
.x
V
cacaoccccn‘
OOOOOOOOOOOOOOOOOOOO
DOOOOOOOOOOOOOOOOOOO
oouoooooo K
coococncu
AIMB-258 User Manual 26
1.14.14 LCD Inverter Connector (VP1)
1.14.15 LVDS Connector (LVDS1)
VDDSAFE_1 VDDSAFE_2
GND_1 GND_7
VDDSAFE_3 VDDSAFE_4
OD0- ED0-
OD0+ ED0+
GND_2 GND_8
OD1-
OD1+
ED1-
ED1+
GND_3 GND_9
OD2-
OD2+
ED2-
ED2+
GND_4 GND_10
OCK-
OCK+ ECK-
ECK+
GND_5 GND_11
DDC_CLK DDC_DAT
GND_6 GND_12
NC
NC
HPLG
NC
NC
VCON
Q v§V GND
0 o SHEDATA_PCI SMHCLKJ’CI
E E o|o_cp11 DIO_GP27
g g] mo_sp1s mo_spzs
3 8 DIO_GP15 DIO_GP15
3 3 molar“ o|o_cm
.5 ”076?“ Dlojms
DIO_GP1Z DIO_EP21
DIO_GP1I DIO_GPZI
mo_sm mo_am
n *L V—‘
0 0 SATA_TXNO
0 0 GND SATA_TXPO
a mun;
GND SATAJIXNO
SATA_RXPI|
0200000000
0530003000
SATA_TXN2
GND SATA_TXP2
GND SATAJIXNZ
SATA_RXP2
27 AIMB-258 User Manual
Chapter 1 Product Introduction
1.14.16 Digital I/O Connector (DIO_CN1)
1.14.17 Serial ATA Connector 1 & 2 (SATA1, SATA2)
SATA1
SATA2
Note! AIMB-258 features a high performance serial ATA interface (up to 300
MB/s) which eases cabling to hard drives with thin and long cables.
n32; ooooo33°9338338338338
ooooo canonBanana.33333333333
o o
2463
0000
D000
1357
3.3023330 E
AIMB-258 User Manual 28
1.14.18 PCIe x 16 Slot (PCIE X 16)
1.14.19 SPI Flash Connector(SPI_CN1)
Note! This connector is for factory use only.
D000
12
N» 3593325
. ooaoooooou
29
29 AIMB-258 User Manual
Chapter 1 Product Introduction
1.14.20 Memory Connector Channel A/B(DIMM1/2)
1.14.21 SPDIF1 out connector(SPDIF1)
1
2
4
3
Mflfiooaooboo
AIMB-258 User Manual 30
1.14.22 CF connector

Chapter 2
2BIOS Operation

AIMB-258 User Manual 32
2.1 BIOS Introduction
Advantech provides full-featured AwardBIOSes, which deliver the superior perfor-
mance, compatibility, and functionality that today’s manufacturers of industrial PCs
and embedded boards demand. The many options and extensions let you customize
your products to a wide range of designs and target markets.
The modular, adaptable AwardBIOS 6.0 supports the broadest range of third-party
peripherals and all popular chipsets, plus Intel®, AMD, nVidia, VIA, and compatible
CPUs from 386 through Pentium and AMD Geode, K7 and K8 (including multiple pro-
cessor platforms), and VIA Eden C3 and C7 CPU.
You can use Advantech’s utilities to select and install features to suit your exclusive
designs.
2.2 BIOS Setup
The AIMB-258 Series system has built-in AwardBIOS with a CMOS SETUP utility
which allows user to configure required settings or to activate certain system fea-
tures.
The CMOS SETUP saves the configuration in the CMOS RAM of the motherboard.
When the power is turned off, the battery on the board supplies the necessary power
to the CMOS RAM.
When the power is turned on, pressing the <Del> button during the BIOS POST
(Power-On Self Test) will take you to the CMOS SETUP screen.
CONTROL KEYS
<↑>< ↓>< ←>< →>Move to select item
<Enter> Select Item
<Esc> Main Menu - Quit and not save changes into CMOS
Sub Menu - Exit current page and return to Main Menu
<Page Up/+> Increase the numeric value or make changes
<Page Down/-> Decrease the numeric value or make changes
<F1> General help, for Setup Sub Menu
<F2> Item Help
<F5> Load Previous Values
<F7> Load Optimized Default
<F10> Save all CMOS changes
)‘hnpn w 7 menus“
1“ u“;
LIM‘AL.
. rum Lum mm: 1.: ,
'PPPE :Lnu,
‘luu
nlrlrv hem
um; flu L. Lu-l Z) 1 mm.
33 AIMB-258 User Manual
Chapter 2 BIOS Operation
2.2.1 Main Menu
Press <Del> to enter AwardBIOS CMOS Setup Utility, the Main Menu will appear on
the screen. Use arrow keys to select among the items and press <Enter> to accept or
enter the sub-menu.
!Standard CMOS Features
This setup page includes all the items in standard compatible BIOS.
!Advanced BIOS Features
This setup page includes all the items of Award BIOS enhanced features.
!Advanced Chipset Features
This setup page includes all the items of Chipset configuration features.
!Integrated Peripherals
This setup page includes all onboard peripheral devices.
!Power Management Setup
This setup page includes all the items of Power Management features.
!PnP/PCI Configurations
This setup page includes PnP OS and PCI device configuration.
!PC Health Status
This setup page includes the system auto detect CPU, and reports system tem-
perature, CPU temperature, fan speeds, and system voltages.
!Load Setup Defaults
This setup page includes Load system optimized value, and the system would
be in best performance configuration.
!Set Password
Establish, change or disable password.
!Save & Exit Setup
Save CMOS value settings to CMOS and exit BIOS setup.
!Exit Without Saving
Abandon all CMOS value changes and exit BIOS setup.
:my: fl;
n nimfl
E bum-mu
11 mm
mmnnm _
mu Eitvmn
yam
mm)"
AIMB-258 User Manual 34
2.2.2 Standard CMOS Features
!Date
The date format is <weekday>, <month>, <day>, <year>.
!Time
The times format in <hour> <minute> <second>, based on the 24-hour time
!IDE Channel 0/1/2, Master
IDE HDD Auto-Detection Press "Enter" for automatic device detection.
!Video
Select EGA or VGA display.
!Halt on
The item determines whether the computer will stop if an error is detected dur-
ing power up.
!Base Memory
The POST of the BIOS will determine the amount of base (or conventional)
memory installed in the system.
!Extended Memory
The POST of the BIOS will determine the amount of extended memory (above
1MB in CPU’s memory address map) installed in the system.
!Total Memory
This item displays the total system memory size.
Weekday From Sun to Sat, determined and display by BIOS only
Month From Jan. to Dec.
Day From 1 to 31
Year From 1999 through 2098
No Errors The system boot will not stop for any error
All Errors Whenever the BIOS detects a non-fatal error the system will be
stopped.
All, But Keyboard The system boot will not stop for a keyboard error; it will stop for
all other errors. (Default value)
All, But Diskette The system boot will not stop for a disk error; it will stop for all
other errors.
All, But Disk/Key The system boot will not stop for a keyboard or disk error; it will
stop for al other errors.
Mum « , fluuuUHUS cm]: 321“; Uh
ed M; Fuahue
u-u raw“ 2 ' mm )lzly
"an! m
uh H.“ mm. prx >
um 11 I'vlm
an x Pumsx n.. su Run. mm
A fluul Hr: in: - rm ‘2 12.”.st
arm: n - :
“mm.
m ml»: "pun n m
Han! Up mmmu 2m“.
Eula r115: Eluhun
{up mu , 1m m
3; ‘u nu mum“.
nu ma:
Summny :men 5, m.
: m-sm“, 'I‘Uv‘VD'L‘ulLu: ran-5am 2r u! Hmong”; HL-
rs-vm iuv- Hahn: H 1m. new.”
35 AIMB-258 User Manual
Chapter 2 BIOS Operation
2.2.3 Advanced BIOS Features
!CPU Feature
This item allows user to adjust CPU features, CPU ratio, VID and thermal and
special feature like XD flag.
!Hard Disk Boot Priority
This item allows user to select boot sequence for system device HDD, SCSI,
RAID.
!Virus Warning [Disabled]
Enables or disables the virus warning.
!CPU L3 Cache
This item allows users to enable CPU L3 cache.
!Quick Power On Self Test [Enabled]
This field speeds up the Power-On Self Test (POST) routine by skipping retest-
ing a second, third and forth time. Setup setting default is enabled.
!First / Second / Third / Other Boot Drive
BIOS attempts to load the operating system from the boot devices in the order
assigned.
!Boot Other Device
Use this to boot another device. The options are "Enabled" and "Disabled".
!Boot Up NumLock Status [Enabled]
This item enables users to activate the Number Lock function upon system boot
!Gate A20 Option [Fast]
This item enables users to switch A20 control by port 92 or not.
!Typematic Rate Setting
This item enables users to set the two typematic controls items.
Hard Disk Assign this boot device priority to Hard Disk.
CDROM Assign this boot device priority to CDROM.
USB-FDD Assign this boot device priority to USB-FDD.
USB-ZIP Assign this boot device priority to USB-ZIP.
USB-CDROM Assign this boot device priority to USB-CDROM.
LAN Assign this boot device priority to LAN.
Disabled Do not attempt to boot from this device.
> yu 5.1..» Fuul 1m. Iluly
I114
mum an >
FEB/umlnp use
r 1» .u
lln 1‘ Frnm: Buller
mm: m:
"nu! g r mmnr
mu;- mm:
Enm (urpmg
pm: 11“):-
n .uenrn I HM}:
AIMB-258 User Manual 36
–Typematic Rate (Chars/Sec)
This item controls the speed at which the system registers repeated key-
strokes. The eight settings are 6, 8, 10, 12, 15, 20, 24 and 30.
–Typematic Delay (Msec)
This item sets the keypress delay before typematic repetition kicks in. The
four delay options are 250, 500, 750 and 1000.
!Security Option [Setup]
!APIC Mode [Enabled]
This item allows user to enabled of disabled “Advanced Programmable Interrupt
Controller”. APIC is implemented in the motherboard and must be supported by
the operating system, and it extends the number of IRQ's available.
!Show summary screen
This item is allowed you to decide if to show the system configuration table.
2.2.4 Advanced Chipset Features
!PCI Express Root port Func [Press Enter]
This item allows the user to adjust PCIE port on, off or auto.
!VT-d (Intel(R) Virtualization Tech)
Virtualization enhanced by Intel Virtualization Technology will allow a platform
to run multiple operating systems and applications in independent partitions.
With virtualization, one computer system can function as multiple “virtual” sys-
tems.
!PEG / Onchip VGA Control
Use this field to select PEG or Onchip VGA. The default is AUTO.
System System requires password both for bootup and for access to the
Setup page.
Setup Setup requires password only for access to the Setup page, not for
bootup. (Default value)
Note! This “Advanced Chipset Features” screen controls the configuration of
the board’s chipset for fine-tuning system performance. Screen options
depend on the specific chipset. It is strongly recommended that only
technical users make changes to the default settings.

37 AIMB-258 User Manual
Chapter 2 BIOS Operation
!PEG Force x1
Enabled or Disabled.
!On-Chip Frame Buffer Size
The On-Chip Frame Buffer Size can be set to 1 MB or 8 MB. This memory
is shared with the system memory.
!DVMT Mode
Intel's Dynamic Video Memory Technology (DVMT) allows the system to dynam-
ically allocate memory resources according to the demands of the system at any
point in time. The key idea in DVMT is to improve the efficiency of the memory
allocated to either system or graphics processor.
!Total GFX Memory
When "Enable" DVMT Mode, the graphics driver will allocate a fixed amount of
memory as dedicated graphics memory, as well as allow more system memory
to be dynamically allocated between the graphics processor
and the operating system.
!PAVP Mode
This setting enables/disables the Protected Audio/Video Path (PAVP) mode.
!Boot Display
Use the field to select the type of device you want to use as the display(s) of
the system.
!Panel type
Select panel resolution.
2.2.5 Integrated Peripherals
!OnChip IDE Device
This item enables users to set the OnChip IDE device status, includes enable
IDE devices and setting PIO and DMA access mode, and some of new chipset
also support for SATA device (Serial-ATA)
Note! This “Integrated Peripherals” option controls the configuration of the
board’s chipset, includes IDE, ATA, SATA, USB, AC97, MC97 and
Super IO and Sensor devices; this page this page depends on the par-
ticular chipset installed.
uzrmmm —
[—1 mm M;
['Ifimhlsifll
- [mam KICK ”calh
[Mflflmfl
{Ml} “A human
unn'v tmmmn
:g mi: N: u: [1“me
m: [mm
‘m mmm»
Y My)“ mmmn
' mm u mmmw
woe mm [mu
m:
:- M 7m mgpm [nuaamuanu
«5: m r u. (Ah um
um:
* mt; sic-mg. 1&1;ny
,Nci
“mm
r11“: m 1H 'thr‘fimi hr_
" 11mm,
n
m a New ., m: [E «ta a: mu. 1m .
25”“ mo.
'rmr : m nun
r47“ 2 “ITEM ”U131
r47“ . \IKWDIW]
rm? w unlit/MW]
r47“ 5F \IHWDIKE]
mm m mmmi
,vw. u. 5- ”:1: mm: ‘ ; mm w' my»: waxy.
4:2 'W LMlh“ mikm‘fim
AIMB-258 User Manual 38
!Onboard Device
This item enables users to set the Onboard device status; it includes enable
LAN1 and LAN2 devices.
!Super IO Device
This item enables users to set the Super IO device status; it includes enabling
COM1~COM6.

39 AIMB-258 User Manual
Chapter 2 BIOS Operation
!Onboard Serial port 1 [3F8 / IRQ4]
This item allows user to adjust serial port 1 address and IRQ.
!Onboard Serial port 2 [2F8 / IRQ3]
This item allows user to adjust serial port 2 address and IRQ.
!Onboard Serial port 3 [3E8 / IRQ4]
This item allows user to adjust serial port 3 address and IRQ.
!Onboard Serial port 4 [2E8 / IRQ3]
This item allows user to adjust serial port 4 address and IRQ.
!Onboard Serial port 5 [4F8 / IRQ5]
This item allows user to adjust serial port 5 address and IRQ.
!Onboard Serial port 6 [4E8 / IRQ7]
This item allows user to adjust serial port 6 address and IRQ.
2.2.6 USE Device Setting
!USB 1.0 Controller
Select “Enabled” if your system contains a Universal Serial Bus (USB) controller
and you have USB peripherals. The choices are "Enabled" and "Disabled".
!USB 2.0 Controller
This entry is used to disable/enable the USB 2.0 controller only. The BIOS itself
may or may not have high-speed USB support. If the BIOS has high speed USB
support built in, the support will automatically turn on when a high speed device
is attached. The choices are "Enabled" or "Disabled".
!USB Operation Mode
Set the USB 2.0 controller to Hi Speed (480 Mbps) or Full Speed (12 Mbps).
!USB Keyboard / Mouse Function
Select Enabled. if you plan to use a USB keyboard/Mouse. The choices are
"Enabled" and "Disabled".
!USB Storage Function
Select "Enabled" if you plan to use an external USB storage device to boot the
system under DOS mode. The choices are "Enabled" and "Disabled".
V £1 34 m.» 9mm:
Dams; .kmgm .00 «am?
L: 1!;
'36": w
Ca‘ 5";
LEE‘
@535 Egg 1. m
:m all IN:
m 2am » Sam M
.nmrum— wmam m; K am a:
a- mu “hm hm
hm A)“, m :flH-V n \[flui’unM—mlm
u m ’ '4- u mun
mm
5. utwv- a;
m: Midi]
\[mi'sziflhlwll
{rmnnumn
mm rlmmn
r . mi '7'an .mm:
wwimfignaa 2mm .m'mx -.>—: JAKPL." ‘54:»me
m JET!“
mm
AIMB-258 User Manual 40
2.2.7 Power Management Setup
!PCI Express PM Function
This allows you to enable or disable system wake up via PCI Express PME
(Power Management Event).
!Power-Supply Type [ATX]
This item allows user to set power-supply type, ATX or AT mode.
!ACPI Function [Enabled]
This item defines the ACPI (Advanced Configuration and Power Management)
feature that makes hardware status information available to the operating sys-
tem, and communicate PC and system devices for improving the power man-
agement.
!ACPI Suspend Type [S3 (STR)]
This item allows user to select sleep state when suspend.
!Run VGA BIOS if S3 Resume [Auto]
This item allows system to reinitialize VGA BIOS after system resume from
ACPI S3 mode.
Note! Use this "Power Management Setup" screen to configure the system for
most effective power management while still operating in a manner con-
sistent with intended computer use.
S1(POS) The suspend mode is equivalent to a software power down;
S3(STR) The system shuts down with the exception of a refresh current to
the system memory.

41 AIMB-258 User Manual
Chapter 2 BIOS Operation
!Power Management [User Defined]
This item allows user to select system power saving mode.
!Video Off Method [DPMS]
This item allows user to determine the manner is which the monitor is blanked.
!Video Off In Suspend [Yes]
This item allows user to turn off Video when the system enters suspend mode.
!Suspend Type [Stop Grant]
This item allows user to determine the suspend type.
!Modem use IRQ [3]
This item allows user to determine the IRQ which the MODEM can use.
!Suspend Mode [Disabled]
Shows the time of system inactivity before all devices except the CPU will be
shut off.
!HDD Power Down Mode [Disabled]
This item allows user to determine the time of system inactivity, the hard disk
drive will be powered down.
!Soft-Off by PWR-BTTN [Instant-Off]
This item allows user to define function of power button.
!PWRON After PWR-Fail [ON/Off/Former-Sts]
Use this to set up the system after power failure. The “Off” setting keeps the sys-
tem powered off after power failure, the “On” setting boots up the system after
failure, and the “Former-Sts” returns the system to the status before power fail-
ure.
!PowerOn by LAN [Enabled]
This item allows users to power on the system via LAN. The choices are
“Enabled” and “Disabled”.
!PowerOn by Modem [Enabled]
This item allows users to power on the system by Modem. The choices are
“Enabled” and “Disabled”.
!USB KB Wake_Up From S3 [Disabled]
This item allows user to set USB keyboard wake up system from S3 Enable or
Disable.
!PowerOn by Alarm [Disabled]
The choices are “Enabled” and “Disabled”. If enabled, the fields that follow indi-
cate dates and times of alarm settings.
Min Saving Minimum power management. Suspend Mode=1 hr.
Max Saving Maximum power management. Suspend Mode=1 min.
User Define Allows user to set each mode individually. Suspend Mode= Dis-
abled or 1 min ~1 hr.
V/H SYNC+Blank This option will cause system to turn off vertical and horizontal syn-
chronization ports and write blanks to the video buffer.
Blank Screen This option only writes blanks to the video buffer.
DPMS Initial display power management signaling.
Instant-Off Press power button then Power off instantly.
Delay 4 Sec Press power button 4 sec. to Power off.
Phuenix 7 RMardHlflS nuns Sehlp LHing
PnP/PEI Enufignridinn:
Reset :unnguraunn nah} [Disabled] new Help
Resunrces Enmrulled Hg mummstnn Hen“ Level >
nu] Nasnllrta: Pra : [My
llafan“ flxsahled.
.. r new»); Iglnhva mm .. 5:12“ 1; “mm Iu
Maximum Pagluad Size [123] rzsec [Manned Sgsvem
Eunfignraliuu 1mm
mun whpu u . nxi!
Szhlp u gun have
a |nlled u m. mum.”
and «he sgscm
recunfignrahun has
rmlAIMB-258 User Manual 42
2.2.8 PnP/PCI Configurations
!Reset Configuration Data [Disabled]
The default is Disabled. Select Enabled to reset Extended System Configuration
Data (ESCD) if you have installed a new add-on card, and system configuration
is in such a state that the OS cannot boot, enable this.
!Resources Controlled By [Auto(ESCD)]
The commands here are “Auto(ESCD)” or “Manual”. Choosing “Manual”
requires you to choose resources from the following sub-menu. ”Auto(ESCD)”
automatically configures all of the boot and Plug and Play devices, but you must
be using Windows 95 or above.
!Maximum Payload Size [128]
This allows you to set the maximum TLP payload size for PCI Express devices.
2.2.9 PC Health Status
!ACPI Shutdown Temperature [Disabled]
The system will shut down automatically if the CPU temperature goes over the
selected setting.
wen/«um: a
mf'?
um
m m an
wnunn
h maunmu mug [EL-Marni
h M, .11 name maid-aim
» mmwn um um l‘L—ml‘uu’fli
’* MI. MEI/Wm flan-IE
5m! wmamm:
a.“
:4 m: yum“
rm: - «2 w z ‘31:“:
_ m :0 Wm
wen/«m: : a
ww'fl
um
1 JV»:
|\. man
h man imfl mug ran-away:
a mm “mm name man-Wm
» nummm NHL-52w l‘L—mlmu‘fli
u anmrraicm wmnnummua
h mnum- m mm. mm sacru-
b w. Mmuum 24mm;
nasal gammy nmsmvm;
mm.- a It“ sump
m; mmmmv 52% .g
rm: -, 9A; 1 Wm :mm
_;:M.
mm
mmgm‘mvm
mm; magnum
43 AIMB-258 User Manual
Chapter 2 BIOS Operation
!CPU Warning Temperature
The system will give an automatic warning if the CPU temperature goes over the
selected setting.
!Current System Temperature
This shows you the current temperature of system.
!Current CPU Temperature
This shows the current CPU temperature.
!VCORE and Other Voltages
This shows the voltage of VCORE, +12 V, +3 V, +5 V, VBAT (V), and 5 VSB (V).
2.2.10 Load Setup Defaults
2.2.11 Set Password
Note! Load Setup Defaults loads the default system values directly from ROM.
If the stored record created by the Setup program should ever become
corrupted (and therefore unusable), these defaults will load automati-
cally when you turn the AIMB-258 Series system on.

AIMB-258 User Manual 44
To Establish Password
1. Choose the Set Password option from the CMOS Setup Utility main menu and
press <Enter>.
2. When you see “Enter Password”, enter the desired password and press
<Enter>.
3. At the “Confirm Password” prompt, retype the desired password, then press
<Enter>.
4. Select Save to CMOS and EXIT, type <Y>, then <Enter>.
To Change Password
1. Choose the Set Password option from the CMOS Setup Utility main menu and
press <Enter>.
2. When you see “Enter Password”, enter the existing password and press
<Enter>.
3. You will see “Confirm Password”. Type it again, and press <Enter>.
4. Select Set Password again, and at the “Enter Password” prompt, enter the new
password and press <Enter>.
5. At the “Confirm Password” prompt, retype the new password, and press
<Enter>.
6. Select Save to CMOS and EXIT, type <Y>, then <Enter>.
To Disable Password
1. Choose the Set Password option from the CMOS Setup Utility main menu and
press <Enter>.
2. When you see “Enter Password”, enter the existing password and press
<Enter>.
3. You will see “Confirm Password”. Type it again, and press <Enter>.
4. Select Set Password again, and at the “Enter Password” prompt, please don’t
enter anything; just press <Enter>.
5. At the “Confirm Password” prompt, again, don’t type in anything; just press
<Enter>.
6. Select Save to CMOS and EXIT, type <Y>, then <Enter>.
Note! To enable this feature, you should first go to the Advanced BIOS Fea-
tures menu, choose the Security Option, and select either Setup or Sys-
tem, depending on which aspect you want password protected. Setup
requires a password only to enter Setup. System requires the password
either to enter Setup or to boot the system. A password may be at most
8 characters long.

Chapter 3
3Chipset Software
Install Utility

AIMB-258 User Manual 46
3.1 Before you Begin
To facilitate the installation of the enhanced display device drivers and utility soft-
ware, you should read the instructions in this chapter carefully before you begin. The
device drivers for the AIMB-258 board are located on the software installation CD.
The auto-run function of the driver CD will guide you to the utilities and device drivers
required for a Windows system. The Intel® Chipset Software Installation Utility is not
required on any systems running Windows NT 4.0. Updates are provided via Service
Packs from Microsoft®.
Before you begin, it is important to note that most display drivers need to have the
relevant software application already installed in the system prior to installing the
enhanced display drivers. In addition, many of the installation procedures assume
that you are familiar with both the relevant software applications and operating sys-
tem commands. Review the relevant operating system commands and the pertinent
sections of your application software's user's manual before performing the installa-
tion.
3.2 Introduction
The Intel® Chipset Software Installation utility installs to the target system the Win-
dows INF files that outline to the operating system how the chipset components will
be configured. This is needed for the proper functioning of the following features:
!Core PCI and ISA PnP services
!IDE Ultra ATA 100/66/33 and Serial ATA interface support
!USB 1.1/2.0 support
!Identification of Intel® chipset components in the Device Manager
!Integrates superior video features. These include filtered sealing of 720 pixel
DVD content, and MPEG-2 motion compensation for software DVD
Note! The files on the software installation CD are compressed. Do not
attempt to install the drivers by copying the files manually. You must use
the supplied SETUP program to install the drivers
Note! This utility is used for the following versions of Windows system, and it
has to be installed before installing all the other drivers:
Windows XP
Windows Vista
vim mus) mm mm: Isa: may
9hr o. 7 pm 'Lm Emma
m» Dnumszswmu
Ixxninr
.1; man-aims
a 5mm
13 taxi/mum
. niimamlm
g warm;
3 figwukmuuk
xmmi
my mm mm «mm 15m am)
oh» 9 n pg: pm m
mum Dummzsl mm”?
nun-nus
q winning.
a Ml¥llmliéumi
x mam
47 AIMB-258 User Manual
Chapter 3 Chipset Software Install Utility
3.3 Windows Vista/XP Driver Setup
Insert the driver CD into your system's CD-ROM drive. You can see the driver folders
items. Move the mouse cursor over the folder "Drv_INF". In Drv_INF folder, you can
click "infinst_autol.exe" to complete the implement of the driver.

AIMB-258 User Manual 48

Chapter 4
4VGA Setup

AIMB-258 User Manual 50
4.1 Introduction
The Intel GM45 integrated graphics controller provides an analog display port. You
need to install the VGA driver to enable the function.
Intel Graphics Media Accelerator 4500MHD: Incorporating the latest Microsoft*
DirectX*10 support capabilities and Shader Model 4.0 features., it allows software
developers to create lifelike environments and characters. Dual independent display,
enhanced display modes for widescreen flat panels, and optimized 3D support
deliver an intense and realistic visual experience without requiring a separate graph-
ics card. @ 75 Hz refresh rate) and Intel GMA 4500MHD provides Intel® Clear Video
Technology, and graphics core speeds up to 533 MHz improve graphics and 3D ren-
dering performance, and enable high-definition video playback.
4.2 Windows Vista/XP Driver Setup
Insert the driver CD into your system's CD-ROM drive. In a few seconds, the software
installation main menu appears, as shown in the following figure.
The following installation procedure is for Windows XP. For other operating systems,
please do a manual installation.
Move the mouse cursor over the folder "Drv_VGA". In Drv_VGA folder, you can click
Installshield Wizard under folders named Vista, Vista64, XP64, or XP to automatically
complete driver installation.
Note! Before installing this driver, make sure the CSI utility has been installed
in your system. See Chapter 3 for information on installing the CSI util-
ity.

Chapter 5
5LAN Configuration

AIMB-258 User Manual 52
5.1 Introduction
The AIMB-258 features single/dual Gigabit Ethernet network interface. With the
Realtek RTL8111C GbE controller designed-in, AIMB-258 implements the PCI
Express host interface (PCI-E X1) in LAN connection with the maximum throughput
of 2Gbps for heavy-duty industrial network application.
5.2 Features
Integrated 10/100/100 BASE-T transceiver
1. 10/100/1000 BASE-T triple-speed MAC
2. High-speed RISC core with 24-KB cache
3. On-chip voltage regulation
4. Supporting Wake-on-LAN (WOL) function
5. PCI Express X1 host interface
5.3 Installation
The AIMB-258's Realtek RTL8111C Gigabit integrated controller supports all major
network operating systems. However, the installation procedure varies with different
operating systems. In the following sections, refer to the one that provides driver
setup procedure for the operating system you are using.
5.4 Windows Vista/XP Driver Setup (Realtek
RTL8111C)
Insert the driver CD into your system's CD-ROM drive. Select the Drv_LAN folder.
Note! Before installing the LAN drivers, make sure the CSI utility has been
installed on your system. See Chapter 3 for information on installing the
CSI utility.

53 AIMB-258 User Manual
Chapter 5 LAN Configuration
Select the subdirectory based OS version; install the appropriate LAN driver.

AIMB-258 User Manual 54

Appendix A
AProgramming the
Watchdog Timer

AIMB-258 User Manual 56
A.1 Programming the Watchdog Timer
The AIMB-258's watchdog timer can be used to monitor system software operation
and take corrective action if the software fails to function after the programmed
period. This section describes the operation of the watchdog timer and how to pro-
gram it.
A.1.1 Watchdog timer overview
The watchdog timer is built into the super I/O controller W83627UHG. It provides the
following functions for user programming:
!Can be enabled and disabled by user's program.
!Timer can be set from 1 to 255 seconds or 1 to 255 minutes.
!Generates an interrupt or resets signal if the software fails to reset the timer
after time-out.
A.1.2 Programming the Watchdog Timer
The I/O port address of the watchdog timer is 2E(hex) and 2F(hex).
2E (hex) is the address port. 2F(hex) is the data port.
You must first assign the address of register by writing address value into address
port 2E(hex), then write/read data to/from the assigned register through data port 2F
(hex).
Unlock
W83627UHG
Select register of
watchdog timer
Enable the function 0
the watchdog timer
Use the function of
the watchdog timer
LJ.
Lock
W83627U HG
57 AIMB-258 User Manual
Appendix A Programming the Watchdog Timer

AIMB-258 User Manual 58
Table A.1: Watchdog Timer Registers
Address of register (2E) Attribute
Read/Write Value (2F) and description
87 (hex) - Write this address to I/O address port 2E
(hex) twice to unlock the W83627UHG
07 (hex) write Write 08 (hex) to select register of
watchdog timer.
30 (hex) write Write 01 (hex) to enable the function of
the watchdog timer. Disabled is set as
default.
F5 (hex) write Set seconds or minutes as units for the
timer.
Write 0 to bit 3: set second as counting unit. [default]
Write 1 to bit 3: set minute as counting unit.
F6 (hex) write 0: stop timer [default]
01~FF (hex): The amount of the count,
in seconds or minutes, depends on the
value set in register F5 (hex). This num-
ber decides how long the watchdog
timer waits for strobe before generating
an interrupt or reset signal. Writing a
new value to this register can reset the
timer to count with the new value.
F7 (hex) read/write Bit 6: Write 1 to enable keyboard to reset
the timer, 0 to disable.[default]
Bit 5: Write 1 to generate a timeout sig-
nal immediately and automatically
return to 0. [default=0]
Bit 4: Read status of watchdog timer, 1
means timer is ""time out""."
AA (hex) - Write this address to I/O port 2E (hex)
to lock the watchdog timer.2.

59 AIMB-258 User Manual
Appendix A Programming the Watchdog Timer
A.1.3 Example Program
1. Enable watchdog timer and set 10 sec. as timeout interval
;-----------------------------------------------------------
Mov dx,2eh ; Unlock W83627UHG
Mov al,87h
Out dx,al
Out dx,al
;-----------------------------------------------------------
Mov al,07h ; Select registers of watchdog timer
Out dx,al
Inc dx
Mov al,08h
Out dx,al
;-----------------------------------------------------------
Dec dx ; Enable the function of watchdog timer
Mov al,30h
Out dx,al
Inc dx
Mov al,01h
Out dx,al
;-----------------------------------------------------------
Dec dx ; Set second as counting unit
Mov al,0f5h
Out dx,al
Inc dx
In al,dx
And al,not 08h
Out dx,al
;-----------------------------------------------------------
Dec dx ; Set timeout interval as 10 seconds and start counting
Mov al,0f6h
Out dx,al
Inc dx
Mov al,10
Out dx,al
;-----------------------------------------------------------
Dec dx ; lock W83627UHG
Mov al,0aah
Out dx,al
2. Enable watchdog timer and set 5 minutes as timeout interval
;-----------------------------------------------------------
Mov dx,2eh ; unlock W83627UHG
Mov al,87h
Out dx,al
Out dx,al

AIMB-258 User Manual 60
;-----------------------------------------------------------
Mov al,07h ; Select registers of watchdog timer
Out dx,al
Inc dx
Mov al,08h
Out dx,al
;-----------------------------------------------------------
Dec dx ; Enable the function of watchdog timer
Mov al,30h
Out dx,al
Inc dx
Mov al,01h
Out dx,al
;-----------------------------------------------------------
Dec dx ; Set minute as counting unit
Mov al,0f5h
Out dx,al
Inc dx
In al,dx
Or al,08h
Out dx,al
;-----------------------------------------------------------
Dec dx ; Set timeout interval as 5 minutes and start counting
Mov al,0f6h
Out dx,al
Inc dx
Mov al,5
Out dx,al
;-----------------------------------------------------------
Dec dx ; lock W83627UHG
Mov al,0aah
Out dx,al
3. Enable watchdog timer to be reset by mouse
;-----------------------------------------------------------
Mov dx,2eh ; unlock W83627UHG
Mov al,87h
Out dx,al
Out dx,al
;-----------------------------------------------------------
Mov al,07h ; Select registers of watchdog timer
Out dx,al
Inc dx
Mov al,08h
Out dx,al
;-----------------------------------------------------------

61 AIMB-258 User Manual
Appendix A Programming the Watchdog Timer
Dec dx ; Enable the function of watchdog timer
Mov al,30h
Out dx,al
Inc dx
Mov al,01h
Out dx,al
;-----------------------------------------------------------
Dec dx ; Enable watchdog timer to be reset by mouse
Mov al,0f7h
Out dx,al
Inc dx
In al,dx
Or al,80h
Out dx,al
;-----------------------------------------------------------
Dec dx ; lock W83627UHG
Mov al,0aah
Out dx,al
4. Enable watchdog timer to be reset by keyboard
;-----------------------------------------------------------
Mov dx,2eh ; unlock W83627UHG
Mov al,87h
Out dx,al
Out dx,al
;-----------------------------------------------------------
Mov al,07h ; Select registers of watchdog timer
Out dx,al
Inc dx
Mov al,08h
Out dx,al
;-----------------------------------------------------------
Dec dx ; Enable the function of watchdog timer
Mov al,30h
Out dx,al
Inc dx
Mov al,01h
Out dx,al
;-----------------------------------------------------------
Dec dx ; Enable watchdog timer to be strobed reset by keyboard
Mov al,0f7h
Out dx,al
Inc dx
In al,dx
Or al,40h
Out dx,al

AIMB-258 User Manual 62
;-----------------------------------------------------------
Dec dx ; lock W83627UHG
Mov al,0aah
Out dx,al
5. Generate a time-out signal without timer counting
;-----------------------------------------------------------
Mov dx,2eh ; unlock W83627UHG
Mov al,87h
Out dx,al
Out dx,al
;-----------------------------------------------------------
Mov al,07h ; Select registers of watchdog timer
Out dx,al
Inc dx
Mov al,08h
Out dx,al
;-----------------------------------------------------------
Dec dx ; Enable the function of watchdog timer
Mov al,30h
Out dx,al
Inc dx
Mov al,01h
Out dx,al
;-----------------------------------------------------------
Dec dx ; Generate a time-out signal
Mov al,0f7h
Out dx,al ;Write 1 to bit 5 of F7 register
Inc dx
In al,dx
Or al,20h
Out dx,al
;-----------------------------------------------------------
Dec dx ; lock W83627UHG
Mov al,0aah
Out dx,al

Appendix B
BPin Assignments
00
CO
on
Table B.2: VGA Connector (VGA1A)
Pln Slgnal Pln
1 RED 9
2 GREEN 1O
3 BLUE 11
4 N10 12
5 GND 13
6 GND 14
7 GND 15
8 GND
B.3 DVI Connector (VGA1 B)
AIME-258 User Manual 64
AIMB-258 User Manual 64
B.1 USB Connector (USB56,USB78)
B.2 VGA Connector (VGA1A)
B.3 DVI Connector (VGA1B)
Table B.1: USB5/USB6 Connector (USB56)
Pin USB1 Signal Pin USB2 Signal
1+5 V 2+5 V
3 LP5- 4 LP5+
5 LP5+ 6 LP5-
7 GND 8 GND
9NC 10GND
7531
10864 2
Table B.2: VGA Connector (VGA1A)
Pin Signal Pin Signal
1RED 9VCC
2 GREEN 10 GND
3BLUE 11N/C
4N/C 12SDAT
5 GND 13 H-SYNC
6 GND 14 V-SYNC
7GND 15SCLK
8GND
5
15
1
11
10 6
Table B.3: DVI Connector (VGA1B)
Pin Signal Pin Signal
1RED 11NC
2 GREEN 12 VGADATA
3 BLUE 13 VHSYNC
4 N/C 14 VVSYNC
5 GND 15 VGACLK
65 AIMB-258 User Manual
Appendix B Pin Assignments
B.4 RS-232 Serial Port (COM1~COM2)
6GND 16GND
7GND 17GND
8GND
9+5V_VGA
10 GND
Table B.3: DVI Connector (VGA1B)
Table B.4: RS-232 Serial Port (COM1~COM2)
Pin Signal
1 DCD/TX_422N/TX_485N
2 RXD/TX_422P/TX_485P
3 TXD/RX_422P
4 DTR/RX_422N
5GND
6DSR
7RTS
8CTS
9 RRI
1
6
COMLMDCD D O COM3J¢DSR
COM3_SI'N 00 COM3 #RTS
COM3_SOUT O O COM3JC1'S
COMSJfDTR O O COMSJCRI
GND 0 0 GND
COM4_#DCD O O COM4_#DSR
COM4_S O O COM4J¢RTS
COM4_SOUT O O COMAJCF S
COM4JDTR O O COMAJCRI
GND 0 0 GND
COMSJIDCD O O OM5_#DSR
COM5_STN 0 O COMSJCRTS
COM5_SOUT O O COM5JC1'S
COMSJDTR 0 O COMSJRI
GND 0 0 GND
COM6_#DCD 0 O COMéthSR
COM6_SIN O O COMGJCRTS
COMELSCIUT O O COMGJCI‘ S
COMG #DTR OO COMG #RI
GND 0 0 GND
AIMB-258 User Manual 66
B.5 RS-232 Serial Port (COM3 ~ COM6)
Table B.5: RS-232 Serial Port (COM23)
Pin Signal Pin Signal
1 COM3_#DCD 2 COM3_#DSR
3 COM3_SIN 4 COM3_#RTS
5 COM3_SOUT 6 COM3_#CTS
7 COM3_#DTR 8 COM3_#RI
9GND 10GND
11 COM4_#DCD 12 COM4_#DSR
13 COM4_SIN 14 COM4_#RTS
15 COM4_SOUT 16 COM4_#CTS
17 COM4_#DTR 18 COM4_#RI
19 GND 20 GND
21 COM5_#DCD 22 COM5_#DSR
23 COM5_SIN 24 COM5_#RTS
25 COM5_SOUT 26 COM5_#CTS
27 COM5_#DTR 28 COM5_#RI
29 GND 30 GND
31 COM6_#DCD 32 COM6_#DSR
33 COM6_SIN 34 COM6_#RTS
35 COM6_SOUT 36 COM6_#CTS
37 COM6_#DTR 38 COM6_#RI
39 GND 40 GND
67 AIMB-258 User Manual
Appendix B Pin Assignments
B.6 PS/2 Keyboard/ Mouse Connector (KBMS1)
B.7 CPU Fan Power Connector (CPUFAN1)
Table B.6: PS/2 Keyboard/ Mouse Connector (KBMS1)
Pin Signal Pin Signal
1 KB DATA 2 NC
7MS DATA 6NC
3GND 8NC
4VCC 9GND
5 KB CLOCK 10 VCC
11 MS CLOCK 12 NC
12 11
10 9
87
5
3
12
4
6
Table B.7: CPU Fan Power Connector (CPUFAN1)
Pin Signal
1GND
2+12 V
3DEC
1
2
3
#01034
DO
00
OO
00
WGAN
AIMB-258 User Manual 68
B.8 Power LED & Keyboard Lock Connector (JFP3)
You can use an LED to indicate when the single board computer is on. Pin 1 of JFP3
supplies the LED's power, and Pin 3 is the ground.
B.9 HDD LED and External Speaker
Connector(JFP2/HDD LED and SPEAKER)
The single board computer has its own buzzer. You can also connect it to the external
speaker on your computer chassis.
Table B.8: Power LED and Keylock Connector (JFP3)
Pin Function
1 LED power (+5 V)
2NC
3GND
4 KEYLOCK#
5GND
Table B.9: External Speaker Connector (JFP2/SPEAKER)
Pin Signal Pin Signal
1 SPK+ 2 HDDLED+
3 NC 4 HDDLED-
5 SPK_IN 6 SMB_DAATA
7 SPK- 8 SMB_CLK
N
OOOEI
Table 3.10: Audio Front Panel Connec
Pln Slgnal
1 F’WR_BTN#
2 G N D
3 RESET
4 G N D
3.11 Audio Front Panel Conne
GOO O
DOOOO
69
69 AIMB-258 User Manual
Appendix B Pin Assignments
B.10 ATX Soft Power Switch and Reset Connector
(JFP1/ PWR-SW and RESET)
B.11 Audio Front Panel Connector (FPAUD1)
Table B.10: Audio Front Panel Connector (JFP1/ RESET)
Pin Signal
1PWR_BTN#
2GND
3 RESET
4GND
1
2
4
3
Table B.11: Audio front panel connector (FPAUD1)
1 MIC-IN 2 GND
3 MIC_VCC 4 VCC
5 LRR 6 LOUT_R
7 JDO 8 NC
9 LRL 10 LOUT_L
DO
00
OO
00
00
OO
00
00
OO
00
AIMB-258 User Manual 70
B.12 GPIO Pin Header (GPIO1)
Table B.12: GPIO Pin Header (GPIO1)
Pin Signal Pin Signal
1 DIO_GP20 2 DIO_GP10
3 DIO_GP21 4 DIO_GP11
5 DIO_GP22 6 DIO_GP12
7 DIO_GP23 8 DIO_GP13
9DIO_GP24 10DIO_GP14
11 DIO_GP25 12 DIO_GP15
13 DIO_GP26 14 DIO_GP16
15 DIO_GP27 16 DIO_GP17
17 SMBCLK_PCI 18 SMBDATA_PCI
19 GND 20 VCC5_DIO
12
34
17 18
19 20
DOOOOOOOOOOOOOOOOOOO
OOOOOOOOOOOOOOOOOOOO
71 AIMB-258 User Manual
Appendix B Pin Assignments
B.13 LVDS Connector (LVDS1)
Table B.13: LVDS Connector (LVDS1)
Pin Signal Pin Signal
1 VDDSAFE_1 2 VDDSAFE_2
3 GND_1 4 GND_7
5 VDDSAFE_3 6 VDDSAFE_4
7OD0- 8 ED0-
9OD0+ 10ED0+
11 GND_2 12 GND_8
13 OD1- 14 ED1-
15 OD1+ 16 ED1+
17 GND_3 18 GND_9
19 OD2- 20 ED2-
21 OD2+ 22 ED2+
23 GND_4 24 GND_10
25 OCK- 26 ECK-
27 OCK+ 28 ECK+
29 GND_5 30 GND_11
31 DDC_CLK 32 DDC_DAT
33 GND_6 34 GND_12
35 OD3- 36 ED3-
37 OD3+ 38 ED3+
39 HPLG 40 VCON
2438
40

AIMB-258 User Manual 72
B.14 LVDS Power Jumper (J1)
*default setting
B.15 LVDS Invert (VP1)
Table B.14: LVDS Power Jumper (J1)
Pin Signal
1 VCC3
2 VDD_LCD
3VCC
3
1
2
3
1
2
*3.3V
5V
Voltage Jumper Setting
Table B.15: LVDS Invert (VP1)
Pin Signal
1 VCC12
2GND
3 BKLTEN
4 VBR
5VCC

73 AIMB-258 User Manual
Appendix B Pin Assignments
B.16 System I/O Ports
B.17 DMA Channel Assignments
Table B.16: System I/O Ports
Addr. range (Hex) Device
000-01F DMA controller
020-021 Interrupt controller 1, master
022-023 Chipset address
040-05F 8254 timer
060-06F 8042 (keyboard controller)
070-07F Real-time clock, non-maskable interrupt (NMI)
mask
080-09F DMA page register
0A0-0BF Interrupt controller 2
0C0-0DF DMA controller
0F0 Clear math co-processor
0F1 Reset math co-processor
0F8-0FF Math co-processor
1F0-1F8 Fixed disk
200-207 Game I/O
290-29F On-board hardware monitor
2F8-2FF Serial port 2
300-31F Prototype card
360-36F Reserved
380-38F SDLCm bisynchronous 2
3A0-3AF Bisynchronous 1
3C0-3CF Reserved
3D0-3DF Color/graphics monitor adapter
3F0-3F7 Diskette controller
3F8-3FF Serial port 1
3E8-3EF Serial port3
2E8-2EF Serial port4
4F8-4FF Serial port5
4E8-4EF Serial port6
Table B.17: DMA Channel Assignments
Channel Function
0 Available
1 Available
2 Floppy disk (8-bit transfer)
3 Available
4 Cascade for DMA controller 1
5 Available
6 Available
7 Available

AIMB-258 User Manual 74
B.18 Interrupt Assignments
B.19 1st MB Memory Map
Table B.18: Interrupt Assignments
Priority Interrupt# Interrupt Source
1 NMI Parity error detected
2 IRQ0 Interval timer
3 IRQ1 Keyboard
- IRQ2 Interrupt from controller 2 (cascade)
4 IRQ8 Real-time clock
5 IRQ9 Cascaded to INT 0A (IRQ 2)
6 IRQ10 Available
7 IRQ11 Available
8 IRQ12 PS/2 mouse
9 IRQ13 INT from co-processor
10 IRQ14 Primary IDE Channel
12 IRQ3 Serial communication port 2/4
13 IRQ4 Serial communication port 1/3
14 IRQ5 Serial communication port 5
15 IRQ6 Diskette controller (FDC)
16 IRQ7 Serial communication port 6
Table B.19: 1st MB Memory Map
Addr. range (Hex) Device
E0000h - FFFFFh BIOS
CC000h - DFFFFh Unused
C0000h - CBFFFh VGA BIOS
A0000h - BFFFFh Video Memory
00000h - 9FFFFh Base memory

75 AIMB-258 User Manual
Appendix B Pin Assignments
Dusttd IPlat/arm Services
AD\-\NTECH
www.advantech.com
Please verify specifications before quoting. This guide is intended for reference
purposes only.
All product specifications are subject to change without notice.
No part of this publication may be reproduced in any form or by any means,
electronic, photocopying, recording or otherwise, without prior written permis-
sion of the publisher.
All brand and product names are trademarks or registered trademarks of their
respective companies.
© Advantech Co., Ltd. 2009
Products related to this Datasheet
CIRC MOD C2D MINI ITX FSB