PREV601 Demo Board Quick Start Datasheet by NXP USA Inc.

View All Related Products | Download PDF Datasheet
Ow
AN11281
Quick Start Up Guide PREV601 Demo Board
Rev. 1.510 November 2013
243915
Application note
COMPANY PUBLIC
Document information
Info
Keywords
NxpRdLib, HTRC110, MCU, Code Red, eclipse, LPC1227, reader library
Abstract
PREV601 board. It describes the actions to be done to become
acquainted with the demo reader.
AN11281 hug://www.nxg.cum salesaddressesangcom
NXP Semiconductors
AN11281
PREV601 Quick Startup Guide
AN11281
All information provided in this document is subject to legal disclaimers.
© NXP B.V. 2013. All rights reserved.
Application note
COMPANY PUBLIC
Rev. 1.510 November 2013
243915
2 of 37
Contact information
For more information, please visit:
http://www.nxp.com
For sales office addresses, please send an email to: salesaddresses@nxp.com
Revision history
Rev
Date
Description
1.5
20131110
Added a note about the LPCXpresso IDE version in chapter 4
1.4
20130613
Added description about the P2P Snep Client
1.3
20130608
Small alignments between new project structure and this document
1.2
20130116
Small alignments between the referenced code and this guide.
1.1
20130107
Added chapter 6.4 about the hardware setting
Added chapter 6.5 about the LPCD mode
1.0
20121019
First release
AN11281
NXP Semiconductors
AN11281
PREV601 Quick Startup Guide
AN11281
All information provided in this document is subject to legal disclaimers.
© NXP B.V. 2013. All rights reserved.
Application note
COMPANY PUBLIC
Rev. 1.510 November 2013
243915
3 of 37
1. Introduction
This application note gives a detailed overview of the hardware for working with the
PRH601 integrated reader module (Chapter 2), the installation procedures of the
Development Environment (Chapter 4.1) and the handling of the reader projects using
the NXP Reader Library (Chapter 4.2).
The PREV601 board can be used for software development for the PR601 as well as the
PRH601 reader IC. The only difference between these ICs is the additional 125kHz
capability of the PRH601 IC.
The projects used in this documentation are:
Communication with MIFARE Ultralight Chapter 5.1
Communication with MIFARE Classic Chapter 5.2
Communication with MIFARE DESFire Chapter 5.3
Polling for Tags in the RF - field Chapter 5.4
All projects can also operate in Low Power Card Detection Mode [11].
2. Hardware overview of the Demo Reader
The demo reader is made up of one single board including two reader ICs and one
processor with flash memory. The IC that contains these reader ICs and the processor is
the PRH601HL. For more details, please see our website at [9]. The multi chip package
contains the following ICs:
A CLRC663 Reader IC. For detailed information please see [2].
A HITAG HTRC110. For detailed information please see [7].
The HTRC110 is supported by breakout pads. A developer has to attach his own
antenna incl. matching to make use of the 125KHz functionality of the PRH601.
Software for the 125Khz functionality can be found on the NXP website [8].
A LP1227 IC. For detailed information please see [3]
To flash the LPC1227 micro controller, one also needs a LPC-Link board (LPC3154)
2.1 PREV601 board
Fig 1. Picture of the PREV601 board
AN11281 37
NXP Semiconductors
AN11281
PREV601 Quick Startup Guide
AN11281
All information provided in this document is subject to legal disclaimers.
© NXP B.V. 2013. All rights reserved.
Application note
COMPANY PUBLIC
Rev. 1.510 November 2013
243915
4 of 37
The PREV601 board embeds the contactless communication transceiver IC CLRC663,
HTRC and LPC1227 processor.
The software provided with this evaluation board also works with the significantly smaller
PREV601M Microboard.
Fig 2. PREV601M Microboard
2.2 LPC-Link LPC3154
The LPC-Link is equipped with an 8-pin JTAG header and it seamlessly connects the
target via USB (the USB interface and other debug features are provided by NXP’s
ARM9 based LPC3154 MCU).
Since this LPC-Link is not available as single device, one has to cut that part from any
LPCXpresso board. The LPCXpresso boards containing the LPC-Link with the LPC3154
MCU are as follows:
LPC11C24 LPCXpresso Board
LPC11U14 LPCXpresso Board
LPC1114 LPCXpresso Board
LPC1115 LPCXpresso Board
LPC1227 LPCXpresso Board
LPC1347 LPCXpresso Board
LPC1343 LPCXpresso Board
LPC1769 LPCXpresso Board
To use the LPC-Link, one has to cut it off from the LPCXpresso board.
AN11281 HHIIIH JI‘IJJJJAVL;
NXP Semiconductors
AN11281
PREV601 Quick Startup Guide
AN11281
All information provided in this document is subject to legal disclaimers.
© NXP B.V. 2013. All rights reserved.
Application note
COMPANY PUBLIC
Rev. 1.510 November 2013
243915
5 of 37
Fig 3. LPC-Link
2.3 Preparation of the hardware
The first step after unpacking the PREV601 board and the LPC-Link board is soldering
the connectors onto the boards in order to attach them. In our example we use a
multipoint connector as one can see on the pictures below.
Fig 4. Multipoint Connectors
One may buy these connectors at any electronic store. Here are some examples [4].
After soldering the connectors, connect the boards as shown on the following figure.
AN11281 3V3 PSU for ' of PRH601 re stor R Ohm has to be assembled .a 37
NXP Semiconductors
AN11281
PREV601 Quick Startup Guide
AN11281
All information provided in this document is subject to legal disclaimers.
© NXP B.V. 2013. All rights reserved.
Application note
COMPANY PUBLIC
Rev. 1.510 November 2013
243915
6 of 37
Fig 5. Connecting the PREV601 board to the LPC Link
Fig 6. LPCXpresso with the Multipoint Connectors
While soldering the connectors onto the board, an opportunity arises to solder either a
bridge or - as shown on Fig 5- a zero ohm resistor near the program interface (R24).
After bridging this connection, you’ll need two instead of three USB cables connected like
shown on Fig 6.
AN11281 «MEIBIIEIQIRQS ‘. I» @ Mounors A \ p Q Network adapters 1, 7 Pans(COM mum x» B anessovs ‘ rrfl 5mm m1 Mada: l; i Sound, wdeo um game tommlkrs x. c- Stung! (ummllm » fl mam dukes a , 6 Unwanl Sena! Bus mnwlkrs ‘ 6 Genuk use Hub 6 Generic use Huh 0 «men: use Hub ‘ ‘ 6 6mm use Hub 6 5mm use Hub ‘ 1 6 1mm 6 Sens/cm Suits Chipsa mm, uss Enhanced Host Controller - 1cm ‘ ‘ 0 1mm 5 Sass/cm Series Cmpset ramiry usa Enhanced Hon (:0me Jan w usa Composnz Dam: ‘ 37
NXP Semiconductors
AN11281
PREV601 Quick Startup Guide
AN11281
All information provided in this document is subject to legal disclaimers.
© NXP B.V. 2013. All rights reserved.
Application note
COMPANY PUBLIC
Rev. 1.510 November 2013
243915
7 of 37
Now the hardware is ready for use.
3. Connecting the hardware to a computer
The guidelines to install the reader are as follows:
Connect the LPC-Link board to a real USB2.0 port of the PC using the mini-USB
connector. The PC detects and installs the board automatically.
Once the board has been installed, open the Device Manager of the PC to check
that the installation has been successful. The item “USB Device with DFU
Capabilities” is being displayed.
After connecting the LPC-Link board, please also connect the second USB connector on
the PREV601 board to the computer. In summary one will need to connect 2 USB cables
(see picture above).
Fig 7. Enumeration of the LPCXpresso Board in Device Manager Window
4. Managing the Demo Reader project with LPCXpresso IDE
The demo reader project is delivered in a zip package. It can be extracted, edited,
compiled and linked with LPCXpresso™ IDE.
LPCXpresso™ is a new, low-cost development platform available at NXP. It supports
NXP's ARM-based LPC microcontrollers. The platform comprises a simplified Eclipse-
based IDE and low-cost target boards which include an attached JTAG debugger.
For development please use the LPCXpresso version 4.x. Newer versions of the
IDE are known not to work correctly with the provided software examples.
AN11281 Wdcome m the LPCXpresso Setup Wizard mmmumuammlmmmm. llslmfllfildedmmdosefloflla meefm mum-:9. Gdflkxtmcnnmmtcmdmexilsemp. h' .nm @— 37
NXP Semiconductors
AN11281
PREV601 Quick Startup Guide
AN11281
All information provided in this document is subject to legal disclaimers.
© NXP B.V. 2013. All rights reserved.
Application note
COMPANY PUBLIC
Rev. 1.510 November 2013
243915
8 of 37
This tool can be freely downloaded from the LPCXpresso website [1]. Before one can
download the software, it is necessary to create an account. Creating an account is
absolutely free.
4.1 Installation of LPCXpresso IDE
The IDE is installed into a single directory, of one’s choice. Multiple versions can be
installed simultaneously without any issues. The installation starts after double-clicking
the installer file. Then click “next” on the setup wizard.
Fig 8. LPCXpresso installation setup wizard 1
Read the license agreement then click next.
AN11281 lbw-2m Em“ mammmmmmemm, mmummwmmmummm mIHannmn-m, commnzcmzommm WWWMWWW Ink [1 Nun—bu m Tfllsmbmlmci AEREEMDI'I ('le‘CE‘HSALEGAI. Ammmrr mm YOU mm A SINGLE INDIVIDUAL, 0: 3mm": lFfiAl Irmrm .wn mmummwmmlrs reran ' an M1 .1" I Ina-g Heatwalfiiekwrstfimmmmwu. 8““ C:\ nm‘fook‘xmw‘amm-efius. [blue ——1 37
NXP Semiconductors
AN11281
PREV601 Quick Startup Guide
AN11281
All information provided in this document is subject to legal disclaimers.
© NXP B.V. 2013. All rights reserved.
Application note
COMPANY PUBLIC
Rev. 1.510 November 2013
243915
9 of 37
Fig 9. LPCXpresso installation setup wizard 2
There are numbers of other screens on the setup wizard but generally the default options
can be accepted. After installation, an information file will be displayed. Click “Next” to
accomplish the installation.
Fig 10. LPCXpresso installation setup wizard 3
After this installation step one will be asked if he wants to install some required drivers.
The installation of these drivers should be accepted.
AN11281 Would you like in inskall ‘his device soflware? Name Code Rm 1mm§ Publ'dulz (at Rs! naming: ud Mmmmmm @- Tthlogiu mr. O Vummmmimmmmmymm Hawanldetidewhidi devim software is 521m imam i CampIeIing the LPCXpresso Setup i Np i m wmmmmmmmwu meninhnuvhehmdbvmmnfled m. i PRESSO: man- an ExtSew. Emu-my“ 62mm Powered by End-Jud 37
NXP Semiconductors
AN11281
PREV601 Quick Startup Guide
AN11281
All information provided in this document is subject to legal disclaimers.
© NXP B.V. 2013. All rights reserved.
Application note
COMPANY PUBLIC
Rev. 1.510 November 2013
243915
10 of 37
Fig 11. Windows Security dialog
After the setup wizard has finished one can launch the newly installed IDE.
Fig 12. LPCXpresso installation setup wizard 4
AN11281 EWvW-kmmrwwm ElEIE u. w my. mm mm a... MW .43, . nzl§fi~ r: ELSE-LLLJJ-‘a a xv an: it 93- th lv»~ “an ’mwhm‘ \lmcflhfiw.‘ ‘ ‘ I} . WM... mnmmu MW . mm .. Mm... “MA“...rmm z “gamma“... uanaAu-emnmam ‘nymanvAAyl-wsmmwwmunuurmwuummummvm . m... mum-aw m wlnaédmww nwnwnuwwumm m. mnmvmwum m v gumm‘ u “my suwmm} Damn-mummy; R “My @ WW“ 5) a: w W 5::th DymmKHdp mm Cm'Shme TIpsanleKks.. Pmdun lfllvllion 5mm < g="" cm="" sum="" numb:="" m1="" anivlle...="" 1..an="" nan="" 3mm...="" '="" '="" mm="" u’cxpressn="" g="" upgrideyou‘r="" mam="" 37="">
NXP Semiconductors
AN11281
PREV601 Quick Startup Guide
AN11281
All information provided in this document is subject to legal disclaimers.
© NXP B.V. 2013. All rights reserved.
Application note
COMPANY PUBLIC
Rev. 1.510 November 2013
243915
11 of 37
Fig 13. LPCXpresso IDE
Directly after the first start of the Eclipse IDE one will see an info dialogue that this is only
an unregistered copy of LPCXpresso IDE. Just confirm the dialog and follow the
instructions on the Welcome Screen to get a registered version without the debug limit of
8k. The registration is free and is needed to navigate to the website of Code Red. The
Link is shown in the menu, Help Product activation Create Serial number and
Activate...
Fig 14. Product activation
AN11281 s —__ Create Serial number and Activate a puss-- mwmmmmmmmeyuum styygmpmd mimmmvfionc Suiahumbu m‘rzewwmxanu‘nm-nmm-m-mfifin ‘ Icwywmmmw Windw Hap am ©"flv‘m'": 5m: 2:; avasv our 7 g Search — Dynamic Help KqusiQ." Qflvshiftvl Tips andTricks... Pmdudmiminn » '2 Displuykmsetype... Suppnlt I: ‘ :r and Amman, mummsonmm, < i:="" ema="" rm="" “code="" %="" ahmnu’cxmsso="" e="" upgradeyourplodud="" 37="">
NXP Semiconductors
AN11281
PREV601 Quick Startup Guide
AN11281
All information provided in this document is subject to legal disclaimers.
© NXP B.V. 2013. All rights reserved.
Application note
COMPANY PUBLIC
Rev. 1.510 November 2013
243915
12 of 37
Fig 15. Product activation
If one doesn’t already have an account at Code Red, please sign up to get an activation
code. The code will be sent to the provided e-mail address.
Fig 16. Product activation
Once the activation code arrives please open the activation window by pointing to Help
Product activation Enter Activation code, and enter the code.
The success of the product activation will be confirmed by an info dialogue.
4.2 Extraction of the demo reader project
Once the LPCXpresso™ IDE has been installed on a computer, the sequence of
installing the reference reader project is indicated:
Start the LPCXpresso™ IDE.
Select the option “Import project(s)” (see picture below).
Browse the zip archive.
LPCXpresso™ IDE unzips the software package.
AN11281 mm mm, a.“ V i“: H mm ‘ MA». ~ xii-2mm Emma-x Emu:- numy SMY-ulhm mmmmw} V Efi-Ez-‘rsm 7' 4 , m g flwuugg 37
NXP Semiconductors
AN11281
PREV601 Quick Startup Guide
AN11281
All information provided in this document is subject to legal disclaimers.
© NXP B.V. 2013. All rights reserved.
Application note
COMPANY PUBLIC
Rev. 1.510 November 2013
243915
13 of 37
The software package is ready for use.
Fig 17. Importing a project into the LPCXpresso IDE
In the Quick Panel on the left hand side, choose “Import projects(s)”.
AN11281 , , , ,._._ Impnn pm‘EEI(S) E" seed m mmybalflfiw Me (a man A m1“ ave {untamed wnhmardfws a.» a! m unpxbd mm adwennry. Seku your Mamamhm a! m dynasty and was < um="" .="" on="" m:="" m:="" i139:="" mmmme="" med:="" yuu="" “a="" ”wm="" 2nd="" wm="" 4mm,="" mm="" "(hm="" (up;="" mm:="" c\rmfi}?m|mgup="" ‘="" 5m”="" mm="" mummy="" (.1..po="" m="" ”satay="" am"="" m:="" fur="" mm="" mmpla="" mm="" “dmglav="" mmmmpug="" mm.="" m="" lam="" mum="" m="" dumnlaidln="" yam="" ‘nzi‘="" am="" thank="" pm="" “5mm="" ,-="" mm)”="" .mpmmymwmm="" 5="" "“5““="" ”‘9“="" 7="" 1="" 1="" |mpnnpmjm1(1)="" 2mm:="" e="" mam“="" mmxrvoum)="" ’="" gopy="" pm'ecs="" mm="" wmtspm="" 37="">
NXP Semiconductors
AN11281
PREV601 Quick Startup Guide
AN11281
All information provided in this document is subject to legal disclaimers.
© NXP B.V. 2013. All rights reserved.
Application note
COMPANY PUBLIC
Rev. 1.510 November 2013
243915
14 of 37
Fig 18. Importing a project into the LPCXpresso IDE
Browse the desired project and click “Next”.
Fig 19. Importing a project into the LPCXpresso IDE
When the import process has finished one can start browsing the code. Most interesting
might be the main.c which is located in ../src/main.c in the project.
Before one can run the project, the PREV601 board with the PRH601 needs to be
connected to the computer. Wait until the adequate drivers have been installed.
AN11281 mun» my mums-“Luau. Ir“ '4' {21 ~ ~ {My mynggfl =u" \ —u mum g wuss I am I m. (MW m mm .h (my): - manna“; , mm. a "m 9 mun be»; m... - man. an n Mscxlnen :exeu - m “Manna Mme, I...» xtsmnnzlhn v mum, to: m r K m». aancannn um he swab): m m speuneu ‘ mm” begun; c: mamncazlcn. . gm mm m. a m m & hwmpruxds! Wflww m w ‘umwmw m 323$ $3,323.: étanwk 2?\ mm” In mmammom flammukswdwxjhnhmn ‘m, ‘ Wm M... mumum 37
NXP Semiconductors
AN11281
PREV601 Quick Startup Guide
AN11281
All information provided in this document is subject to legal disclaimers.
© NXP B.V. 2013. All rights reserved.
Application note
COMPANY PUBLIC
Rev. 1.510 November 2013
243915
15 of 37
4.3 Start the project
One can quickly start the reader project by editing the main function in the module
main.c. This function first performs the hardware initializations of the LPC1227 and the
RF transceiver RC663.
Detailed descriptions of the code in the form of comments have been provided in the
main.c file. This should provide a detailed overview of how to initialize certain
components and get data out of and onto the card in the RF field.
4.3.1 Run the project
Before running the project, please ensure that the LPCXpresso with the Blueboard is
connected to the computer.
Fig 20. Run the project
Choose the desired project and click the Debug Button on the left hand side as shown in
the example picture.
AN11281 Bummms-flmmm :‘Jfl na/twv ma mnaaw‘um a :~ My 3 ~ m-m or ,» ,.,. (.1...‘ =n mwm‘ =n- m. ”mm; s a naacxlsclun m, In: mm.“ nu. mu! 5: n a." u d=acubm Mrs)" H m m“ m: “mm CM), mm pzcvxdty mm": .m “mm...” mfnunaum mum, m m a m “mm. mm; m linen-e M e m: any 9-; mwxm: u: ask um mm m m M . m Smcumutcoxs mum m man: u .m mm. n. m m .m mum.“ mm“ char am mum,“ wall D: m m m ammix=n m mm: mm.“ cu no u mmmm. z. (. mum“, m mum mm, vs . acwmkgmnm‘sunnm at \flnfinmavnvfll _ cum», ‘ arm-nun: pnflrnuun nap- ‘ errmHm W:wumq..m um.rm,chm 4) may msshmnqufl uiiarmu‘MJm ; um... rn mung“ 7n ncsiarsunmaJnn; :_rmrm,¢]my 4. m “mm.“ x m... m ‘ m m m m. . WNW, Crzuud mum nusd > Fvlllanun m. affltz m: [I Wmmmaw E‘fi mum mam/3m = _ ‘ w "m“ w 1/......0...n...n..............n..."a...............................n... ... 2 - 51m: )2c_na)n.c 3 - pzmecc: pr chuxx 12c exallvle 5 - Descxlpnan: e « Thu tile cnnLAu-m mam entry. zlid‘k ”CM :5 only Lng the mixes. x the acencx tax: or )fled E le: 23"\ I}; mums] II Manny} D mnmm 0 9 E‘ :5 SE Em r: C-Bnild [REED-Pulling] 8 M91: 37
NXP Semiconductors
AN11281
PREV601 Quick Startup Guide
AN11281
All information provided in this document is subject to legal disclaimers.
© NXP B.V. 2013. All rights reserved.
Application note
COMPANY PUBLIC
Rev. 1.510 November 2013
243915
16 of 37
Fig 21. Run the project
After the build process one can see the size of the image in the console window.
Fig 22. Run the project
The initialization of the LPC-Link can take a few seconds.
AN11281 lemma-am WMMMMM ran J3 dolfifiv 31a mammsnm a §~ su ‘ a— sv . \vlc tlv a.” unco‘gk‘ =a"¢m..,:; awn: .m. \ E.” ammwmmm u gm w” ”mama. h “mm 4 {wmjfumuow m , _ m, . 3...“, om“ \ ==- 2 n m 129m: s m 3 o W mmm mm xmm hexem u m magma Dukcses my - n aml‘ed us 15' uxchw' m “mum ‘ Solcu-xe co.c 13 4: product: n.” m‘ woman, or my Ema: mmnm‘gmnflm IxfoiElfiD‘r'EvrfiV‘T" mm mm” mwycwwmm,us)mmw an IQ cm or ”q muncun . In om a: w; “(amen Ila mud or m dkxuzzzd mm mmum mo «5:ch mm. mm...» m omcm Ll ECMXK EWWDW13wnxohm‘ lxis‘mEF-‘fl‘flfl'fi'Efi mum", comma. WW) QUMSVWWMJDSJEWVWMVPH no mm a: rag detected . no card at no flattered no cam or tag dttecred no can Dr :39 dettcttd no cam at cm] detected no card or Izaq flattered leare filtraquhI: cam dtrected foare murauqh: card ammo g mwungam _ o . - a. 37
NXP Semiconductors
AN11281
PREV601 Quick Startup Guide
AN11281
All information provided in this document is subject to legal disclaimers.
© NXP B.V. 2013. All rights reserved.
Application note
COMPANY PUBLIC
Rev. 1.510 November 2013
243915
17 of 37
Fig 23. Run the project
After the software upload, the execution of the project starts immediately.
Fig 24. Run the project
In the console window at the bottom one will see the debug output of the execution.
AN11281 mmmumvwmmmmw ram J3 fislfifiv 313 mflh‘iifi‘fln‘.‘ O Sv SQ § 3— ~ \v‘e aw A ,. v ww:»fil>\ m»: "‘ng =a‘tws EIV Em wgmlclc”ucuw~mq A gm A enummwm u Wm,“ .- nmmwm» V “I" ‘ m ,_ www-mmwv m , am. “My 413 mm m DSK ; ./ DW,M-
NXP Semiconductors
AN11281
PREV601 Quick Startup Guide
AN11281
All information provided in this document is subject to legal disclaimers.
© NXP B.V. 2013. All rights reserved.
Application note
COMPANY PUBLIC
Rev. 1.510 November 2013
243915
18 of 37
Fig 25. Stop the project
After the execution has reached the end of the main function please click the Terminate
button to stop the execution. Otherwise one won’t be able to rerun the project.
One can now do the following with the buttons near the top of the “Debug” view:
Run the program.
Step over C/C++ line.
Step into a function.
Stop the debugger.
Pause execution of the running
program.
Instruction stepping mode
(disassembly).
Fig 26. Debug Buttons
AN11281
NXP Semiconductors
AN11281
PREV601 Quick Startup Guide
AN11281
All information provided in this document is subject to legal disclaimers.
© NXP B.V. 2013. All rights reserved.
Application note
COMPANY PUBLIC
Rev. 1.510 November 2013
243915
19 of 37
5. Associated Projects
5.1 Communication with MIFARE Ultralight
Based on examples the MIFARE Ultralight project shows how read-write access can be
achieved on this type of card.
If one uses a card which is not write protected or secured the example program writes a
valid NDEF message onto the card. One can read this message with any NFC enabled
mobile phone which can read NDEF messages.
5.2 Communication with MIFARE Classic
Based on examples this project shows how read-write access can be achieved on this
type of card.
5.3 Communication with MIFARE DESFire
Based on examples this project shows how read access can be achieved on this type of
card.
5.4 Polling
Based on examples this project shows how to initiate a basic communication with the
following cards:
MIFARE Ultralight
MIFARE Classic
MIFARE Plus
MIFARE DESFire
FeliCa compliant cards
ISO/IEC 14443-B cards
ISO/IEC 15693 Tags
This example project also looks for cards in range of the RF field in a continuous loop
and returns the type of the detected card or tag to the console window.
5.5 Peer to Peer functionality
Based on examples this project shows an implementation of Peer to Peer (P2P)
functionality.
Because the P2P implementation is still in alpha phase, one will find very rudimentary
support for the protocol.
At the moment the project supports the communication via the SPI protocol and runs on
the LPCXpresso LPC1227 development board.
5.5.1 Installation
After downloading and unpacking the zip file, please run the installer. The installer just
copies the LPCXpresso project files to the file system. After the installation has finished,
please run the included batch file located in the installation directory
…\NxpRdLibP2PExtensions-x.x.x\NxpRdLib_P2PExtensions\ex\Rc663_Lpc12xx_P2P_Demo
After the batch file has been executed successfully, please start the LPCXpresso IDE
and import the project. Browse to the root of the installation directory.
AN11281 sum m ample; mm: m: a: "mu, pm In comma mm mm: (11p) 51 m mum min . dreamy. swam Wu Inhwe nr m1 dimory m1 pier (Man). On m net my: mm mm pmkds ynn mu m mm. indpv— mm». mm mm (in) 37
NXP Semiconductors
AN11281
PREV601 Quick Startup Guide
AN11281
All information provided in this document is subject to legal disclaimers.
© NXP B.V. 2013. All rights reserved.
Application note
COMPANY PUBLIC
Rev. 1.510 November 2013
243915
20 of 37
Fig 27. Importing the project
After the import there are two new projects in the workspace - one for the use with the
RC663 Blueboard or PREV601 board and one for the use with the PN512 board.
Basically these two projects provide the same functionality.
5.5.2 SNEP client project
In this project the PREV601 board behaves like SNEP client with performing the Put
request functionality only [14][14]. On the other side there must be a device peer
capable of NFC communication and providing the SNEP server service. These
conditions are fulfilled by a mobile device with Android platform (4.0 or later).
Here is a short instruction list how to use the SNEP client software:
1. Run the SNEP client project as described in section 4.3.1 with respect to
LPC1227 microcontroller restriction and hardware configuration in section 6.4.
2. Hold your NFC device (smartphone) approximately 5 centimeters above antenna
of the PREV601 board.
3. Once the NFC detected in the RF field of the transmission of the NDEF message
is started. You may be notified by a sound or vibration of your device. The
transmission may take several seconds depending on the size of the NDEF
message. Hold your NFC device in range of PREV601 board’s field during entire
transmission.
4. After transmission completed there should be the transmitted image displayed in
the device’s screen.
5.5.2.1 What is going on inside?
The SNEP client sends a hardcoded NDEF message encapsulated in a SNEP message
to the NFC device. Thanks to the SNEP client project implements the P2P Reader
Library Extension compliance with the LLCP and ISO18092 protocols on the PNEV512-
Board’s side are ensured, implicitly a correct SNEP client-server communication.
Execution of the SNEP client software can be summarized in following steps:
1. Hardware initialization
AN11281
NXP Semiconductors
AN11281
PREV601 Quick Startup Guide
AN11281
All information provided in this document is subject to legal disclaimers.
© NXP B.V. 2013. All rights reserved.
Application note
COMPANY PUBLIC
Rev. 1.510 November 2013
243915
21 of 37
2. Detecting the RF field for an NFC peer of the tag type F.
The software checks the RF field whether there is tag type F capable of
performing the P2P communication
3. Once such device is found, the LLC link is activated in compliance with the
procedure defined by the NFC forum [15].
4. LLCP socket creation and establishing connection with other peer SNEP
server.
5. Transmission of a given image file to the SNEP server:
The SNEP client sends an initial fragment 128 bytes long. Then it waits for a
response from the server. Because in SNEP header it is declared longer
SNEP message than one fragment, the server should response with the
Continue response. The SNEP client can go on with sending the rest of the
SNEP message. As soon as the entire SNEP message has been transmitted,
the SNEP client shall receive the SNEP Success response from the mobile
device and the transmitted picture should be immediately displayed on the
mobile’s screen.
The SNEP client software is deeply described in [13] in Sample code.
5.5.2.2 Choosing the NDEF message
By default the software sends image of the NXP logo as NDEF message. There are
more NDEF messages prepared in dedicated header files (see Table 1). Only a single
header can be compiled with the SNEP client application. To choose another content of
the NDEF message for transmission just follow the instructions below. In case of URI or
text message just skip from step 1 to step 4 (steps 2 and 3 are for selection of an image).
Concurrently with instructions there are parts of source code to demonstrate choosing of
hardcoded PNG image file for transmission.
1. Open for editing the source file ndef_message.c located in folder src/.
2. Uncomment the line with content a header file to be transmitted. Let all the other
lines commented.
/* select the required type of transported data */
//#include <c_tabletxt.h>
#include <c_tablepng.h>
//#include <c_tablepng_NXP_QR.h>
//#include <c_tablejpg_NXP_logo.h>
3. In Table 1 in the same row as the chosen file look up two identifiers
corresponding to the chosen file.
4. In the array
nmess[]
uncomment the line with the couple of identifiers
corresponding to the type of the chosen file. Comment all the other lines.
5. Save the changes and recompile the project.
NDEF_messages n_mess[]={ /* type, parameter, string */
// {NDEF_TYPE_IMAGE,NDEF_IMAGE_JPEG,c_table, sizeof(c_table)},
{NDEF_TYPE_IMAGE,NDEF_IMAGE_PNG,c_table, sizeof(c_table)},
// {NDEF_TYPE_IMAGE,NDEF_IMAGE_TIFF,c_table, sizeof(c_table)},
// {'T', LANG_NO, text1, sizeof(text1)},
// {'T', LANG_EN, c_table, sizeof(c_table)},
// {'T', LANG_EN, text1, sizeof(text1)},
AN11281 My Slur: Rmz Raw mm tux: (cm; Party) m DODE ILT .a 37
NXP Semiconductors
AN11281
PREV601 Quick Startup Guide
AN11281
All information provided in this document is subject to legal disclaimers.
© NXP B.V. 2013. All rights reserved.
Application note
COMPANY PUBLIC
Rev. 1.510 November 2013
243915
22 of 37
Table 1. Table of files prepared for NDEF message transmission
Identifiers from the last two columns are necessary for choosing the right line from
n_mess[]
.
Content Header Name
NDEF message
identifier
File type
identifier
PNG image
c_tablepng.h
NDEF_TYPE_IMAGE
NDEF_IMAGE_PNG
QR code of NXP
c_tableQR.h
NDEF_TYPE_IMAGE
NDEF_IMAGE_PNG
Image of NXP logo
c_tablenxp.h
NDEF_TYPE_IMAGE
NDEF_IMAGE_JPEG
Long text message
c_tabletxt.t
‘T’
LANG_EN
6. Supplementary Notes
6.1 Software architecture
The software of the reference reader is based on the NXP reader library [5]. It intends to
be simple, modular, easily readable and quickly portable by all the customers. This
philosophy is reflected in its architecture which is divided in 4 layers:
BAL (Bus Abstraction Layer),
HAL (Hardware Abstraction Layer)
PAL (Protocol Abstraction Layer)
AL (Abstraction Layer)
Fig 28. Architecture of the NXP reader library
AN11281
NXP Semiconductors
AN11281
PREV601 Quick Startup Guide
AN11281
All information provided in this document is subject to legal disclaimers.
© NXP B.V. 2013. All rights reserved.
Application note
COMPANY PUBLIC
Rev. 1.510 November 2013
243915
23 of 37
6.1.1 Bus abstraction layer
This layer offers functions to abstract the hardware parts of the LPC1227 microcontroller.
These functions use the specific libraries available for the LPC1227 family
microcontroller. Based on these stacks, the communication routines for the relevant
physical media I2C/SPI can be easily designed. These drivers are specific for the
LPC1227 family and therefore cannot be ported to other microcontrollers.
6.1.2 Hardware abstraction layer
This layer offers functions to abstract the hardware parts of the transceiver RC663.
6.1.3 Protocol abstraction layer
Every PAL function is a low level function realizing a single functionality. It is
encapsulated in a module. Every function is independent from the others. The user can
easily design his application by doing a drag-and-drop of the relevant module.
The following PAL modules are available in this software package:
ISO/IEC 14443-3A,
ISO/IEC 14443-3B,
ISO/IEC 14443-4A/B,
MIFARE,
ISO/IEC15693,
FeliCa,
NFC Initiator
6.1.4 Application layer
Lying on the previous software layers, the application layer is on top of the reader
software package. It combines elements from the previous three parts into high level
functionalities.
For more details on the NXP reader library, the reader is invited to refer to the document
RC663 Software Design Guide of the NXPRDLib [6].
6.2 Build configuration
This project comprises 2 build configurations:
Debug configuration
This configuration is mainly used when the target board is attached to the PC with
the JTAG debugger. It allows the display of debug messages in the console window,
which is useful in the early stage of the project.
Release configuration
Once the project is debugged and mature, it might be interesting to use the release
configuration, to use the hardware stand alone. No debug messages are displayed in
the console window.
Note, that only in Release Configuration one can flash the software onto the
Blueboard and start it automatically, once power has been attached to the board.
The build configuration can be selected as follows:
Click on the project in the project window of the LPCXpresso™ IDE,
AN11281 2 ~ 5m a2c_mun.c 'mjecc: uxp LPClex 12c example » 1> . sexlpclon: V Tlu: file contains mun entry‘ :> v ...........m.................................. . Link: an: n descrxhtd nexem 1: far: lllustrm .m pmvme: cusmeu um: programng infamy " “I“ ”4* Imuse mu software u supplied as Is- wmm Mme... - Saucondllccor: name: no nswneamncy a: 1. [> m a of ch: sofcuaze, canny: no ncense an age . 1> .yrlghlz, or mask Hark :lth. :0 ch: product. m ,, .\_-. mm. ewe: me :1th no make changes :11 the sofcunn D '4 Bum— xlxcatxon‘ uxp Semxcondllccax: also make no [em "my mac such lellc-cion um be sun-me n WW ulthaul: further c=scinq or mndlflcacion. , ............................................... m 5 mxnan: a: umcn dxxvex: we cum I: up have emblem Clw Unvdlkd PM ‘ 5" W “I" W“ “3'" “'3 mum d ~ MW > \ saw v v lmmm ‘ Manny‘s > Manage. zmmm m > I c and» c m. : A. .der defuuclon -/ , M“ ' WW— 1 Purpose Input/Output) fi Ddugh , [—1 37
NXP Semiconductors
AN11281
PREV601 Quick Startup Guide
AN11281
All information provided in this document is subject to legal disclaimers.
© NXP B.V. 2013. All rights reserved.
Application note
COMPANY PUBLIC
Rev. 1.510 November 2013
243915
24 of 37
Right click of the mouse Select build configuration,
Set active Debug build (or Release build).
Fig 29. Select the build configuration
6.3 Level of compiler optimization
When the code size at the current compiler level overloads the FLASH size of the target
board (128K for the ARM-based microcontroller LPC1227), a higher compiler
optimization level can be selected to reduce the code size of the project.
The following steps can be followed to select a level of compiler optimization:
Click on the project in the project window of the LPCXpresso™ IDE,
Right click of the mouse Select properties Select C/C++ build,
Select Settings Optimization,
Choose the desired level in the combo box.
AN11281 Semi-q: MW \mgm, IT mm ; mwliwuix‘m, gnaw; WM WWII-n- mm \L‘ [ENE 37
NXP Semiconductors
AN11281
PREV601 Quick Startup Guide
AN11281
All information provided in this document is subject to legal disclaimers.
© NXP B.V. 2013. All rights reserved.
Application note
COMPANY PUBLIC
Rev. 1.510 November 2013
243915
25 of 37
Fig 30. Select the level of optimization
6.3.1 Optimization issues
When optimization is enabled, it will reorder code. What this means is that the code from
multiple C lines will be intermingled. In addition, assignments and initializations might be
pulled out of loops so they are only executed once. Changes like these will make the
code confusing to debug. Some symptoms one might see are breakpoints that only work
the first time through, or seeing the debugger’s current line indicator fail to advance or
even move backwards when clicking step. It is best to always use O0 for debugging.
Since optimization can make such a big difference in code size and performance, it is a
good idea to test the project with code optimization on, and plan for a final build that is
optimized.
AN11281
NXP Semiconductors
AN11281
PREV601 Quick Startup Guide
AN11281
All information provided in this document is subject to legal disclaimers.
© NXP B.V. 2013. All rights reserved.
Application note
COMPANY PUBLIC
Rev. 1.510 November 2013
243915
26 of 37
6.4 Hardware configuration and SPI usage
The hardware configuration selection of PRH601 is located in the header file
hw_config.h. The file is located in …/lpc1227/. The bus interface is configured in header
file ph_NxpBuild.h located in …/src/NxpRdLib_PublicRelease/types/.
6.4.1 Hardware configuration
The configuration file hw_config.h provides the following settings:
6.4.1.1 PREV601 board type definition
/* -----------------------------------------------------------
* Definition of the used board.
* If nothing is defined, we assume the CLEV663B board is meant
* ----------------------------------------------------------- */
#define BOARD_PRH601
#ifdef BOARD_PRH601
#define PREV601M
#endif //BOARD_PRH601
The preprocessor directive BOARD_PRH601 activates the pin configuration according to
the hardware layout of the PREV601 board. Each pin setting has its own #define.
(SSP_CLK, SSP_MOSI, …)
Beside the PREV601 board, the software also supports the smaller Microboard
(PREV601M). To activate the appropriate hardware configuration, one just needs to
uncomment the
#define
PREV601M
. Like the PREV601 board, the Microboard also contains
the integrated reader module PRH601HL.
In respect to the software, there are two main differences. As opposed to the PREV601
board, the Microboard uses its internal clock oscillator for the system clock generation.
The second difference concerns the Rx threshold register which depends on the antenna
pattern. (see chapter 6.5)
6.4.1.2 Reading IC or board type
/* -----------------------------------------------------------
* reading IC or board type
* ----------------------------------------------------------- */
#ifndef BOARD_PRH601
/* TUSA board cannot be used if PRH601 board is set */
//#define TUSA // definition TUSA card reader instead of BlueBoard
#endif // BOARD_PRH601
Because the software projects provided with the PREV601(M) boards are preconfigured
for the use with the LPC1227 micro controller, the TUSA board cannot be used with
these projects. For more information about this reader module from SILICA, please refer
to the quick start guide for the CLEV663B evaluation board [12].
6.4.1.3 Low Power Card Detection mode (LPCD) definition
/* -----------------------------------------------------------
* low power mode (LPCD) definition
* ----------------------------------------------------------- */
#ifndef TUSA
/* not allowed for TUSA baord type */
#define LOW_POWER_MODE /* allow implementation of LPCD mode (low power card
detection)*/
#endif
AN11281
NXP Semiconductors
AN11281
PREV601 Quick Startup Guide
AN11281
All information provided in this document is subject to legal disclaimers.
© NXP B.V. 2013. All rights reserved.
Application note
COMPANY PUBLIC
Rev. 1.510 November 2013
243915
27 of 37
The #define LOW_POWER_MODE allows and switches the application into the Low
Power Card Detection (LPCD) mode. This setting is not available for TUSA board. The
LPCD mode directly works with the reader IC CLRC663 (note: there are some more
reader ICs with LPCD functionality)
6.4.1.4 Communication interface definition
The bus interface is configured via #defines in ph_NxpBuild.h in the directory
src/NxpRdLib_PublicRelease/types/.
/* BAL components */
#define NXPBUILD__PHBAL_REG_STUB /**< Stub BAL definition */
//#define NXPBUILD__PHBAL_REG_SERIALWIN /**< SerialWin BAL definition */
//#define NXPBUILD__PHBAL_REG_PCSCWIN /**< PcscWin BAL definition */
//#define NXPBUILD__PHBAL_REG_RD70XUSBWIN /**< Rd70X_UsbWin BAL definition */
The #define NXPBUILD__PHBAL_REG_STUB is prerequisite for enabling any type of
bus connection between MCU and reader chip.
/* BAL uC components */
#if defined (NXPBUILD__PHBAL_REG_STUB)
#define NXPBUILD__PHHAL_HW_BUS_SPI /**< SPI Bus definition */
// #define NXPBUILD__PHHAL_HW_BUS_I2C /**< I2C Bus definition */
// #define NXPBUILD__PHHAL_HW_BUS_UART /**< UART Bus definition */
#if defined (NXPBUILD__PHHAL_HW_BUS_SPI) || \
defined (NXPBUILD__PHHAL_HW_BUS_I2C) || \
defined (NXPBUILD__PHHAL_HW_BUS_UART)
#define NXPBUILD__PHHAL_HW_BUS /**< Generic BUS uC definition */
#endif
#endif
The #defines NXPBUILD__PHHAL_HW_BUS_SPI and
NXPBUILD__PHHAL_HW_BUS_I2C control the communication interface between the
microcontroller LPC1227 and reader IC CLRC663. Each define does small adaptations in
the files lpc1227/ph_HwBus.c and lpc1227/ph_HwBus.h.
Further interface setting for the PREV601 board are described in chapter 6.4.2.
6.4.1.5 Debug printout definition
/* -----------------------------------------------------------
* debug printouts definition
* ----------------------------------------------------------- */
#ifdef LOW_POWER_MODE
#define DEBUG_PRINT_LPCD // print debugging for LPCD mode
#define DEBUG_PRINT_LPCD_2 // register printing during LPCD mode debugging
#define Q_I_DEBUG_PRINT
#endif //LOW_POWER_MODE
The defines DEBUG_PRINT_LPCD, DEBUG_PRINT_LPCD_2 and Q_I_DEBUG_PRINT
allows to activate different levels of debug output about the LPCD mode.
6.4.2 Usage of the SPI interface
Because of the hardware design, the PREV601 board can only use the SPI interface for
the communication between the microcontroller LPC1227 and the reader IC CLRC663.
Nevertheless one may use the I²C interface in a different hardware design with the same
integrated reader module.
The SPI selection is described in the chapter 6.4.1.4.
AN11281 The sofiwale sets the power down time to films and field detection time to 150us. .a 37
NXP Semiconductors
AN11281
PREV601 Quick Startup Guide
AN11281
All information provided in this document is subject to legal disclaimers.
© NXP B.V. 2013. All rights reserved.
Application note
COMPANY PUBLIC
Rev. 1.510 November 2013
243915
28 of 37
The defines regarding the SPI interface are as follows:
#define SSP_CLK PIO0_14
#define SSP_MISO PIO0_16
#define SSP_MOSI PIO0_17
#define SSP_SSEL PIO0_15
The pin SSP_SSEL is set to the typical GPIO mode and the selection is performed
directly from the SPI driver. The remaining three pins are set to SPI mode.
The pins for the selection of the communication interface are as follows:
#define PIN_IFSEL0 18 // select pin to define com. interface type for RC663
#define PIN_IFSEL1 19 // select pin to define com. interface type for RC663
Based on the datasheet of the reader IC CLRC663 [2] the pins have to be set as follows:
/* Select SPI link -> IFSEL0 = 0 & IFSEL1 = 1 */
The RESET pin, or better power down pin, of the reader IC CLRC663 is defined as
follows:
#define PIN_RESET 20 // PDOWN - pin for power down/reset of RC663
6.5 LPCD mode configuration
The reader IC CLRC663 is capable to operate in low power card detection mode. This
mode is an energy saving mode intended for use cases where the CLRC663 is required
to consume minimum current during polling, e. g. for systems powered by battery.
The LPCD feature is independent from the used smartcard/tag communication protocol.
Please consult the more detailed application note about the LPCD [11].
The LPCD operates in two phases. The first is the standby mode, controlled by the wake
up timer T4. This timer defines the standby duration of the CLRC663 reader IC. The
second phase is the detection time. In case that during the detection time an influence of
the RF field is recognized, the values of the I and Q channel are stored to the assigned
registers and compared with the calculated thresholds.
In case the values of the I and Q channel exceeds the thresholds, the LPCD operation
stops and the system continues with the appropriate program flow.
A detuning of the RF field and a resulting stop of the LCPD mode can be evoked by any
metallic object.
In the Polling projectthe implementation returns into LPCD mode if communication with
a supported card or tag cannot be established.
The software sets the power down time to 10ms and field detection time to 150us.
That means that the LPCD detection works at 100Hz (in accordance to [11]).
6.5.1 Library support
The LPCD operation is also supported by the NxpRdLibrary by the following two
functions from the phhalHw_Rc663.c software module:
The function phhalHw_Rc663_Cmd_LpcdConfig() takes values of the I and Q field
registers.
phStatus_t phhalHw_Rc663_Cmd_LpcdConfig(
phhalHw_Rc663_DataParams_t * pDataParams,
uint8_t * pI,
uint8_t * pQ
AN11281 37
NXP Semiconductors
AN11281
PREV601 Quick Startup Guide
AN11281
All information provided in this document is subject to legal disclaimers.
© NXP B.V. 2013. All rights reserved.
Application note
COMPANY PUBLIC
Rev. 1.510 November 2013
243915
29 of 37
)
The function phhalHw_Rc663_Cmd_LpcdConfig() performs the LPCD functionality. The
input parameters set the I and Q registers, power down time and the detection time. The
parameter bMode sets the type of the LPCD (one time operation or cycling operation)
phStatus_t phhalHw_Rc663_Cmd_Lpcd(
phhalHw_Rc663_DataParams_t * pDataParams,
uint8_t bMode,
uint8_t bI,
uint8_t bQ,
uint16_t wPowerDownTimeMs,
uint16_t wDetectionTimeUs )
6.5.2 LPCD software usage
The reader IC CLRC663 indicates the LPCD card detection via the IRQ1 register
(address 07h), bit 5 (LPCD_IRQ). See reference [2]. The additional functionality is an
interrupt signal generation at pin 32 (IRQ - interrupt request). But this additional
functionality is not yet supported by the NxpRdLibrary.
The following snippet describes the standard LPCD mode setting and detection.
void *pHal;
/* BFL (Basic Function Library) data parameter storage */
phbalReg_Stub_DataParams_t balReader;
phhalHw_Rc663_DataParams_t halReader;
/* Initialize the Reader HAL (Hardware Abstraction Layer) component */
status = phhalHw_Rc663_Init(
&halReader,
sizeof(phhalHw_Rc663_DataParams_t),
&balReader,
0,
bHalBufferReader,
sizeof(bHalBufferReader),
bHalBufferReader,
sizeof(bHalBufferReader));
/* Set the generic pointer */
pHal = &halReader;
#ifdef LOW_POWER_MODE
uint8_t bI_Register;
uint8_t bQ_Register;
#endif // LOW_POWER_MODE
……..
#ifdef LOW_POWER_MODE
debug_printf(" -------------------------- ");
debug_printf(" --- LPCD configuration --- ");
PH_CHECK_SUCCESS_FCT(status, phhalHw_Rc663_Cmd_LpcdConfig(pHal,
&bI_Register, &bQ_Register));
AN11281 37
NXP Semiconductors
AN11281
PREV601 Quick Startup Guide
AN11281
All information provided in this document is subject to legal disclaimers.
© NXP B.V. 2013. All rights reserved.
Application note
COMPANY PUBLIC
Rev. 1.510 November 2013
243915
30 of 37
#ifdef DEBUG_PRINT_LPCD
debug_printf("\n --- register I= ");
debug_puts_hex(bI_Register);
debug_printf("\n --- register Q= ");
debug_puts_hex(bQ_Register);
#endif // DEBUG_PRINT_LPCD
debug_printf(" --- LPCD detection --- ");
PH_CHECK_SUCCESS_FCT(status, phhalHw_Rc663_Cmd_Lpcd(
pHal,
PHHAL_HW_RC663_CMD_LPCD_MODE_POWERDOWN,
bI_Register,
bQ_Register,
10, // power down time
150)); // operation time
debug_printf(" --- field activated ---");
#endif // LOW_POWER_MODE
6.5.3 The I and Q Register settings
The values of the I and Q channel are detected and stored in the register map:
42h LPCD_I_Result Low-power card detection I channel result register
43h LPCD_Q_Result Low-power card detection Q channel result register
At the beginning the values for the empty field, rather for the initial conditions, are stored
in these registers.
The detection threshold levels are calculated from the values of the I and Q registers.
Registers LPCD_IMin_Reg, LPCD_IMax_Reg; LPCD_QMin_Reg and PCD_QMax_Reg
are written to, and stored in the follow registers:
3Fh LPCD_QMin Low-power card detection Q channel minimum threshold
40h LPCD_QMax Low-power card detection Q channel maximum threshold
41h LPCD_IMin Low-power card detection I channel minimum threshold
NOTE: LPCD_Imax is stored at the highest bit of these 3 registers. See [2].
The detection thresholds are calculated in the following area of the NxpRdLibrary:
…\src\NxpRdLib_PublicRelease\comps\phhalHw\src\Rc663\phhalHw_Rc663_Cmd.c
Snippet starting at line 180.
/* Calculate I/Q min/max. values */
bQMin = bQ - 1;
bQMax = bQ + 1;
bIMin = bI - 1;
bIMax = bI + 1;
/* Set Qmin register */
bRegister = bQMin | (uint8_t)((bIMax & 0x30) << 2);
PH_CHECK_SUCCESS_FCT(statusTmp, phhalHw_WriteRegister(pDataParams,
PHHAL_HW_RC663_REG_LPCD_QMIN, bRegister));
/* Set Qmax register */
bRegister = bQMax | (uint8_t)((bIMax & 0x0C) << 4);
AN11281 37
NXP Semiconductors
AN11281
PREV601 Quick Startup Guide
AN11281
All information provided in this document is subject to legal disclaimers.
© NXP B.V. 2013. All rights reserved.
Application note
COMPANY PUBLIC
Rev. 1.510 November 2013
243915
31 of 37
PH_CHECK_SUCCESS_FCT(statusTmp, phhalHw_WriteRegister(pDataParams,
PHHAL_HW_RC663_REG_LPCD_QMAX, bRegister));
/* Set Imin register */
bRegister = bIMin | (uint8_t)((bIMax & 0x03) << 6);
PH_CHECK_SUCCESS_FCT(statusTmp, phhalHw_WriteRegister(pDataParams,
PHHAL_HW_RC663_REG_LPCD_IMIN, bRegister));
6.5.4 What to do if the PREV601 board does not stay in LPCD mode
If the CLRC663 often leaves the LPCD mode without any metallic object being put into its
RF field, a solution may be to enlarge the detection thresholds from +/- 1 to +/-3 or +/-4.
The following code shows an example:
File …\src\NxpRdLib_PublicRelease\comps\phhalHw\src\Rc663\phhalHw_Rc663_Cmd.c
Snippet starting at line 180.
/* Calculate I/Q min/max. values */
bQMin = bQ - 3;
bQMax = bQ + 3;
bIMin = bI - 3;
bIMax = bI + 3;
AN11281 D Jug" . p G dnvu Gnlnho p a linker ‘7 8 “my OpeninNewWindow " 6 5" E Co cm~c b 9 stamp [Q W I) a (my; Fan: CHI“! x Dela: Dem Mm." “W" H F: Probkmsfl] Memory\ 3 Redexe .\-_. lmpm... yo disphy mhusum 2 awn“ E 51mm u a New plojedm W“ PM!“ . Clean Project & Impon mm“ 0 mm. F5 elm projm ‘ 8"“ Rafi," Close Unvelma Projeds / Chin 'Rcw-p Buiid Carflgurmm , it Debug R666}? Mikael?!“ b Ind: , CowenTom RnnAs , DebugAs » Pmfil: As Tum fawn: wm. ‘ Launch Configumms » i Cram Liam. Cunfigmmns 37
NXP Semiconductors
AN11281
PREV601 Quick Startup Guide
AN11281
All information provided in this document is subject to legal disclaimers.
© NXP B.V. 2013. All rights reserved.
Application note
COMPANY PUBLIC
Rev. 1.510 November 2013
243915
32 of 37
6.6 Removing the initial breakpoint on debug startup
When the debugger starts, it automatically sets a breakpoint at the first statement in the
main() function. One can remove this breakpoint as follows:
1. Right click on the project and choose Launch Configurations Open Current
Launch Configuration.
Fig 31. Open Current Launch Configuration
2. Choose the Debug configuration
3. Choose the tab Debugger
4. Uncheck the box near “Stop on startup at:”
5. Click onto Apply and then Close.
AN11281 male. manage, and mu mmigumunns O [M- v ngnmdnsnoi as: ‘ , , 1 “Mm: RC“! Puma-1mm ‘ l‘ ; Enemommm “ 7,— Q [E I \ 'E 3' ' typgmmtm r5 tic» Winn m tic“ Ana 1:: Aw.:.[ ' ' om towns mm" 99! Yugm :onfigumvrm m up. Pumnmum m p hunch Group deggu (anfiguiunn 33x chnTm Emma" ‘ m! 37
NXP Semiconductors
AN11281
PREV601 Quick Startup Guide
AN11281
All information provided in this document is subject to legal disclaimers.
© NXP B.V. 2013. All rights reserved.
Application note
COMPANY PUBLIC
Rev. 1.510 November 2013
243915
33 of 37
Fig 32. Disable the initial breakpoint
AN11281 LPCXpresso website www.nxp.com/redirect/|pcware.c0m/|pcxpresso/downloads/older htlD://www.nxu.com/documents/dala sheel/CLR0663.Ddf htlD://www.nxu.com/documents/user manual/UM10441.Ddf www.nxD.cum/redirectjconrad.aUce/de/Droduct/741119/STIFTLEISTEr1rXraer POLIGVVERGOLVRM7254 www.nxD.ccmiredirectjconrad.aUce/de/Droduct/736427/BUCHSENLEISTEr EIN REIH IG7367POL|G7RM254 hug://www.nxg.com/documents/software/ZOOE1 0.119 htlD://www.nxD.com/documents/aup‘icalicn note/AN11021.Dd1 htlD://www.nxu.com/documents/dala sheet/h1037030.pdf htlD://www.nxD.com/urod[Acts/identification and securitv/nfc and reader ics/hitaq reader ics/HTRC11001T.htm1#documentalicn htlD://www.nxD.com/uroducts/identiflcation and securitv/reader ics/conlact‘ess re ader systems/PRH601HL.htm1 hug://www.nxg.com/demoboard/PREV601.html htlD://www.nxD.com/documents/aup‘icalicn note/AN11145.Dd1 htlg://www.nxg.com/demob0ard/CLEV6633.htm| htlD://www.nxu.com/documents/user manual/UM10721.Ddf www.nxp.ccmiredirectjnfcrfcrum.cm/suecs/soec license www.nXD.com/redirem/nicrforum.ora/suecs/suec license m 37
NXP Semiconductors
AN11281
PREV601 Quick Startup Guide
AN11281
All information provided in this document is subject to legal disclaimers.
© NXP B.V. 2013. All rights reserved.
Application note
COMPANY PUBLIC
Rev. 1.510 November 2013
243915
34 of 37
7. References
[1] LPCXpresso website
www.nxp.com/redirect/lpcware.com/lpcxpresso/downloads/older
[2] RC663 data sheet
http://www.nxp.com/documents/data_sheet/CLRC663.pdf
[3] LPC1227 User Manual
http://www.nxp.com/documents/user_manual/UM10441.pdf
[4] Multipoint Connectors we used:
Grid Dimension: 2.54mm, at least 27 pins
www.nxp.com/redirect/conrad.at/ce/de/product/741119/STIFTLEISTE-1-X-36-
POLIG-VERGOL-RM-254
and
www.nxp.com/redirect/conrad.at/ce/de/product/736427/BUCHSENLEISTE-
EINREIHIG-36-POLIG-RM254
[5] Direct link to the NXP Reader Library
http://www.nxp.com/documents/software/200310.zip
[6] RC663 and NXP Reader Library
http://www.nxp.com/documents/application_note/AN11021.pdf
[7] HITAG HTRC110 data sheet
http://www.nxp.com/documents/data_sheet/ht037030.pdf
[8] HTRC11001T
http://www.nxp.com/products/identification_and_security/nfc_and_reader_ics/hitag_
reader_ics/HTRC11001T.html#documentation
[9] PRH601HL
http://www.nxp.com/products/identification_and_security/reader_ics/contactless_re
ader_systems/PRH601HL.html
[10] PREV601 demo board
http://www.nxp.com/demoboard/PREV601.html
[11] AN11145 - low power card detection Quick Start Guide
http://www.nxp.com/documents/application_note/AN11145.pdf
[12] Product information page of the CLEV663B evaluation board
http://www.nxp.com/demoboard/CLEV663B.html
[13] NXP Reader Library P2P user manual
http://www.nxp.com/documents/user_manual/UM10721.pdf
[14] Technical SpecificationSimple NDEF Exchange Protocol, NFCForum-TS-
SNEP_1.0, available on www.nxp.com/redirect/nfc-forum.org/specs/spec_license
[15] Technical Specification Logical Link Control Protocol, NFCForum-TS-LLCP_1.1,
available on www.nxp.com/redirect/nfc-forum.org/specs/spec_license
AN11281 37
NXP Semiconductors
AN11281
PREV601 Quick Startup Guide
AN11281
All information provided in this document is subject to legal disclaimers.
© NXP B.V. 2013. All rights reserved.
Application note
COMPANY PUBLIC
Rev. 1.510 November 2013
243915
35 of 37
8. Legal information
8.1 Definitions
DraftThe document is a draft version only. The content is still under
internal review and subject to formal approval, which may result in
modifications or additions. NXP Semiconductors does not give any
representations or warranties as to the accuracy or completeness of
information included herein and shall have no liability for the consequences
of use of such information.
8.2 Disclaimers
Limited warranty and liabilityInformation in this document is believed to
be accurate and reliable. However, NXP Semiconductors does not give any
representations or warranties, expressed or implied, as to the accuracy or
completeness of such information and shall have no liability for the
consequences of use of such information.
In no event shall NXP Semiconductors be liable for any indirect, incidental,
punitive, special or consequential damages (including - without limitation -
lost profits, lost savings, business interruption, costs related to the removal
or replacement of any products or rework charges) whether or not such
damages are based on tort (including negligence), warranty, breach of
contract or any other legal theory.
Notwithstanding any damages that customer might incur for any reason
whatsoever, NXP Semiconductors’ aggregate and cumulative liability
towards customer for the products described herein shall be limited in
accordance with the Terms and conditions of commercial sale of NXP
Semiconductors.
Right to make changesNXP Semiconductors reserves the right to make
changes to information published in this document, including without
limitation specifications and product descriptions, at any time and without
notice. This document supersedes and replaces all information supplied prior
to the publication hereof.
Suitability for useNXP Semiconductors products are not designed,
authorized or warranted to be suitable for use in life support, life-critical or
safety-critical systems or equipment, nor in applications where failure or
malfunction of an NXP Semiconductors product can reasonably be expected
to result in personal injury, death or severe property or environmental
damage. NXP Semiconductors accepts no liability for inclusion and/or use of
NXP Semiconductors products in such equipment or applications and
therefore such inclusion and/or use is at the customer’s own risk.
ApplicationsApplications that are described herein for any of these
products are for illustrative purposes only. NXP Semiconductors makes no
representation or warranty that such applications will be suitable for the
specified use without further testing or modification.
Customers are responsible for the design and operation of their applications
and products using NXP Semiconductors products, and NXP
Semiconductors accepts no liability for any assistance with applications or
customer product design. It is customer’s sole responsibility to determine
whether the NXP Semiconductors product is suitable and fit for the
customer’s applications and products planned, as well as for the planned
application and use of customer’s third party customer(s). Customers should
provide appropriate design and operating safeguards to minimize the risks
associated with their applications and products.
NXP Semiconductors does not accept any liability related to any default,
damage, costs or problem which is based on any weakness or default in the
customer’s applications or products, or the application or use by customer’s
third party customer(s). Customer is responsible for doing all necessary
testing for the customer’s applications and products using NXP
Semiconductors products in order to avoid a default of the applications and
the products or of the application or use by customer’s third party
customer(s). NXP does not accept any liability in this respect.
Export controlThis document as well as the item(s) described herein
may be subject to export control regulations. Export might require a prior
authorization from competent authorities.
Evaluation productsThis product is provided on an “as is” and “with all
faults” basis for evaluation purposes only. NXP Semiconductors, its affiliates
and their suppliers expressly disclaim all warranties, whether express,
implied or statutory, including but not limited to the implied warranties of non-
infringement, merchantability and fitness for a particular purpose. The entire
risk as to the quality, or arising out of the use or performance, of this product
remains with customer.
In no event shall NXP Semiconductors, its affiliates or their suppliers be
liable to customer for any special, indirect, consequential, punitive or
incidental damages (including without limitation damages for loss of
business, business interruption, loss of use, loss of data or information, and
the like) arising out the use of or inability to use the product, whether or not
based on tort (including negligence), strict liability, breach of contract, breach
of warranty or any other theory, even if advised of the possibility of such
damages.
Notwithstanding any damages that customer might incur for any reason
whatsoever (including without limitation, all damages referenced above and
all direct or general damages), the entire liability of NXP Semiconductors, its
affiliates and their suppliers and customer’s exclusive remedy for all of the
foregoing shall be limited to actual damages incurred by customer based on
reasonable reliance up to the greater of the amount actually paid by
customer for the product or five dollars (US$5.00). The foregoing limitations,
exclusions and disclaimers shall apply to the maximum extent permitted by
applicable law, even if any remedy fails of its essential purpose.
8.3 Licenses
Purchase of NXP ICs with ISO/IEC 14443 type B functionality
This NXP Semiconductors IC is ISO/IEC 14443 Type
B software enabled and is licensed under Innovatron’s
Contactless Card patents license for ISO/IEC 14443 B.
The license includes the right to use the IC in systems
and/or end-user equipment.
RATP/Innovatron
Technology
8.4 Trademarks
Notice: All referenced brands, product names, service names and
trademarks are property of their respective owners.
MIFARE is a trademark of NXP B.V.
DESFire is a trademark of NXP B.V.
MIFARE Ultralight is a trademark of NXP B.V.
MIFARE Plus is a trademark of NXP B.V.
AN11281
NXP Semiconductors
AN11281
PREV601 Quick Startup Guide
AN11281
All information provided in this document is subject to legal disclaimers.
© NXP B.V. 2013. All rights reserved.
Application note
COMPANY PUBLIC
Rev. 1.510 November 2013
243915
36 of 37
9. List of figures
Fig 1. Picture of the PREV601 board .......................... 3
Fig 2. PREV601M Microboard .................................... 4
Fig 3. LPC-Link ........................................................... 5
Fig 4. Multipoint Connectors ....................................... 5
Fig 5. Connecting the PREV601 board to the LPC
Link ................................................................... 6
Fig 6. LPCXpresso with the Multipoint Connectors ..... 6
Fig 7. Enumeration of the LPCXpresso Board in
Device Manager Window .................................. 7
Fig 8. LPCXpresso installation setup wizard 1 ............ 8
Fig 9. LPCXpresso installation setup wizard 2 ............ 9
Fig 10. LPCXpresso installation setup wizard 3 ............ 9
Fig 11. Windows Security dialog ................................. 10
Fig 12. LPCXpresso installation setup wizard 4 .......... 10
Fig 13. LPCXpresso IDE ............................................. 11
Fig 14. Product activation ........................................... 11
Fig 15. Product activation ........................................... 12
Fig 16. Product activation ........................................... 12
Fig 17. Importing a project into the LPCXpresso IDE .. 13
Fig 18. Importing a project into the LPCXpresso IDE .. 14
Fig 19. Importing a project into the LPCXpresso IDE .. 14
Fig 20. Run the project ................................................ 15
Fig 21. Run the project ................................................ 16
Fig 22. Run the project ................................................ 16
Fig 23. Run the project ................................................ 17
Fig 24. Run the project ................................................ 17
Fig 25. Stop the project ............................................... 18
Fig 26. Debug Buttons ................................................ 18
Fig 27. Importing the project ....................................... 20
Fig 28. Architecture of the NXP reader library ............. 22
Fig 29. Select the build configuration .......................... 24
Fig 30. Select the level of optimization ........................ 25
Fig 31. Open Current Launch Configuration ............... 32
Fig 32. Disable the initial breakpoint ........................... 33
AN11281
NXP Semiconductors
AN11281
PREV601 Quick Startup Guide
Please be aware that important
notices concerning this document and the product(s)
described herein, have been included in the section 'Legal information'.
© NXP B.V. 2013. All rights reserved.
For more information, visit:
http://www.nxp.com
For sales office addresses, please send an email to: salesaddresses@nxp.com
Date of release:
10 November 2013
243915
Document identifier:
AN11281
10. Contents
1. Introduction ......................................................... 3
2. Hardware overview of the Demo Reader ........... 3
2.1 PREV601 board ................................................. 3
2.2 LPC-Link LPC3154 ............................................ 4
2.3 Preparation of the hardware ............................... 5
3. Connecting the hardware to a computer ........... 7
4. Managing the Demo Reader project with
LPCXpresso IDE .................................................. 7
4.1 Installation of LPCXpresso IDE .......................... 8
4.2 Extraction of the demo reader project .............. 12
4.3 Start the project ................................................ 15
4.3.1 Run the project ................................................. 15
5. Associated Projects .......................................... 19
5.1 Communication with MIFARE Ultralight ........... 19
5.2 Communication with MIFARE Classic .............. 19
5.3 Communication with MIFARE DESFire ............ 19
5.4 Polling .............................................................. 19
5.5 Peer to Peer functionality ................................. 19
5.5.1 Installation ........................................................ 19
5.5.2 SNEP client project .......................................... 20
5.5.2.1 What is going on inside? .................................. 20
5.5.2.2 Choosing the NDEF message .......................... 21
6. Supplementary Notes ....................................... 22
6.1 Software architecture ....................................... 22
6.1.1 Bus abstraction layer ........................................ 23
6.1.2 Hardware abstraction layer .............................. 23
6.1.3 Protocol abstraction layer ................................. 23
6.1.4 Application layer ............................................... 23
6.2 Build configuration ............................................ 23
6.3 Level of compiler optimization .......................... 24
6.3.1 Optimization issues .......................................... 25
6.4 Hardware configuration and SPI usage ............ 26
6.4.1 Hardware configuration .................................... 26
6.4.1.1 PREV601 board type definition ........................ 26
6.4.1.2 Reading IC or board type ................................. 26
6.4.1.3 Low Power Card Detection mode (LPCD)
definition ........................................................... 26
6.4.1.4 Communication interface definition .................. 27
6.4.1.5 Debug printout definition .................................. 27
6.4.2 Usage of the SPI interface ............................... 27
6.5 LPCD mode configuration ................................ 28
6.5.1 Library support ................................................. 28
6.5.2 LPCD software usage ...................................... 29
6.5.3 The I and Q Register settings........................... 30
6.5.4 What to do if the PREV601 board does not stay
in LPCD mode .................................................. 31
6.6 Removing the initial breakpoint on debug
startup .............................................................. 32
7. References ......................................................... 34
8. Legal information .............................................. 35
8.1 Definitions ......................................................... 35
8.2 Disclaimers ....................................................... 35
8.3 Licenses ........................................................... 35
8.4 Trademarks ...................................................... 35
9. List of figures ..................................................... 36
10. Contents ............................................................. 37

Products related to this Datasheet

EVAL BOARD FOR PR601