ENC8 Model Datasheet by Red Lion Controls

View All Related Products | Download PDF Datasheet
MODEL ENC
1
MODEL ENC8 - NEMA 4 ENCLOSURES FOR CUB4, CUB5, DT8 & DT9 UNITS
Bulletin No. ENC8/8B-F
Drawing No. LP0389
Released 04/13
Tel +1 (717) 767-6511
Fax +1 (717) 764-0839
www.redlion.net
ENC8A & ENC8B - PLASTIC ENCLOSURES
ENC8A DIMENSIONS In inches (mm)
ENC8B DIMENSIONS In inches (mm)
3.14
5.12 (130.0) 3.04
(79.8)
(77.2)
(121.9)
4.72 (119.9) 3.77
(95.8)
4.80
DESCRIPTION
These enclosures are designed for applications requiring a water resistant
instrument enclosure. The enclosures are fabricated of polycarbonate and are
designed to withstand NEMA 4X/IP65 wash-down applications. The enclosures
must be drilled to accept conduit fittings or other types of wiring connectors.
The enclosures can be used free-standing, or securely fastened to a mounting
surface.
ORDERING INFORMATION
MODEL NO. DESCRIPTION PART NUMBER
ENC8A
Plastic Enclosure for single units
ENC8A000
ENC8B
Plastic Enclosure for units with an MLPS1 attached
ENC8B000
For More information on Pricing, Enclosures & Panel Mount Kits, refer to the
RLC Catalog or contact your local RLC Distributor.
ENC8A INSTALLATION
It is recommended to wire the unit before mounting it in the enclosure to
ensure good electrical connections. The following steps outline the most
common sequence for installing a unit without an MLPS1 attached.
1. Determine the location of the conduit fitting and drill the necessary hole.
Install the fitting and bring the wiring into the enclosure.
2. Slide the panel gasket over the rear of the unit to the back of the bezel.
3. Assemble nut fastener and mounting screw onto both sides of the mounting
clip. The tip of the screw should not project from the hole in mounting clip.
4. Install the unit through the opening in the front of the lid until the bezel
flange contacts the panel.
5. Slide the mounting plate over the rear of the unit until it is against the inside
front of the enclosure.
6. Slide the mounting clip over the rear of the unit until the mounting clip is
against the inside of the enclosure. The mounting clip has latching features
which engage into mating features on the unit’s housing.
Note: It is necessary to hold the unit in place when sliding
the mounting clip into position.
7. Alternately tighten each screw to ensure uniform gasket
pressure. Visually inspect the front panel gasket. The
gasket should be compressed to about 75 to 80% of its
original thickness (Recommended torque is 28 to 36
in-oz.). If not, gradually turn mounting screws to
further compress the gasket.
8. If the gasket is not adequately compressed, and the
mounting screws can no longer be turned, loosen the
mounting screws and check that the mounting clip is
latched as close as possible to the inside of enclosure.
Repeat the procedure for tightening the screws.
9. Connect the necessary wires to the unit for the application desired.
10. Assemble the enclosure with the screws provided. Alternately tighten each
screw to ensure uniform gasket pressure.
ENCLOSURE,
SCREW
MOUNTING
MOUNTING
CLIP
CONTROL
LINES
GASKET
UNIT
LATCHING
FEATURE
NUT
FASTENER
UNIT
FRONT
ENCLOSURE,
REAR
MOUNTING
PLATE
2
ENC8B w/ MLPS1 Installation
Installing a unit with an MLPS1 attached requires some planning. It is
recommended that the unit with the MLPS1 attached be temporarily installed
in the enclosure to determine the best location for the conduit fitting to avoid
interference with the MLPS1.
1. Determine the location of the conduit fitting and drill the necessary hole.
Install the fitting and bring the wiring into the enclosure.
2. Slide the panel gasket over the rear of the unit to the back of the bezel.
3. Remove the common and V+ screw terminals from the rear of the unit (save
for later use) and replace them with the stand-offs (supplied with the
MLPS1).
4. Assemble nut fastener and mounting screw onto both sides of the mounting
clip. The tip of the screw should not project from the hole in mounting clip.
5. Install the unit through the opening in the front of the lid until the bezel
flange contacts the panel mounted gasket.
6. Slide the mounting plate over the rear of the unit until it is against the inside
front of the enclosure.
7. Slide the mounting clip over the rear of the unit until the mounting clip is
against the inside of the enclosure. The mounting clip has latching features
which engage into mating features on the unit’s housing.
Note: It is necessary to hold the unit in place when sliding the
mounting clip into position.
8. Alternately tighten each screw to ensure uniform gasket pressure. Visually
inspect the front panel gasket. The gasket should be compressed to about 75
to 80% of its original thickness (Recommended torque is 28 to 36 in-oz.). If
not, gradually turn mounting screws to further compress the gasket.
9. If the gasket is not adequately compressed, and the mounting screws can no
longer be turned, loosen the mounting
screws and check that the mounting clip
is latched as close as possible to the
inside of enclosure. Repeat the
procedure for tightening the screws.
10. Mount the MLPS1 and optional sensor wires needed, to the stand-offs
using the screw terminals from the unit with the supplied square washers.
11. Connect AC power to the terminal block of the MLPS1.
12. After all electrical connections have been made, assemble the enclosure
with the screws provided. Alternately tighten each screw to ensure uniform
gasket pressure.
ENCLOSURE, SCREW
MOUNTING
SQUARE
SCREW TERMINALS
FROM REAR OF UNIT
HEX STAND-OFF ( 2 )
MLPS
MOUNTING
CLIP
WASHER
SENSOR
EXCITATION
CONTROL
LINES
GASKET
UNIT
LATCHING
FEATURE
NUT
FASTENER
UNIT
(OPTIONAL)
AC POWER
FOR MLPS
FRONT
REAR
ENCLOSURE,
MOUNTING
PLATE
DIMENSIONS In inches (mm)
3.504.50
4.15
4.00
(88.9)(114.3)
(105.4)
(101.6)
DESCRIPTION
This enclosure is designed for use with the CUB4, CUB5, DT8 & DT9 units.
The enclosures are large enough to accommodate a Micro-line Power Supply
(MLPS1) attached to the unit. These rugged enclosures are fabricated of formed
steel with all seams welded to withstand NEMA 4/IP65 wash-down applications.
The kits are coated with a durable black polyurethane finish.
The holes for conduit fittings or other types of wiring connectors can be
drilled through the removable rear access panel, or through the enclosure itself.
The enclosures can be free standing or securely fastened to a mounting
surface with the brackets and hardware found in the mounting kit (provided
with the enclosure). The brackets also allow the enclosure to be raised and/or
tilted from the mounting surface in order to achieve the most favorable
operating position. Provided are four self-stick foot pads that can be applied to
the bottom of the enclosure to protect the mounting surface. The foot pads are
particularly useful for free standing installations.
PART NUMBERMODEL NO
ENC80000
DESCRIPTION
ENC8
NEMA 4/IP65 ENCLOSURE
For More information on Pricing, Enclosures & Panel Mount Kits,
refer to the RLC Catalog or contact your local RLC Distributor.
ORDERING INFORMATION
ENC8 - STEEL ENCLOSURE
ENCH INSTALLATION ENCH w/ MLPS1 Installation
3
ENC8 w/ MLPS1 Installation
Installing a unit with an MLPS1 attached requires some planning. It is
recommended that the unit with the MLPS1 attached be temporarily installed
in the enclosure to determine the best location for the conduit fitting to avoid
interference with the MLPS1.
1. Mark the location of the conduit fitting and drill the necessary hole.
2. Apply adhesive side of panel gasket to rear enclosure opening.
DO NOT APPLY THE ADHESIVE SIDE OF THE GASKET TO THE
ACCESS PANEL.
3. Slide the panel gasket over the rear of the unit to the back of the bezel.
4. Remove the common and V+ screw terminals from the rear of the unit (save
for later use) and replace them with the hex drive stand-offs (supplied with
the MLPS1).
5. Assemble nut fastener and mounting screw onto both sides of the mounting
clip. The tip of the screw should not project from the hole in mounting clip.
6. Route the wire to be connected to the unit from the conduit fitting through the
mounting clip, and then through the rear of the enclosure and out the front.
7. Connect the necessary wires to the unit for the application desired.
8. Install the unit through the opening in the front of the enclosure until the
bezel flange contacts the panel mounted gasket.
9. Slide the mounting clip over the rear of the unit until the mounting clip is
against the inside of the enclosure. The mounting clip has latching features
which engage into mating features on the unit’s housing.
Note: It is necessary to hold the unit in
place when sliding the
mounting clip into
position.
10. Alternately tighten each screw to ensure uniform gasket pressure. Visually
inspect the front panel gasket. The gasket should be compressed to about 75
to 80% of its original thickness (Recommended torque is 28 to 36 in-oz.). If
not, gradually turn mounting screws to further compress the gasket.
11. If the gasket is not adequately compressed, and the mounting screws can
no longer be turned, loosen the mounting screws and check that the
mounting clip is latched as close as possible to the inside of enclosure.
Repeat the procedure for tightening the screws.
12. Connect AC power to the terminal block of the MLPS1.
13. Mount the MLPS1 and optional sensor wires needed, to the stand-offs
using the screw terminals from the unit with the supplied square washers.
14. After all electrical connections have been made, attach the rear access
panel to the enclosure with the eight screws provided.
15. Alternately tighten each screw to ensure uniform gasket pressure. Visually
inspect the sponge rubber gasket. The gasket should be compressed to about
75 to 80% of its original thickness.
ENCLOSURE
SCREW
MOUNTING
SQUARE
SCREW TERMINALS
FROM REAR OF UNIT
HEX STAND-OFF (2 TYP)
MLPS
MOUNTING
CLIP
WASHER
REAR
SCREW
CONDUIT FITTING
(8 PLACES)
ACCESS
SENSOR
EXCITATION
CONTROL
LINES
GASKET
PANEL
GASKET
UNIT
LATCHING
FEATURE
NUT
FASTENER
PANEL
UNIT
(OPTIONAL)
AC POWER
FOR MLPS
TO ENSURE ADEQUATE ROOM
TO ROUTE WIRES, CONDUIT
SHOULD BE CONNECTED
IN SHADED AREA
ACCESS PANEL
ENC8 INSTALLATION
It is recommended to wire the unit before mounting it in the enclosure to
ensure good electrical connections. The following steps outline the most
common sequence for installing a unit without an MLPS1 attached.
1. Determine the location of the conduit fitting and drill the necessary hole.
2. Apply adhesive side of panel gasket to rear enclosure opening.
DO NOT APPLY THE ADHESIVE SIDE OF THE GASKET TO THE
ACCESS PANEL.
3. Slide the panel gasket over the rear of the unit to the back of the bezel.
4. Assemble nut fastener and mounting screw onto both sides of the mounting
clip. The tip of the screw should not project from the hole in mounting clip.
5. Route the wire to be connected to the unit from the conduit fitting through
the mounting clip, and then through the rear of the enclosure and out the
front.
6. Connect the necessary wires to the unit for the application desired.
7. Install the unit through the opening in the front of the enclosure until the
bezel flange contacts the panel.
8. Slide the mounting clip over the rear of the unit until the
mounting clip is against the inside of the enclosure. The
mounting clip has latching features which engage into
mating features on the unit’s housing.
Note: It is necessary to hold the unit in place when
sliding the mounting clip into position.
9. Alternately tighten each screw to ensure uniform
gasket pressure. Visually inspect the front panel
gasket. The gasket should be compressed to about
75 to 80% of its original thickness (Recommended
torque is 28 to 36 in-oz.). If not, gradually turn
mounting screws to further compress the gasket.
10. If the gasket is not adequately compressed, and the mounting screws can
no longer be turned, loosen the mounting screws and check that the
mounting clip is latched as close as possible to
the inside of the enclosure. Repeat the
procedure for tightening the screws.
11. Attach the rear access panel to the enclosure
with the eight screws provided.
12. Alternately tighten each screw to
ensure uniform gasket pressure.
Visually inspect the sponge rubber
gasket. The gasket should be
compressed to about 75 to 80% of its
original thickness.
GASKET
ENCLOSURE
GASKET
SCREW
(8 PLACES)
UNIT
MOUNTING
SCREW
NUT
FASTENER
ACCESS
PANEL
LATCHING
FEATURE
LATCHING
FEATURE
CONDUIT
FITTING
CONTROL LINES
PANEL
UNIT
MOUNTING THE ENCLOSURE
1. Self-stick foot pads may be applied to the features on the bottom of the enclosure to
protect the mounting surface.
2. To securely mount the enclosure, attach the adjustable mounting brackets to the
enclosure using the plastic washers and screws. Mounting brackets may be attached to
the top or bottom of the enclosure.
3. Secure the adjustable mounting brackets to mounting location with the screws provided.
ENCLOSURE
GASKET
ACCESS PANEL
SCREW
(8 PLACES)
SCREW
ADJUSTABLE MOUNTING BRACKET
(BOTH SIDES)
PLASTIC
WASHER
PLASTIC
WASHER
UNIT WITH OR
WITHOUT
POWER SUPPLY
FOOT PADS
(4 PLACES)
(4 PLACES)
FOOT PADS
TYPICAL MOUNT WITH
WATERTIGHT CABLE
ENTERING THROUGH
BACK COVER
LIMITED WARRANTY
The Company warrants the products it manufactures against defects in materials and workmanship
for a period limited to two years from the date of shipment, provided the products have been stored,
handled, installed, and used under proper conditions. The Company’s liability under this limited
warranty shall extend only to the repair or replacement of a defective product, at The Company’s
option. The Company disclaims all liability for any affirmation, promise or representation with
respect to the products.
The customer agrees to hold Red Lion Controls harmless from, defend, and indemnify RLC against
damages, claims, and expenses arising out of subsequent sales of RLC products or products
containing components manufactured by RLC and based upon personal injuries, deaths, property
damage, lost profits, and other matters which Buyer, its employees, or sub-contractors are or may be
to any extent liable, including without limitation penalties imposed by the Consumer Product Safety
Act (P.L. 92-573) and liability imposed upon any person pursuant to the Magnuson-Moss Warranty
Act (P.L. 93-637), as now in effect or as amended hereafter.
No warranties expressed or implied are created with respect to The Company’s products except
those expressly contained herein. The Customer acknowledges the disclaimers and limitations
contained herein and relies on no other warranties or affirmations.
Red Lion Controls
Headquarters
20 Willow Springs Circle
York PA 17406
Tel +1 (717) 767-6511
Fax +1 (717) 764-0839
Red Lion Controls
China
Unit 302, XinAn Plaza
Building 13, No.99 Tianzhou Road
ShangHai, P.R. China 200223
Tel +86 21 6113 3688
Fax +86 21 6113 3683
Red Lion Controls
Europe
Softwareweg 9
NL - 3821 BN Amersfoort
Tel +31 (0) 334 723 225
Fax +31 (0) 334 893 793
Red Lion Controls
India
201-B, 2nd Floor, Park Centra
Opp 32 Mile Stone, Sector-30
Gurgaon-122002 Haryana, India
Tel +91 984 487 0503

Products related to this Datasheet

ENCLOSURE CUB4/CUB5 CHASSIS MNT
ENCLOSURE CUB4/5 DT8 CHASSIS MNT
ENCLOSURE CUB4/CUB5 CHASSIS MNT