CP2114 Eval Kit Quick Start Guide Datasheet by Silicon Labs

View All Related Products | Download PDF Datasheet
SEV'I NUUI'IIS - connectthe CP2114 evaluation board to ttie daughter card. a connect headphones andior powered speakers to the appropriate daughteroard connector: HP our: headphone output LINE OUT: line output [to powered speakers) HPlLINE OUT (wmaoza daughtercard only); common connector tor headphone or line output. connect the use cable to the CF2114 evaluation board (42). Next, connect the other end or the use cable directty to the host computer, Note: Do not use a USB hub. Right—click on the “Speakers" icon in the Windows systems Tray and left—cllck “Playback devtces". a select “CFZIM USE-Audio Bridge", click “set Default" button, Next, Verlfy the ch1 14 is checked as the default Play audio from the host computer using any media player application and verlfy high-quality audio trom the headphones playback or powered speakers attached to the r deuice. daughter card, , The “Wlndows Volume and Mute" section “Wk Gems describes how to control playback mute and Recording darka volume Sounds ‘1 “ “l Volume (ontvol options I: J hi; to: din mm - Right ick on the “Speakers" icon and Set volume and mute. Volume and mute DeVice Audio Source Volume left-cllck “Open Volume Mixer". can be controlled in two ways, and both Volume methods are supported by the CP211A: n- t m p,.. “Managua“, , 1. Device volume and Mute: this control P“ W” “Fe" "0"“! MW sends use volume and mute control [I x! LE lol messages to the device Generally, this s, m ' Wm “Wm 11:“ Playback devices wIII adiust the volume control 0! the DAc V F 1 , , in hardware usln lc writes. Rxcvdmg dszes 9 a ,, ,, , Sounds 2. Audio Source Volume and Mute: these controls scale the audio signal sent over v I t I . uss and can be set indiVidually. The « w «i «2 ° W“ ‘°“ '° ”hm“ CP21IA volume can be set with these A A A EDIIIIOIS. . Deyice _ Mule Audio Source Mme Connect a powered microphone or line- ievel analog audio source to the analog in (AIN) connector (P2). n Right-click on the ‘Speakers‘ icon and left-click on “Recording GEVICeS". Open a recorder application to record the audio input Or listen in real time by selecting “Pmpel’ties” and checklng the “Llsten to this device" button. Selectthe cpziturom the “Playbackthrought is device" dmpdown to select lull loop tastings ‘Note: Audio input is supported only on the csusts daugittercard. not the wmsszs and PCM1774 daughteroards. Although the PCM1774 daughtercard has an ANALOG IN jack,mls audio is not digitized and sent to the host because the PCM1774 is a DAG-only device The PCM1774 has the ability to mix the ANALOG IN signal with the analog output produced by its me.
EVALUATION BOARD/KIT IMPORTANT NOTICE
Silicon Laboratories Inc. and its affiliated companies ("Silicon Labs") provides the enclosed evaluation board/kit to the user ("User") under the following conditions:
This evaluation board/kit ("EVB/Kit") is intended for use for ENGINEERING DEVELOPMENT, TESTING, DEMONSTRATION, OR EVALUATION PURPOSES ONLY and is not a finished
end-product fit for general consumer use. ANY OTHER USE, RESALE, OR REDISTRIBUTION FOR ANY OTHER PURPOSE IS STRICTLY PROHIBITED. This EVB/Kit is not intended to
be complete in terms of required design-, marketing-, and/or manufacturing-related protective considerations, including product safety and environmental measures typically found in end
products that incorporate such semiconductor components or circuit boards. As such, persons handling this EVB/Kit must have electronics training and observe good engineering practice
standards. As a prototype not available for commercial reasons, this EVB/Kit does not fall within the scope of the European Union directives regarding electromagnetic compatibility,
restricted substances (RoHS), recycling (WEEE), FCC, CE or UL, and therefore may not meet the technical requirements of these directives or other related directives.
Should this EVB/Kit not meet the specifications indicated in the User's Guide, the EVB/Kit may be returned within 30 days from the date of delivery for a full refund. THE FOREGOING
WARRANTY IS THE EXCLUSIVE WARRANTY MADE BY SILICON LABS TO USER, IS USER'S SOLE REMEDY, AND IS IN LIEU OF ALL OTHER WARRANTIES, EXPRESSED,
IMPLIED, OR STATUTORY, INCLUDING ANY WARRANTY OF MERCHANTABILITY, NONINFRINGEMENT, DESIGN, WORKMANSHIP, OR FITNESS FOR ANY PARTICULAR PUR-
POSE.
User assumes all responsibility and liability for proper and safe handling of the EVB/Kit. Further, User indemnifies Silicon Labs from all claims arising from User's handling or use of the
EVB/Kit. Due to the open construction of the EVB/Kit, it is User's responsibility to take any and all appropriate precautions with regard to electrostatic discharge.
EXCEPT TO THE EXTENT OF THE INDEMNITY SET FORTH ABOVE, NEITHER PARTY SHALL BE LIABLE TO THE OTHER FOR ANY INDIRECT, SPECIAL, INCIDENTAL, OR CON-
SEQUENTIAL DAMAGES.
Neither Silicon Labs nor User is obligated to perform any activities or conduct any business as a consequence of using the EVB/Kit, and neither party is entitled to any form of exclusivity
with respect to the EVB/Kit.
Silicon Labs assumes no liability for applications assistance, customer product design, software performance, or infringement of patents or services described herein.
Please read the User's Guide and, specifically, the Warnings and Restrictions notice in the User's Guide prior to handling the EVB/Kit. This notice contains important safety information
about temperatures and voltages. For additional environmental and/or safety information, please contact a Silicon Labs application engineer or visit www.silabs.com/support/quality.
No license is granted under any patent right or other intellectual property right of Silicon Labs covering or relating to any machine, process, or combination in which the EVB/Kit or any of its
components might be or are used.
User's use of this EVB/Kit is conditioned upon acceptance of the foregoing conditions. If User is unwilling to accept these conditions, User may request a refund and return the EVB/Kit to
Silicon Labs in its original condition, unopened, with the original packaging and all documentation to:
Mailing Address:
400 W. Cesar Chavez
Austin, TX 78701
CP2114 USB AUDIO TO I2S DIGITAL AUDIO BRIDGE
QUICK-START GUIDE
The CP2114 Evaluation Kits are stand-alone evaluation platforms with easy access to all signals on the device. All evaluation kits
come with a CP2114 evaluation board, USB cable, and RS-232 cable. Some Evaluation Kits come with a CODEC/DAC daughter
card to allow the product to play audio out-of-the-box.
CP2114 Evaluation Kit (CP2114-EK)
CP2114 evaluation board
USB cable
RS-232 cable
CP2114-CS42L55 Evaluation Kit (CP2114-CS42L55EK)
CP2114 evaluation board
Daughter card with Cirrus Logic CS42L55 CODEC
Ear bud headphones
Audio cable: 3.5 mm male-to-male
USB cable
RS-232 cable
CP2114-WM8523 Evaluation Kit (CP2114-WM8523EK)
CP2114 evaluation board
Daughter card with Cirrus Logic WM8523 DAC
Ear bud headphones
USB cable
RS-232 cable
CP2114-PCM1774 Evaluation Kit (CP2114-PCM1774EK)
CP2114 evaluation board
Daughter card with Texas Instruments PCM1774 DAC
Ear bud headphones
USB cable
RS-232 cable
Windows—Audio Output
Windows—Volume and Mute
Windows—Audio Input*
eJeMuos uouemfiguoo em 3er 0: Mon saquosep emu uopeoudde SNJ. .‘epjns UOJJEZJWOJSHQ aqmea XLLZdQ/XOLZdQ ‘LZLNV Jexdepv 21911123 asn-OJ-Buwmfin 'eomos ogpne sq; uo ogpne [em uem ‘fiugplooe; ugfiaa '(‘cna ‘aagquagnD ‘puegafimag 'B'e) Sam ogpmz SploDaJ)2Lfll—l0!1¢3!|dd2 pad! uz uedo ‘mdu! ogpnz y; lZdD ewusuowep o; 'ugafi alu susnfpe gva am pm; 32. 2M ova aq|o1s1uamlsnlpz amnloA esem 8|»wa vuza: mu 'VLLZdD sum gsn JaAo sefizssaw emnlon “as“ $520 ogpnv gsn spues Jepus sLunloA ddv em fiunsnlpv 31102!an aNI‘I PUB (euoudpeau) mo dH euoqdpeeq an; uo )ueseJd sq p|noqs ogpne mu '9"; ogpmz ue field pun ('319 ‘saunl! ‘pod! 13-9) 53"; 0!an sAeld .2.“ uogwogldde pad! ue uedo ‘Jndlno ogpne VLLZdD ewusuowep oi acunos ogpnv eomos owne 0: (Zd) )ndu! Bolauv seuoqdpaaq 0: (de mdmo euoqdpeeH slenaeds pale/mod 0| 15") mo aun w deo 9111 0: pamw Annalmumne aq lllM mp 0mm: all) ‘pad! em 0! PBIOSUUUO s! m, LZdD E JeneueqM {eagnep >102q£u|d em SE n deg at" news Ausnuem o) Alzssaaau wu 8! u 112d! PUB 9A3 vuzao em OI n maepv mum; asn-o;—Bugum6!‘| a mauuo; '319 ‘euoqdoJogw 081318 ‘5qu a; ‘JaABId NW ‘auoqd! ‘pod! ue eq uea aojnos ugpnz an” 1de 1132! my em 0; eanos ogpne Bo|eu2 uB laeuuoz) 'seuoqdpzeq 01 (N) nonuno dH ewe/PUB Slaxeeds P319M°d 01 (9d) >138! mo ENI‘I am iaauuoa 'Jeqwfio; pjaajawfimzq pue pleomalnuw vuzao aumauuoo Amen "sawmoA Jno-auu pu: euoqdpeau qzoq snag: awnloA 5qu 'saficssam aulmoA s52]: ogpnvasn puns Jnu sup 1| 'asn Jane was an 12m saldwcs ogpn: an: all”: M1991"! o: “W am susnu 5qu :aumlnA “uni! 'ln dxno Ina-w” nu: pu: mdana auoqdpuq ova aux llmq N was an swa manna: amnlon 'Auuauna 'uer up sunlp: ova nu pun: 3z| EM 3V0 an: a) sxuauusnIp! amnIaA “all: SWIM”! vuzao “41.17”de an: a: asn nno saBussam amnlaA M365.. ssm '1!an asn Spuas sun 329x521 52w :aumlaA isnfln: o: spoqxam am we null "'sajuaand punos 35PM omnv-asn VIIZdJ u| aun auoudongul |2unlu| /‘ ”m; m =5le WWW—85f} VI I NC) Hamid; pm 31u| r M ,: ”030 'n two in: “3mm“ (.1. a!pn2)pmn1 10 (mo own!) And Mau um mu 11cm in! JD) aolnap In du| all! pun sndmo punos am so VLLZdD aq: wales 'uoal Jaqcads an; >19“: pun uolzdo ploH 'acw an: a) pua Juno aq: PUB P190“ “Vlwnl'ma VlLZdO all! 03 am: gsn aqua pus auo zoauuoo '(Zd) mmhndug Boleu: an: o: wnns punos B loouuoo 'sauoqdpeaq oi (Mundane: aunqdpuq aux 1a “finds panMod 0) (Ed) )IOBIHID Belem: oqunuuog Indu! Bo|cuv sau oqdpceq o: andmo a no qdpcaH slaxcads PBJBMOd o: ano B oleuv 'er : Jaw Bncp on: o: pmoq uouenmu ”was "ll "Ouuoa
iPad (iOS)—Audio Output and Input
Additional Documentation
.
AN721, CP210x/CP211x Device Customization Guide: This application note describes how to use the configuration software
to configure the USB parameters on the CP21xx devices.
AN433, CP2110/4 HID to UART API Specification: This application note describes the API of the interface libraries provided
by Silicon Labs.
AN434, CP2110/4 Interface Specification: This application note describes the HID reports supported by the CP2110/4 and
the configurable parameters.
Where to Find Support
Application Notes
www.silabs.com/appnotes
MCU KnowledgeBase:
www.silabs.comSupportKnowledge Base
Video Training Modules:
www.silabs.comSupportTraining and Resources
Contact an Applications Engineer:
www.silabs.comSupportContact Technical Support
Mac OS-X—Audio Output and Input

Products related to this Datasheet

KIT EVAL CP2114
KIT EVAL CP2114-CS42L55
KIT EVAL CP2114-WM8523
KIT EVAL CP2114-PCM1774