Sensors, Transducers

0 Results
Suggestions

  • Make sure that all words or part numbers are entered correctly
  • Try different keywords
  • Try more general keywords
Additional Questions?

  • Can't find what you're looking for? Ask the TechForum
If new to DigiKey

DigiKey offers the world's largest selection of electronic components in stock and available for immediate shipment. From prototype to production, we are here to fuel innovation all over the world. We are proud to be highly recognized as the leader for:

  • Availability of Products
  • On time Delivery
  • Overall Performance
  • Engineer-Friendly Website

For more information visit Help & Support
Featured Manufacturers
Image of NOSHOK's Logo
Image of Honeywell's Logo
Image of Texas Instruments color logo
Image of SICK Logo
Image of Bourns, Inc. logo
Image of TT Electronics Logo

About Sensors, Transducers


A sensor is a device that detects physical, chemical, or environmental changes and converts them into electrical signals that can be measured or acted upon. These devices are critical in everything from industrial automation and robotics to HVAC systems and smart home technology. Sensors operate by detecting measurable changes—such as temperature, pressure, or motion—and converting them into usable electrical signals like analog voltage, digital pulses, or communication protocols (e.g., I²C, SPI, or 4–20 mA current loops). Selecting the right sensor often depends on the required signal type and the system’s ability to process or amplify that signal.

Different sensor types are suited for specific applications and technologies. For instance, temperature sensors (like thermocouples or RTDs) are used in environmental monitoring and heating systems, while pressure and flow sensors are common in fluid control, medical devices, and HVAC. Photoelectric, optical, and proximity sensors use light or capacitive fields for object detection in automation and safety systems. Humidity and gas sensors monitor environmental conditions in agriculture or lab settings, and motion or accelerometer sensors support robotics and mobile devices. Key technologies such as capacitive, resistive, ultrasonic, or magnetoresistive sensing determine the sensor’s performance characteristics—each with strengths in accuracy, response time, or cost-effectiveness.

Environmental exposure is a key consideration: Will the sensor face dust, vibration, chemicals, or moisture? Many industrial sensors (DIN rail, Chassis or Panel mount) are built to withstand harsh environments, with sealed housings or rugged materials. Others, like touch sensors or strain gauges, may require stable, controlled settings for accurate performance. By understanding both the conditions in which a sensor must operate and how it will interface with the rest of the system, purchasers can confidently choose a sensor that meets both performance and durability requirements.

Image of Thermopile schematic symbol Image of Thermocouple schematic symbol Image of Rotary Encoder schematic symbol